<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: Code Warrior code window</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Code-Warrior-code-window-JM60/m-p/198564#M16085</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;version is IDE 5.9.0 build 2404&lt;/P&gt;&lt;P&gt;The message appears in a window which overlays the code window, hence you have to click on the source code filename or Ctrl-Tab back to that screen.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Jul 2009 03:20:30 GMT</pubDate>
    <dc:creator>donw</dc:creator>
    <dc:date>2009-07-28T03:20:30Z</dc:date>
    <item>
      <title>Code Warrior code window - JM60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Code-Warrior-code-window-JM60/m-p/198562#M16083</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;when I use CW to assemble code (assembler code only) using the 'Make' or 'Debug'&lt;/P&gt;&lt;P&gt;buttons, when complete it shows the message 'project all up to date' at the top of&lt;/P&gt;&lt;P&gt;the source code window &amp;amp; hides the source code.&lt;/P&gt;&lt;P&gt;This is a bother, since I then have to click on the .asm file name&lt;/P&gt;&lt;P&gt;to make the source code reappear.&lt;/P&gt;&lt;P&gt;Is there some way to keep the source code visible?&lt;/P&gt;&lt;DIV class="message-edit-history"&gt;&lt;SPAN class="edit-author"&gt;Message Edited by NLFSJ on&lt;/SPAN&gt; &lt;SPAN class="local-date"&gt;2009-08-18&lt;/SPAN&gt; &lt;SPAN class="local-time"&gt;10:01 AM&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV class="message-edit-history"&gt; &lt;/DIV&gt;&lt;DIV class="message-edit-history"&gt;&lt;SPAN class="local-time"&gt;Added p/n to subject.&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV class="message-edit-history"&gt;&lt;SPAN class="edit-author"&gt;Message Edited by NLFSJ on&lt;/SPAN&gt; &lt;SPAN class="local-date"&gt;2009-08-18&lt;/SPAN&gt; &lt;SPAN class="local-time"&gt;10:01 AM&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Jul 2009 06:40:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Code-Warrior-code-window-JM60/m-p/198562#M16083</guid>
      <dc:creator>donw</dc:creator>
      <dc:date>2009-07-13T06:40:56Z</dc:date>
    </item>
    <item>
      <title>Re: Code Warrior code window</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Code-Warrior-code-window-JM60/m-p/198563#M16084</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;FONT color="#999999"&gt;Hello&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#999999"&gt;&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;- Which version of CodeWarrior are you using?&lt;BR /&gt;To retrieve that info:&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - Start CodeWarrior&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - Select Help -&amp;gt; About Freescale CodeWarrior&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - Click on "Install Products"&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - CodeWarrior version used is displayed on top in the Installed Products dialog.&lt;/P&gt;&lt;P&gt;&lt;FONT color="#999999"&gt;CrasyCat&lt;/FONT&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jul 2009 00:49:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Code-Warrior-code-window-JM60/m-p/198563#M16084</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2009-07-28T00:49:57Z</dc:date>
    </item>
    <item>
      <title>Re: Code Warrior code window</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Code-Warrior-code-window-JM60/m-p/198564#M16085</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;version is IDE 5.9.0 build 2404&lt;/P&gt;&lt;P&gt;The message appears in a window which overlays the code window, hence you have to click on the source code filename or Ctrl-Tab back to that screen.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jul 2009 03:20:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Code-Warrior-code-window-JM60/m-p/198564#M16085</guid>
      <dc:creator>donw</dc:creator>
      <dc:date>2009-07-28T03:20:30Z</dc:date>
    </item>
    <item>
      <title>Re: Code Warrior code window</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Code-Warrior-code-window-JM60/m-p/198565#M16086</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This does not help to identify the product you are using.&lt;/P&gt;&lt;P&gt;As stated in my last message, to retrieve that info:&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - Start CodeWarrior&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - Select Help -&amp;gt; About Freestyle CodeWarrior&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - Click on "Install Products"&lt;BR /&gt;&amp;nbsp;&amp;nbsp; - CodeWarrior version used is displayed on top in the Installed Products dialog.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Did you maximize the source window inside of CodeWarrior?&lt;/P&gt;&lt;P&gt;Is the issue reproducible if you restore source window to its original size?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 08 Aug 2009 15:24:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Code-Warrior-code-window-JM60/m-p/198565#M16086</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2009-08-08T15:24:00Z</dc:date>
    </item>
    <item>
      <title>Re: Code Warrior code window</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Code-Warrior-code-window-JM60/m-p/198566#M16087</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;CW dev studiov6.1 build 7285 -20 oct 07&lt;/P&gt;&lt;P&gt;JM60 service pack build 071128&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have maximised the code window . (And why is it not max'ed on startup!?)&lt;/P&gt;&lt;P&gt;I think this window action is normal, but it is annoying since after a build you have to Cntl-Tab back to the code window. (even though the result window only&amp;nbsp; takes up the top part of the screen)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-If I install a newer version&amp;nbsp; of CW do I have to reinstall the JM60 service pack?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 09 Aug 2009 04:41:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Code-Warrior-code-window-JM60/m-p/198566#M16087</guid>
      <dc:creator>donw</dc:creator>
      <dc:date>2009-08-09T04:41:37Z</dc:date>
    </item>
    <item>
      <title>Re: Code Warrior code window</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Code-Warrior-code-window-JM60/m-p/198567#M16088</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Maximizing the code window will maximize all the windows opened in CodeWarrior.&lt;/P&gt;&lt;P&gt;I would recommend you to remove the maximized and just change size of the window and make it bigger.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Aug 2009 16:38:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Code-Warrior-code-window-JM60/m-p/198567#M16088</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2009-08-18T16:38:59Z</dc:date>
    </item>
  </channel>
</rss>