<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MCU with display driver in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MCU-with-display-driver/m-p/198065#M15978</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Since the display device you have chosen appears to have been designed to simplify the interface between the display and a MCU, I would doubt the neccessity for an additional intervening processor.&amp;nbsp; You would still require a communications interface between the 12XEP100 and the display processor, so nothing to gain here.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So it will depend on the amount of data to be sent to the display processor, versus the amount of data required by the display itself.&amp;nbsp; There would need to be a&amp;nbsp;massive disparity to justify an additional processor.&amp;nbsp; Maybe if your application required high resolution graphics with rapid animation.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 08 May 2010 20:02:07 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2010-05-08T20:02:07Z</dc:date>
    <item>
      <title>MCU with display driver</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MCU-with-display-driver/m-p/198062#M15975</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;I have a display like this one (&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.lextronic.fr%2FP1614-afficheur-tactile-couleur-320-x-240-dpp-ctp3224.html" rel="nofollow" target="_blank"&gt;http://www.lextronic.fr/P1614-afficheur-tactile-couleur-320-x-240-dpp-ctp3224.html&lt;/A&gt;) and I would like to know if there is a 8bits MCU with a driver to control it.&lt;/P&gt;&lt;P&gt;Thank you in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 May 2010 22:14:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MCU-with-display-driver/m-p/198062#M15975</guid>
      <dc:creator>hasaur</dc:creator>
      <dc:date>2010-05-06T22:14:21Z</dc:date>
    </item>
    <item>
      <title>Re: MCU with display driver</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MCU-with-display-driver/m-p/198063#M15976</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It would appear that the display device has several interface options available, including serial port (SCI), IIC (often known as&amp;nbsp;I2C), and SPI (slave?).&amp;nbsp; Most Freescale MCUs incorporate the hardware for one or more of these communication methods.&amp;nbsp; Many devices will&amp;nbsp;incorporate all three peripheral modules.&amp;nbsp; SPI is likely to provide the fastest communications.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;A further USB option for the display is really intended for PC usage, rather than&amp;nbsp;for a&amp;nbsp;MCU application.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 May 2010 23:27:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MCU-with-display-driver/m-p/198063#M15976</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2010-05-06T23:27:48Z</dc:date>
    </item>
    <item>
      <title>Re: MCU with display driver</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MCU-with-display-driver/m-p/198064#M15977</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you very much.&lt;/P&gt;&lt;P&gt;I have a 16bit MCU (MC9S12XEP100) that already has much work to do&amp;nbsp;and I would like to know if I can drive the display with it or if it will become slow (and I'd rather use a 8bit MCU in addition, specially for the display). And if it's better to use a 8bit, which one would be a good choice (because there is too many 8-bits that incorporate SPI module)&amp;nbsp;?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your help.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 May 2010 14:34:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MCU-with-display-driver/m-p/198064#M15977</guid>
      <dc:creator>hasaur</dc:creator>
      <dc:date>2010-05-07T14:34:28Z</dc:date>
    </item>
    <item>
      <title>Re: MCU with display driver</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MCU-with-display-driver/m-p/198065#M15978</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Since the display device you have chosen appears to have been designed to simplify the interface between the display and a MCU, I would doubt the neccessity for an additional intervening processor.&amp;nbsp; You would still require a communications interface between the 12XEP100 and the display processor, so nothing to gain here.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So it will depend on the amount of data to be sent to the display processor, versus the amount of data required by the display itself.&amp;nbsp; There would need to be a&amp;nbsp;massive disparity to justify an additional processor.&amp;nbsp; Maybe if your application required high resolution graphics with rapid animation.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 08 May 2010 20:02:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MCU-with-display-driver/m-p/198065#M15978</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2010-05-08T20:02:07Z</dc:date>
    </item>
  </channel>
</rss>