<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: HC08 and HCS08 in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HC08-and-HCS08/m-p/197824#M15948</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Also from a developer's standpoint, HCS08's BDM interface can be a real pain compared to the HC08's MMDS emulator.&amp;nbsp; As stated, the HCS08 is still superior.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 08 May 2010 01:29:00 GMT</pubDate>
    <dc:creator>rocco</dc:creator>
    <dc:date>2010-05-08T01:29:00Z</dc:date>
    <item>
      <title>HC08 and HCS08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HC08-and-HCS08/m-p/197821#M15945</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What is the difference between HC08 and HCS08 families?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 May 2010 14:31:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HC08-and-HCS08/m-p/197821#M15945</guid>
      <dc:creator>TMirnik</dc:creator>
      <dc:date>2010-05-05T14:31:00Z</dc:date>
    </item>
    <item>
      <title>Re: HC08 and HCS08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HC08-and-HCS08/m-p/197822#M15946</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello and welcome to the fora.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Simply put HCS08 (or S08) is a later updated version of the HC08.&lt;/P&gt;&lt;P&gt;Here is an &lt;A href="http://www.freescale.com/webapp/search/Serp.jsp?QueryText=an2717&amp;amp;&amp;amp;attempt=-1" rel="nofollow" target="_self" title="AN2717"&gt;application note&lt;/A&gt; about it.&lt;/P&gt;&lt;P&gt;If you know little about either I would suggest you simply forget HC08 ever existed and just look at the S08.&lt;/P&gt;&lt;P&gt;S08 is always better, cheaper and most of the HC08's are dying off.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 May 2010 17:53:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HC08-and-HCS08/m-p/197822#M15946</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2010-05-05T17:53:58Z</dc:date>
    </item>
    <item>
      <title>Re: HC08 and HCS08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HC08-and-HCS08/m-p/197823#M15947</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;From a developer's standpoint, HC08's MON08 interface can be a real pain compared to the HCS08's BDM interface.&amp;nbsp; As stated, HCS08 is far superior.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 May 2010 08:50:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HC08-and-HCS08/m-p/197823#M15947</guid>
      <dc:creator>Klined</dc:creator>
      <dc:date>2010-05-07T08:50:49Z</dc:date>
    </item>
    <item>
      <title>Re: HC08 and HCS08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HC08-and-HCS08/m-p/197824#M15948</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Also from a developer's standpoint, HCS08's BDM interface can be a real pain compared to the HC08's MMDS emulator.&amp;nbsp; As stated, the HCS08 is still superior.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 08 May 2010 01:29:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HC08-and-HCS08/m-p/197824#M15948</guid>
      <dc:creator>rocco</dc:creator>
      <dc:date>2010-05-08T01:29:00Z</dc:date>
    </item>
  </channel>
</rss>