<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Re: MC9S08DN32</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08DN32/m-p/197438#M15878</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you very much!I&lt;SPAN class="short_text"&gt;&lt;SPAN&gt;think I am understand.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 07 May 2010 07:52:57 GMT</pubDate>
    <dc:creator>lyong</dc:creator>
    <dc:date>2010-05-07T07:52:57Z</dc:date>
    <item>
      <title>MC9S08DN32</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08DN32/m-p/197436#M15876</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hello everybody, I have two problems on MC9S08DN32 would like to consult. 1. when the MC9S08DN32 using the internal reference clock, how much the highest multiplication frequency? 2. Internal reference clock with temperature (assuming no change in voltage). Best to have a temperature tolerance 。 Thanks!&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 May 2010 20:30:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08DN32/m-p/197436#M15876</guid>
      <dc:creator>lyong</dc:creator>
      <dc:date>2010-05-04T20:30:29Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08DN32</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08DN32/m-p/197437#M15877</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, and welcome to the forum.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Assuming you are using FEI mode, the DCO frequency will be 1024 times the reference frequency.&amp;nbsp; This frequency is then divided by the BDIV factor, and a further divide by 2, to give the bus frequency.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;After POR the default BDIV factor will be 2, so that the bus frequency would be 256 times the reference frequency, i.e. a bus frequency between the limits 8 MHz to10 MHz after the internal reference has been trimmed to the required frequency.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The frequency tolerance for the internal reference, over the temperature range 0C to 70C is given in the datasheet (Appendix A).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 May 2010 09:09:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08DN32/m-p/197437#M15877</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2010-05-05T09:09:42Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08DN32</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08DN32/m-p/197438#M15878</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you very much!I&lt;SPAN class="short_text"&gt;&lt;SPAN&gt;think I am understand.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 May 2010 07:52:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08DN32/m-p/197438#M15878</guid>
      <dc:creator>lyong</dc:creator>
      <dc:date>2010-05-07T07:52:57Z</dc:date>
    </item>
  </channel>
</rss>