<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: DEMO09S08DZ60</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/DEMO09S08DZ60/m-p/197115#M15838</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hii&lt;BR /&gt;so what you are telling me is that i have to connect voltage to vdd, vss vrfh and vrefl if i have the 64 pin? and vdd can be any voltage and vrefh must be lower than vdd??&lt;BR /&gt;another little question...do you know how do i use the buttons and leds and pots that are in the board? im not quite sure how to access them. thanks a lot&lt;BR /&gt;lau&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 27 Oct 2008 05:15:05 GMT</pubDate>
    <dc:creator>laura</dc:creator>
    <dc:date>2008-10-27T05:15:05Z</dc:date>
    <item>
      <title>DEMO09S08DZ60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/DEMO09S08DZ60/m-p/197113#M15836</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hi&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;My name is Laura and I'm having trouble understanding something on the datasheet of my microcontroller. I solved some doubts already but I cannto understand the voltage in the ADC. What pins do I use to specify the range of the voltage to compare or is it fixed? Hope you can help me because this is my first time programming &lt;/SPAN&gt;&lt;A href="http://freescale.i.lithium.com/i/smilies/16x16_smiley-frustrated.gif"&gt;&lt;IMG alt=":smileyfrustrated:" class="emoticon emoticon-smileyfrustrated" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-frustrated.gif" title="Smiley Frustrated" /&gt;&lt;/A&gt;&lt;SPAN&gt;, bye!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Oct 2008 07:06:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/DEMO09S08DZ60/m-p/197113#M15836</guid>
      <dc:creator>laura</dc:creator>
      <dc:date>2008-10-24T07:06:11Z</dc:date>
    </item>
    <item>
      <title>Re: DEMO09S08DZ60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/DEMO09S08DZ60/m-p/197114#M15837</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;Hello Laura,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;For the DZ60 device, external Vref connections are available for the 64-pin package only.&amp;nbsp; For the smaller packages the connections are internally tied to VddA and VssA, which require to be externally wired to Vdd and Vss, respectively.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;For the 64-pin package, the VrefL&amp;nbsp;pin needs to be at the same potential as VssA.&amp;nbsp; However, the VrefH pin may have an applied voltage between the limits 2.7 volts and VddA.&amp;nbsp; The reference voltage must not exceed VddA.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;However, I do not know whether&amp;nbsp;the demo board configuration makes provision for an externally applied reference voltage.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Mac&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;Message Edited by bigmac on &lt;SPAN class="date_text"&gt;2008-10-24&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;11:24 AM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Oct 2008 08:19:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/DEMO09S08DZ60/m-p/197114#M15837</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2008-10-24T08:19:31Z</dc:date>
    </item>
    <item>
      <title>Re: DEMO09S08DZ60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/DEMO09S08DZ60/m-p/197115#M15838</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hii&lt;BR /&gt;so what you are telling me is that i have to connect voltage to vdd, vss vrfh and vrefl if i have the 64 pin? and vdd can be any voltage and vrefh must be lower than vdd??&lt;BR /&gt;another little question...do you know how do i use the buttons and leds and pots that are in the board? im not quite sure how to access them. thanks a lot&lt;BR /&gt;lau&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Oct 2008 05:15:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/DEMO09S08DZ60/m-p/197115#M15838</guid>
      <dc:creator>laura</dc:creator>
      <dc:date>2008-10-27T05:15:05Z</dc:date>
    </item>
    <item>
      <title>Re: DEMO09S08DZ60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/DEMO09S08DZ60/m-p/197116#M15839</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello Laura,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Since you are using the demo board, the various power supply connections have already been made - you do not need to make any external connections to the chip.&amp;nbsp; Note that the ADC reference voltage is already connected to Vdd (refer to the board schematic).&amp;nbsp; For&amp;nbsp;a different&amp;nbsp;externally applied voltage level, this would required some modifications to the board.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;To utilize the various buttons, LEDs and potentiometers, you will need to&amp;nbsp;install "fabricated jumpers" at the appropriate locations on the USER dual row header strip.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Mac&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Oct 2008 19:03:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/DEMO09S08DZ60/m-p/197116#M15839</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2008-10-29T19:03:41Z</dc:date>
    </item>
  </channel>
</rss>