<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックPWM with device initialization</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/PWM-with-device-initialization/m-p/196834#M15778</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi im using a MC9s08QE32&lt;/P&gt;&lt;P&gt;I want to have a constant pwm&lt;/P&gt;&lt;P&gt;So in device initialization I set the right timer and channel for the pin im using&lt;/P&gt;&lt;P&gt;Set it to edge aligned&lt;/P&gt;&lt;P&gt;Set modulo to 99 and compare value to 50 for now&lt;/P&gt;&lt;P&gt;and set output on compare&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;but the thing doesnt seem to work&lt;/P&gt;&lt;P&gt;I must use ovf interruption to clear the pin??&lt;/P&gt;&lt;P&gt;and another thing is how do i increase or decrease the pwm&lt;/P&gt;&lt;P&gt;simply writing c0vl and c0vh at any moment?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 30 Apr 2010 17:46:06 GMT</pubDate>
    <dc:creator>Juls</dc:creator>
    <dc:date>2010-04-30T17:46:06Z</dc:date>
    <item>
      <title>PWM with device initialization</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/PWM-with-device-initialization/m-p/196834#M15778</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi im using a MC9s08QE32&lt;/P&gt;&lt;P&gt;I want to have a constant pwm&lt;/P&gt;&lt;P&gt;So in device initialization I set the right timer and channel for the pin im using&lt;/P&gt;&lt;P&gt;Set it to edge aligned&lt;/P&gt;&lt;P&gt;Set modulo to 99 and compare value to 50 for now&lt;/P&gt;&lt;P&gt;and set output on compare&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;but the thing doesnt seem to work&lt;/P&gt;&lt;P&gt;I must use ovf interruption to clear the pin??&lt;/P&gt;&lt;P&gt;and another thing is how do i increase or decrease the pwm&lt;/P&gt;&lt;P&gt;simply writing c0vl and c0vh at any moment?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Apr 2010 17:46:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/PWM-with-device-initialization/m-p/196834#M15778</guid>
      <dc:creator>Juls</dc:creator>
      <dc:date>2010-04-30T17:46:06Z</dc:date>
    </item>
    <item>
      <title>Re: PWM with device initialization</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/PWM-with-device-initialization/m-p/196835#M15779</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;settings on attached screenshot should help you to solve your problem.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;best regards&lt;BR /&gt;Vojtech Filip&lt;BR /&gt;Processor Expert Support Team&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 May 2010 21:04:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/PWM-with-device-initialization/m-p/196835#M15779</guid>
      <dc:creator>ProcessorExpert</dc:creator>
      <dc:date>2010-05-06T21:04:39Z</dc:date>
    </item>
  </channel>
</rss>