<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S08QE8 with External Oscillator in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/S08QE8-with-External-Oscillator/m-p/196698#M15754</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BLOCKQUOTE&gt;&lt;HR /&gt;bigmac wrote:&lt;BR /&gt;&lt;BR /&gt;&lt;P&gt;An additional consideration may be, that if ICSC2_EREFS bit is set to zero, the XTAL pin should be available as GPIO.&lt;/P&gt;&lt;HR /&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Good point. You do not need to "leave it hanging". You can do something useful with it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Jan 2012 08:21:02 GMT</pubDate>
    <dc:creator>rocco</dc:creator>
    <dc:date>2012-01-11T08:21:02Z</dc:date>
    <item>
      <title>S08QE8 with External Oscillator</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/S08QE8-with-External-Oscillator/m-p/196695#M15751</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am designing with the 16 pin S08QE8 and plan to use an external oscillator (not a crystal or resonator). &amp;nbsp;Do I drive the EXTAL pin with the oscillator output and leave the XTAL pin hanging or is there another setup that should be used?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you very much for your time&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Jan 2012 00:03:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/S08QE8-with-External-Oscillator/m-p/196695#M15751</guid>
      <dc:creator>MatthewScott_DE</dc:creator>
      <dc:date>2012-01-11T00:03:42Z</dc:date>
    </item>
    <item>
      <title>Re: S08QE8 with External Oscillator</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/S08QE8-with-External-Oscillator/m-p/196696#M15752</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Matthew Scott,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Welcome to the forum.&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;HR /&gt;Do I drive the EXTAL pin with the oscillator output and leave the XTAL pin hanging?&lt;HR /&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Yes.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Jan 2012 04:27:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/S08QE8-with-External-Oscillator/m-p/196696#M15752</guid>
      <dc:creator>rocco</dc:creator>
      <dc:date>2012-01-11T04:27:04Z</dc:date>
    </item>
    <item>
      <title>Re: S08QE8 with External Oscillator</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/S08QE8-with-External-Oscillator/m-p/196697#M15753</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;An additional consideration may be, that if ICSC2_EREFS bit is set to zero, the XTAL pin should be available as GPIO.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Jan 2012 08:03:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/S08QE8-with-External-Oscillator/m-p/196697#M15753</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2012-01-11T08:03:04Z</dc:date>
    </item>
    <item>
      <title>Re: S08QE8 with External Oscillator</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/S08QE8-with-External-Oscillator/m-p/196698#M15754</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BLOCKQUOTE&gt;&lt;HR /&gt;bigmac wrote:&lt;BR /&gt;&lt;BR /&gt;&lt;P&gt;An additional consideration may be, that if ICSC2_EREFS bit is set to zero, the XTAL pin should be available as GPIO.&lt;/P&gt;&lt;HR /&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Good point. You do not need to "leave it hanging". You can do something useful with it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Jan 2012 08:21:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/S08QE8-with-External-Oscillator/m-p/196698#M15754</guid>
      <dc:creator>rocco</dc:creator>
      <dc:date>2012-01-11T08:21:02Z</dc:date>
    </item>
    <item>
      <title>Re: S08QE8 with External Oscillator</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/S08QE8-with-External-Oscillator/m-p/196699#M15755</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you both very much&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Jan 2012 23:49:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/S08QE8-with-External-Oscillator/m-p/196699#M15755</guid>
      <dc:creator>MatthewScott_DE</dc:creator>
      <dc:date>2012-01-13T23:49:11Z</dc:date>
    </item>
  </channel>
</rss>