<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: flash card and SPI</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/flash-card-and-SPI/m-p/196220#M15689</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 01 May 2010 15:42:59 GMT</pubDate>
    <dc:creator>xavier12358</dc:creator>
    <dc:date>2010-05-01T15:42:59Z</dc:date>
    <item>
      <title>flash card and SPI</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/flash-card-and-SPI/m-p/196218#M15687</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;I program a MC9S08DZ60 in order to read informations&amp;nbsp;from&amp;nbsp; SD card. I send it&amp;nbsp;CMD0 and CMD1 commands to reset and init it, the card answers proprely. But for example when I send it a CMD17 command in order to read a single block, first the answer is correct 0x00 and then the card send me the data. But the probleme is that the&amp;nbsp;start block is 0xfc whereas it should be 0xfe and then there is the data from the card. I don't know if the probleme could come from the class of my SD card?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can someone who has already work on a SD card help me?&lt;/P&gt;&lt;P&gt;Thank you in advance.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Apr 2010 14:30:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/flash-card-and-SPI/m-p/196218#M15687</guid>
      <dc:creator>xavier12358</dc:creator>
      <dc:date>2010-04-28T14:30:35Z</dc:date>
    </item>
    <item>
      <title>Re: flash card and SPI</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/flash-card-and-SPI/m-p/196219#M15688</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Try looking here:&lt;/P&gt;&lt;P&gt;&lt;A href="http://elm-chan.org/docs/mmc/mmc_e.html" rel="nofollow" target="_self"&gt;http://elm-chan.org/docs/mmc/mmc_e.html&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Apr 2010 23:37:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/flash-card-and-SPI/m-p/196219#M15688</guid>
      <dc:creator>ballen</dc:creator>
      <dc:date>2010-04-29T23:37:24Z</dc:date>
    </item>
    <item>
      <title>Re: flash card and SPI</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/flash-card-and-SPI/m-p/196220#M15689</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 01 May 2010 15:42:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/flash-card-and-SPI/m-p/196220#M15689</guid>
      <dc:creator>xavier12358</dc:creator>
      <dc:date>2010-05-01T15:42:59Z</dc:date>
    </item>
  </channel>
</rss>