<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollersのトピックuse DEMO9S08AW60 as poor man's P&amp;E device programmer</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/use-DEMO9S08AW60-as-poor-man-s-P-E-device-programmer/m-p/196168#M15681</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Title explains it all.&amp;nbsp; But I have a strange observation.&amp;nbsp; With my DEMO9S08&lt;SPAN style="text-decoration: underline;"&gt;&lt;STRONG&gt;QG8&lt;/STRONG&gt;&lt;/SPAN&gt; board, I can successfully use its BDM header to program other QG8 device target boards.&amp;nbsp; Of course, I have removed the DEMO board's QG8 MCU first.&amp;nbsp; I'm using the P&amp;amp;E programming software, PROGHCS08 Programmer v1.37.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Repeat the same steps with my DEMO9S08AW60 board, remove it's AW60 MCU, BDM header J32 out to my target QG8 board, but I get no sync.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've read elsewhere about the voltage on the BDM header's pin 6.&amp;nbsp; On the DEMO9S08QG8, pin 6 is open circuit.&amp;nbsp; On the DEMO9S08AW60, pin 6 is connected to VDD, which is selectable on W2 for 5V or 3V.&amp;nbsp; Leaving that jumper off completely, I measure 0.9V (a diode drop I presume)&lt;STRONG&gt;&amp;nbsp;&lt;/STRONG&gt;.&amp;nbsp; But even that doesn't allow me to communicate with a QG8 target board.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Feels like I'm missing something really obvious.&amp;nbsp; Any ideas?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 Apr 2010 05:13:01 GMT</pubDate>
    <dc:creator>irob</dc:creator>
    <dc:date>2010-04-28T05:13:01Z</dc:date>
    <item>
      <title>use DEMO9S08AW60 as poor man's P&amp;E device programmer</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/use-DEMO9S08AW60-as-poor-man-s-P-E-device-programmer/m-p/196168#M15681</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Title explains it all.&amp;nbsp; But I have a strange observation.&amp;nbsp; With my DEMO9S08&lt;SPAN style="text-decoration: underline;"&gt;&lt;STRONG&gt;QG8&lt;/STRONG&gt;&lt;/SPAN&gt; board, I can successfully use its BDM header to program other QG8 device target boards.&amp;nbsp; Of course, I have removed the DEMO board's QG8 MCU first.&amp;nbsp; I'm using the P&amp;amp;E programming software, PROGHCS08 Programmer v1.37.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Repeat the same steps with my DEMO9S08AW60 board, remove it's AW60 MCU, BDM header J32 out to my target QG8 board, but I get no sync.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've read elsewhere about the voltage on the BDM header's pin 6.&amp;nbsp; On the DEMO9S08QG8, pin 6 is open circuit.&amp;nbsp; On the DEMO9S08AW60, pin 6 is connected to VDD, which is selectable on W2 for 5V or 3V.&amp;nbsp; Leaving that jumper off completely, I measure 0.9V (a diode drop I presume)&lt;STRONG&gt;&amp;nbsp;&lt;/STRONG&gt;.&amp;nbsp; But even that doesn't allow me to communicate with a QG8 target board.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Feels like I'm missing something really obvious.&amp;nbsp; Any ideas?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Apr 2010 05:13:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/use-DEMO9S08AW60-as-poor-man-s-P-E-device-programmer/m-p/196168#M15681</guid>
      <dc:creator>irob</dc:creator>
      <dc:date>2010-04-28T05:13:01Z</dc:date>
    </item>
    <item>
      <title>Re: use DEMO9S08AW60 as poor man's P&amp;E device programmer</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/use-DEMO9S08AW60-as-poor-man-s-P-E-device-programmer/m-p/196169#M15682</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Nevermind, everyone.&amp;nbsp; Peg turned me onto &lt;A href="https://community.freescale.com/message/49272#49272" title="https://community.freescale.com/message/49272#49272"&gt;https://community.freescale.com/message/49272#49272&lt;/A&gt; to hack some DLLs.&amp;nbsp; The DEMO9S08AW60 now functions as a multi-device BDM programmer under a CW 6.3 installation with these downgraded DLLs.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Apr 2010 05:51:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/use-DEMO9S08AW60-as-poor-man-s-P-E-device-programmer/m-p/196169#M15682</guid>
      <dc:creator>irob</dc:creator>
      <dc:date>2010-04-28T05:51:54Z</dc:date>
    </item>
  </channel>
</rss>