<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Re: How to Add the protection to internal Flash ??</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-Add-the-protection-to-internal-Flash/m-p/196119#M15676</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Harlen,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What you want can be achieved by using Flash block protection.&lt;/P&gt;&lt;P&gt;See section 4.4.6 of the manual. Maybe look at the GT16A manual for a better description.&lt;/P&gt;&lt;P&gt;You just programme NVPROT with the appropriate value and that's it. ($BE)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This only provides protection from internal access.&lt;/P&gt;&lt;P&gt;When you connect via a BDM adapter the software will un-protect the flash so it may be then modified.&lt;/P&gt;&lt;P&gt;Note that this un-protecting can only be done through the BDM.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If still not clear on this perhaps you can narrow down your area of concern.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 03 Jul 2009 10:20:35 GMT</pubDate>
    <dc:creator>peg</dc:creator>
    <dc:date>2009-07-03T10:20:35Z</dc:date>
    <item>
      <title>How to Add the protection to internal Flash ??</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-Add-the-protection-to-internal-Flash/m-p/196117#M15674</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We use the MC908GT16 for 3 years. Currently, we find the internal flash to be changed. The program can not run correctly. Originally, we dont add the protection to the internal Flash. We want to know:&lt;/P&gt;&lt;P&gt;1. How to add protection to the entire Flash?&lt;/P&gt;&lt;P&gt;2. If protection , We can read the program of Flash? How to read?&lt;/P&gt;&lt;P&gt;3. If protection, the Flash can be re-program ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;harlen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Jul 2009 08:31:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-Add-the-protection-to-internal-Flash/m-p/196117#M15674</guid>
      <dc:creator>Harlen_CHen</dc:creator>
      <dc:date>2009-07-03T08:31:41Z</dc:date>
    </item>
    <item>
      <title>Re: How to Add the protection to internal Flash ??</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-Add-the-protection-to-internal-Flash/m-p/196118#M15675</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I've read your post but can't understand it completely....can you be more specific?&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Jul 2009 09:36:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-Add-the-protection-to-internal-Flash/m-p/196118#M15675</guid>
      <dc:creator>OmarAI</dc:creator>
      <dc:date>2009-07-03T09:36:42Z</dc:date>
    </item>
    <item>
      <title>Re: How to Add the protection to internal Flash ??</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-Add-the-protection-to-internal-Flash/m-p/196119#M15676</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Harlen,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What you want can be achieved by using Flash block protection.&lt;/P&gt;&lt;P&gt;See section 4.4.6 of the manual. Maybe look at the GT16A manual for a better description.&lt;/P&gt;&lt;P&gt;You just programme NVPROT with the appropriate value and that's it. ($BE)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This only provides protection from internal access.&lt;/P&gt;&lt;P&gt;When you connect via a BDM adapter the software will un-protect the flash so it may be then modified.&lt;/P&gt;&lt;P&gt;Note that this un-protecting can only be done through the BDM.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If still not clear on this perhaps you can narrow down your area of concern.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Jul 2009 10:20:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-Add-the-protection-to-internal-Flash/m-p/196119#M15676</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2009-07-03T10:20:35Z</dc:date>
    </item>
  </channel>
</rss>