<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: SMAC in MC9S08QG8</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/SMAC-in-MC9S08QG8/m-p/195660#M15633</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;You can actually implement SMAC in devices as small as a QG4. No bells and whistles here though.&lt;BR /&gt;See this &lt;A href="http://www.freescale.com/files/microcontrollers/doc/brochure/8BITZIGBEEFS.pdf?fsrch=1" rel="nofollow" target="_blank"&gt;document&lt;/A&gt;. This was prior to beekit.&lt;BR /&gt;I suspect that the automation inherent in beekit may have introduced inefficiencies that may now preclude the QG, but you can definitely do it the old way with just SMAC. (sans B&amp;amp;W)&lt;BR /&gt;As far as the connections go, they would be pretty much the same (the same named pins MISO, MOSI etc)&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;Message Edited by peg on &lt;SPAN class="date_text"&gt;2008-10-21&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;06:39 PM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 Oct 2008 15:33:05 GMT</pubDate>
    <dc:creator>peg</dc:creator>
    <dc:date>2008-10-21T15:33:05Z</dc:date>
    <item>
      <title>SMAC in MC9S08QG8</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/SMAC-in-MC9S08QG8/m-p/195658#M15631</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;What I have to do to use SMAC with a MC9S08QG8? (if the supported MCU in BeeKit are MC68HCS08GT60, MC68HCS08GB60 and MC9S08QE128)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;What pins I have to connect between the MC9S08QG8 and the MC13192?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks!&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Oct 2008 06:25:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/SMAC-in-MC9S08QG8/m-p/195658#M15631</guid>
      <dc:creator>facundomaldonad</dc:creator>
      <dc:date>2008-10-21T06:25:06Z</dc:date>
    </item>
    <item>
      <title>Re: SMAC in MC9S08QG8</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/SMAC-in-MC9S08QG8/m-p/195659#M15632</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;Hello, and welcome to the forum.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;What flash and RAM resources are required to support SMAC?&amp;nbsp; I&amp;nbsp;suspect that the 'QG8 would be too small.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Mac&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;Message Edited by bigmac on &lt;SPAN class="date_text"&gt;2008-10-21&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;09:39 AM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Oct 2008 06:38:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/SMAC-in-MC9S08QG8/m-p/195659#M15632</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2008-10-21T06:38:42Z</dc:date>
    </item>
    <item>
      <title>Re: SMAC in MC9S08QG8</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/SMAC-in-MC9S08QG8/m-p/195660#M15633</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;You can actually implement SMAC in devices as small as a QG4. No bells and whistles here though.&lt;BR /&gt;See this &lt;A href="http://www.freescale.com/files/microcontrollers/doc/brochure/8BITZIGBEEFS.pdf?fsrch=1" rel="nofollow" target="_blank"&gt;document&lt;/A&gt;. This was prior to beekit.&lt;BR /&gt;I suspect that the automation inherent in beekit may have introduced inefficiencies that may now preclude the QG, but you can definitely do it the old way with just SMAC. (sans B&amp;amp;W)&lt;BR /&gt;As far as the connections go, they would be pretty much the same (the same named pins MISO, MOSI etc)&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;Message Edited by peg on &lt;SPAN class="date_text"&gt;2008-10-21&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;06:39 PM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Oct 2008 15:33:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/SMAC-in-MC9S08QG8/m-p/195660#M15633</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2008-10-21T15:33:05Z</dc:date>
    </item>
    <item>
      <title>Re: SMAC in MC9S08QG8</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/SMAC-in-MC9S08QG8/m-p/195661#M15634</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;me also new in hcs08's, SO if anything incorrect then plz others correct that.&lt;BR /&gt;&lt;BR /&gt;Peg is very correct.&lt;BR /&gt;&lt;BR /&gt;ram and flash resources.for MC9S08QG8 are 512 bytes and 8K .&lt;BR /&gt;and required for smac are 2.5K-3K. so that can be implemented.&lt;BR /&gt;connections are throughfour wire SPI connections,as&lt;BR /&gt;&lt;BR /&gt;MODEM MCU&lt;BR /&gt;&lt;BR /&gt;MOSI-----MOSI&lt;BR /&gt;MISO-----&amp;gt;MISO&lt;BR /&gt;M_IRQ----&amp;gt;IRQ&lt;BR /&gt;SPICLK---SPICLK&lt;BR /&gt;&lt;BR /&gt;REGARDS..&lt;BR /&gt;KARAN.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Oct 2008 05:04:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/SMAC-in-MC9S08QG8/m-p/195661#M15634</guid>
      <dc:creator>kanu</dc:creator>
      <dc:date>2008-10-22T05:04:22Z</dc:date>
    </item>
  </channel>
</rss>