<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Using BDM-Interface from DEMO9RS08KASP for Programming HCS08-Devices? in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-Interface-from-DEMO9RS08KASP-for-Programming-HCS08/m-p/195545#M15621</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello Prometeus,&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;BR /&gt;&lt;BLOCKQUOTE&gt;&lt;DIV&gt;&lt;HR /&gt;prometeus wrote:&lt;BR /&gt;...&amp;nbsp;the 'S08 MCUs don't use a programming voltage of 12V, so the Reset pin of the BDM connector is just used for reseting the MCU? So maybe I can use a transistor or a Z-diode+resistor to take down the voltage to 5V during reseting while programming. What do you think?&lt;BR /&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;/DIV&gt;&lt;/BLOCKQUOTE&gt;From the schematic, I see that there is provision made&amp;nbsp;for the selection of either Vpp or Vdd to be applied to the Reset pin, controlled&amp;nbsp;by the USB to BDM processor.&amp;nbsp; It is possible that you may not need to do anything except select the correct MCU type from within CW.&lt;BR /&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Mac&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 Feb 2008 01:35:49 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2008-02-28T01:35:49Z</dc:date>
    <item>
      <title>Using BDM-Interface from DEMO9RS08KASP for Programming HCS08-Devices?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-Interface-from-DEMO9RS08KASP-for-Programming-HCS08/m-p/195540#M15616</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a DEMO9RS08KASP Board and like to to programm some HCS08-devices (like 9S08QG8). May I use the USB2BDM-Interface from my DEMO9RS08KASP Board to do this? I don't try it yet because I don't have a HCS08-controller. Is there somebody who already tried such a thing? I guess it's just a question of software&amp;nbsp; - programmer software and (hopefully not) the firmware of the USB2BDM-Interface...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Best regards&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 24 Feb 2008 21:11:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-Interface-from-DEMO9RS08KASP-for-Programming-HCS08/m-p/195540#M15616</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2008-02-24T21:11:02Z</dc:date>
    </item>
    <item>
      <title>Re: Using BDM-Interface from DEMO9RS08KASP for Programming HCS08-Devices?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-Interface-from-DEMO9RS08KASP-for-Programming-HCS08/m-p/195541#M15617</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello and welcome to the forums prometeus,&lt;BR /&gt;&lt;BR /&gt;I'm not familiar with this exact demo board, but in the general case it is possible to use these demo boards as a standalone BDM to connect to another board. It is simply a matter of removing/disconnecting the device on the demo board and soldering a 6 pin cable/header in place.&lt;BR /&gt;&lt;BR /&gt;Hmm, after another look.... what I have said above I know works with P&amp;amp;E demoboards, it looks like this may be a softec product so I can't be as sure. I don't seem to be able to find your exact board but the two I did find are Softec.&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Feb 2008 13:37:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-Interface-from-DEMO9RS08KASP-for-Programming-HCS08/m-p/195541#M15617</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2008-02-25T13:37:21Z</dc:date>
    </item>
    <item>
      <title>Re: Using BDM-Interface from DEMO9RS08KASP for Programming HCS08-Devices?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-Interface-from-DEMO9RS08KASP-for-Programming-HCS08/m-p/195542#M15618</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Be careful.&amp;nbsp; The RS08 device requires an external programming voltage.&amp;nbsp; The standard 9S08 parts do not.&amp;nbsp; You wiould have to make sure that the programming voltage was disabled.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Mac&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Feb 2008 13:46:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-Interface-from-DEMO9RS08KASP-for-Programming-HCS08/m-p/195542#M15618</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2008-02-25T13:46:12Z</dc:date>
    </item>
    <item>
      <title>Re: Using BDM-Interface from DEMO9RS08KASP for Programming HCS08-Devices?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-Interface-from-DEMO9RS08KASP-for-Programming-HCS08/m-p/195543#M15619</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello again,&lt;BR /&gt;&lt;BR /&gt;@peg: Yes, it's from Softec. You can find it on freescale website: &lt;A href="http://forums.freescale.com/Freescale%20DEMO9RS08KASP" rel="nofollow" target="_blank"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=DEMO9RS08KA2&amp;amp;parentCode=MC9RS08KA2&amp;amp;nodeId=016246844994879931&amp;amp;tid=t8ft&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Users Manual: &lt;A href="http://" rel="nofollow" target="_blank"&gt;http://www.freescale.com/files/microcontrollers/doc/user_guide/DEMO9RS08KA2UM.pdf?fpsp=1&amp;amp;WT_TYPE=Users%20Guides&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&lt;/A&gt;&lt;BR /&gt;Schematics:&lt;BR /&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=DEMO9RS08KA2&amp;amp;nodeId=016246844994879931&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab#" rel="nofollow" target="_blank"&gt;http://www.freescale.com/files/microcontrollers/hardware_tools/schematics/DEMO9RS08KA2SCH.pdf?fpsp=1&amp;amp;WT_TYPE=Schematics&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Downloads&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;It already has a BDM connector, that's the&amp;nbsp; reason why I like to use it also to program 'S08 devices. The BDM connector settings are:&lt;BR /&gt;Pin1: BKGD&lt;BR /&gt;Pin2: GND&lt;BR /&gt;Pin3: N.C.&lt;BR /&gt;Pin4: Reset/VPP&lt;BR /&gt;Pin5: N.C.&lt;BR /&gt;Pin6: VDD&lt;BR /&gt;&lt;BR /&gt;I seems to be the same as for 'S08 MCUs, doesn't it? (Except the programming voltage...)&lt;BR /&gt;&lt;BR /&gt;So @bigmac, the 'S08 MCUs don't use a programming voltage of 12V, so the Reset pin of the BDM connector is just used for reseting the MCU? So maybe I can use a transistor or a Z-diode+resistor to take down the voltage to 5V during reseting while programming. What do you think?&lt;BR /&gt;&lt;BR /&gt;Actually my biggest fear is, that Code Warrior doesn't accept the DEMO9RS08KASP as 'S08 programmer...&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;prometeus&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Feb 2008 20:09:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-Interface-from-DEMO9RS08KASP-for-Programming-HCS08/m-p/195543#M15619</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2008-02-27T20:09:14Z</dc:date>
    </item>
    <item>
      <title>Re: Using BDM-Interface from DEMO9RS08KASP for Programming HCS08-Devices?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-Interface-from-DEMO9RS08KASP-for-Programming-HCS08/m-p/195544#M15620</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Sorry for the bad layout of my last post. I have to get used of message editor of this forum...&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Feb 2008 20:14:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-Interface-from-DEMO9RS08KASP-for-Programming-HCS08/m-p/195544#M15620</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2008-02-27T20:14:39Z</dc:date>
    </item>
    <item>
      <title>Re: Using BDM-Interface from DEMO9RS08KASP for Programming HCS08-Devices?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-Interface-from-DEMO9RS08KASP-for-Programming-HCS08/m-p/195545#M15621</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello Prometeus,&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;BR /&gt;&lt;BLOCKQUOTE&gt;&lt;DIV&gt;&lt;HR /&gt;prometeus wrote:&lt;BR /&gt;...&amp;nbsp;the 'S08 MCUs don't use a programming voltage of 12V, so the Reset pin of the BDM connector is just used for reseting the MCU? So maybe I can use a transistor or a Z-diode+resistor to take down the voltage to 5V during reseting while programming. What do you think?&lt;BR /&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;/DIV&gt;&lt;/BLOCKQUOTE&gt;From the schematic, I see that there is provision made&amp;nbsp;for the selection of either Vpp or Vdd to be applied to the Reset pin, controlled&amp;nbsp;by the USB to BDM processor.&amp;nbsp; It is possible that you may not need to do anything except select the correct MCU type from within CW.&lt;BR /&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Mac&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Feb 2008 01:35:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-Interface-from-DEMO9RS08KASP-for-Programming-HCS08/m-p/195545#M15621</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2008-02-28T01:35:49Z</dc:date>
    </item>
    <item>
      <title>Re: Using BDM-Interface from DEMO9RS08KASP for Programming HCS08-Devices?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-Interface-from-DEMO9RS08KASP-for-Programming-HCS08/m-p/195546#M15622</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello Prometeus,&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp; If you made this work (or not)&lt;BR /&gt;&amp;nbsp; are you going post a summary?&lt;BR /&gt;&lt;BR /&gt;--&lt;BR /&gt;thanks&lt;BR /&gt;&amp;nbsp; Peter&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 16 Mar 2008 00:54:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-BDM-Interface-from-DEMO9RS08KASP-for-Programming-HCS08/m-p/195546#M15622</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2008-03-16T00:54:50Z</dc:date>
    </item>
  </channel>
</rss>