<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: AN2295 (HC08/S08 Developer's Serial Bootloader) updated for rev. 9.2 - CF V1 (alpha) support add</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-HC08-S08-Developer-s-Serial-Bootloader-updated-for-rev-9/m-p/194121#M15290</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, i'm a newbie in this bootloader section i need some help to understand vector redirection without hw support.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a bootloader project developed MC9S08QE64 which doesn't have hw vector redirection and an application project, thisi is application prm:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;/* This is a linker parameter file for the mc9s08qe64 */NAMES END /* CodeWarrior will pass all the needed files to the linker by command line. But here you may add your own files too. */SEGMENTS /* Here all RAM/ROM areas of the device are listed. Used in PLACEMENT below. */    Z_RAM                    =  READ_WRITE   0x0080 TO 0x00FF;    RAM                      =  READ_WRITE   0x0100 TO 0x107F;    /* unbanked FLASH ROM */    ROM                      =  READ_ONLY    0x2080 TO 0x7FFF;    //ROM                      =  READ_ONLY    0x2090 TO 0x3FFF;    //ROM                      =  READ_ONLY    0x2080 TO 0x3FFF;  //ORIGINAL VALUE!!        ROM1                     =  READ_ONLY    0xC000 TO 0xFFAD; /* INTVECTS                 =  READ_ONLY    0xFFC0 TO 0xFFFF; Reserved for Interrupt Vectors */    /* banked FLASH ROM */    PPAGE_0                  =  READ_ONLY    0x008000 TO 0x00A08F; /* PAGE partially contained in ROM segment */    //PPAGE_0                  =  READ_ONLY    0x008000 TO 0x00A07F; //ORIGINAL VALUE!!/* PAGE partially contained in ROM segment */    PPAGE_2                  =  READ_ONLY    0x028000 TO 0x02BFFF;     //PPAGE_1                  =  READ_ONLY    0x018000 TO 0x01BFFF; //PAGE already contained in segment at 0x4000-0x7FFF */    //PPAGE_3                  =  READ_ONLY    0x038000 TO 0x03BFFF; //PAGE already contained in segment at 0xC000-0xFFFF */    //PPAGE_3                  =  READ_ONLY    0x038000 TO 0x03BFAD; /* vectors are at 0xFFAE(banked 0x3BFAE*/ //0x03BFFF;*/ /* this is the same like nonbanked 0xC000-0xFFFF */ENDPLACEMENT /* Here all predefined and user segments are placed into the SEGMENTS defined above. */    DEFAULT_RAM                         /* non-zero page variables */                                        INTO  RAM;    _PRESTART,                          /* startup code */    STARTUP,                            /* startup data structures */    ROM_VAR,                            /* constant variables */    STRINGS,                            /* string literals */    VIRTUAL_TABLE_SEGMENT,              /* C++ virtual table segment */    NON_BANKED,                         /* runtime routines which must not be banked */    COPY                                /* copy down information: how to initialize variables */                                        INTO  ROM; /* ,ROM1: To use "ROM1" as well, pass the option -OnB=b to the compiler */        DEFAULT_ROM, PAGED_ROM                           /* routines which can be banked */                                        INTO  PPAGE_0,PPAGE_2,ROM,ROM1;//PPAGE_1,PPAGE_3;    _DATA_ZEROPAGE,                     /* zero page variables */    MY_ZEROPAGE                         INTO  Z_RAM;ENDSTACKSIZE 0xC0//VECTOR 0 _Startup     /* Reset vector: this is the default entry point for an application. */&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could somebody explain with a simple example how to use vector redirection with jump table ( it seems to that i have to use this way to create a single project )?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This under is the bootloader prm ( i have surely to modify it... &lt;SPAN class="lia-unicode-emoji" title=":disappointed_face:"&gt;&lt;LI-EMOJI id="lia_disappointed-face" title=":disappointed_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;// This is a linker parameter file for the mc9s08qe128NAMES ENDSEGMENTS Z_RAM   =  READ_WRITE   0x0080 TO 0x00FF; RAM    =  READ_WRITE   0x0100 TO 0x17FF; RAM1   =  READ_WRITE   0x1880 TO 0x207F;  //unbanked FLASH ROM USER_VECT  =  READ_ONLY    0xD7A0 TO 0xD7FF;  //user interrupt vectors USER_DATA  =  READ_ONLY    0xD800 TO 0xDFFF;  //user data BOOT_DATA  =  READ_ONLY    0xE000 TO 0xE01F;  //boot code BOOT_CODE  =  READ_ONLY    0xE020 TO 0xFFAD;  //boot code BOOT_VECT  =  READ_ONLY    0xFFC0 TO 0xFFFF;  //boot interrupt vectors  //banked FLASH ROM PPAGE_0   =  READ_ONLY    0x008000 TO 0x00A07F; //PAGE partially contained in ROM segment //PPAGE_1  =  READ_ONLY    0x018000 TO 0x01BFFF; //PAGE already contained in segment at 0x4000-0x7FFF PPAGE_2   =  READ_ONLY    0x028000 TO 0x02BFFF;  //PPAGE_3  =  READ_ONLY    0x038000 TO 0x03BFFF; //PAGE already contained in segment at 0xC000-0xFFFF PPAGE_4   =  READ_ONLY    0x048000 TO 0x04BFFF;  PPAGE_5   =  READ_ONLY    0x058000 TO 0x05BFFF;  PPAGE_6   =  READ_ONLY    0x068000 TO 0x06BFFF;  PPAGE_7   =  READ_ONLY    0x078000 TO 0x07BFFF; ENDPLACEMENT DEFAULT_RAM    INTO  RAM,RAM1; ISR_USER      //    INTO  USER_VECT; // ISR_BOOT      //    INTO  BOOT_VECT; // _PRESTART,      // startup code STARTUP,      // startup data structures ROM_VAR,      // constant variables DEFAULT_ROM, STRINGS,      // string literals VIRTUAL_TABLE_SEGMENT,   // C++ virtual table segment NON_BANKED,      // runtime routines which must not be banked COPY       // copy down information: how to initialize variables    INTO  BOOT_CODE;  // ,ROM1: To use "ROM1" as well, pass the option -OnB=b to the compiler           _DATA_ZEROPAGE,     // zero page variables MY_ZEROPAGE    INTO  Z_RAM;ENDSTACKSIZE 0x0200&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;I know that is really a newbie question but vector redirection in this case is not so clear to me...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance to anyone!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Oct 2020 09:49:23 GMT</pubDate>
    <dc:creator>Stipey75</dc:creator>
    <dc:date>2020-10-29T09:49:23Z</dc:date>
    <item>
      <title>AN2295 (HC08/S08 Developer's Serial Bootloader) updated for rev. 9.2 - CF V1 (alpha) support added</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-HC08-S08-Developer-s-Serial-Bootloader-updated-for-rev-9/m-p/193983#M15152</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Dears,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;software for Application note AN2295 (HC08/S08 Developer's Serial Bootloader) has been updated recently. Since the last rev. 8 (Aug-2006) several additions and enhancements has been done:&lt;/SPAN&gt;&lt;BR /&gt;&lt;UL&gt;&lt;LI&gt;&lt;STRONG&gt;S08LC&lt;/STRONG&gt; family added&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;S08QE&lt;/STRONG&gt; (Flexis) added&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;S08GB/GT&lt;/STRONG&gt; family updated for A-family&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;S08EL/SL&lt;/STRONG&gt; family added (including EEPROM programming)&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;S08QD&lt;/STRONG&gt; family added (with software SCI)&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;S08DZ&lt;/STRONG&gt; family added (including EEPROM programming)&lt;/LI&gt;&lt;LI&gt;HC08GR8A corrected&lt;/LI&gt;&lt;LI&gt;S08QG8 corrected&lt;/LI&gt;&lt;LI&gt;&lt;STRONG style=": ; font-family: 'Courier New';"&gt;hc08sprg.exe&lt;/STRONG&gt; master updated&lt;/LI&gt;&lt;LI&gt;simple &lt;STRONG&gt;Windows GUI&lt;/STRONG&gt; application added&lt;/LI&gt;&lt;LI&gt;all projects updated for CodeWarrior 6.1&lt;/LI&gt;&lt;/UL&gt;&lt;STRONG&gt;HC08&lt;/STRONG&gt;&lt;SPAN&gt; families supported: &lt;/SPAN&gt;&lt;STRONG&gt;AB/AS/AZ, AP, GP32, GR(A), GZ, JKJL, JKJL8, JW32, KX/EY/GT, LB, LJ, MR, QB, QC, QT/QY, SR&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;S08&lt;/STRONG&gt;&lt;SPAN&gt; families supported: &lt;/SPAN&gt;&lt;STRONG&gt;AW, DZ, EL/SL, GB/GT(A), LC, QD, QE, QG, RC/RD/RE/RG, SR&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any comments, reports, suggestions or wishes are more than welcome. Some of the latest bootloaders are still in alpha stage, tested briefly.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Direct download link is here:&lt;/SPAN&gt;&lt;BR /&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.freescale.com%2Fwebapp%2Fsps%2Fdownload%2Flicense.jsp%3FcolCode%3DAN2295SW" rel="nofollow" target="_blank"&gt;http://www.freescale.com/webapp/sps/download/license.jsp?colCode=AN2295SW&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN style="font-size: 1;"&gt;Unfortunately accompanying application note AN2295.pdf has not been updated yet (to reflect new protocol variations).&lt;BR /&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Best regards, Pavel, ok2ucx&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Freescale Czech Republic&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;an2295 developer&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Message Edited by ok2ucx on &lt;/SPAN&gt;&lt;SPAN class="date_text"&gt;2008-02-19&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN class="time_text"&gt;04:16 PM&lt;/SPAN&gt;&lt;DIV class="message-edit-history"&gt;&lt;SPAN class="edit-author"&gt;Message Edited by ok2ucx on&lt;/SPAN&gt; &lt;SPAN class="local-date"&gt;2009-08-04&lt;/SPAN&gt; &lt;SPAN class="local-time"&gt;10:37 AM&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Feb 2008 23:10:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-HC08-S08-Developer-s-Serial-Bootloader-updated-for-rev-9/m-p/193983#M15152</guid>
      <dc:creator>ok2ucx</dc:creator>
      <dc:date>2008-02-19T23:10:24Z</dc:date>
    </item>
    <item>
      <title>Re: AN2295 (HC08/S08 Developer's Serial Bootloader) updated for rev. 9</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-HC08-S08-Developer-s-Serial-Bootloader-updated-for-rev-9/m-p/193984#M15153</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;is the windows gui application backwards compatible with the previous bootloader versions?&lt;BR /&gt;&lt;BR /&gt;Thanks!&lt;BR /&gt;&lt;BR /&gt;Bob&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Feb 2008 12:41:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-HC08-S08-Developer-s-Serial-Bootloader-updated-for-rev-9/m-p/193984#M15153</guid>
      <dc:creator>TurboBob</dc:creator>
      <dc:date>2008-02-20T12:41:39Z</dc:date>
    </item>
    <item>
      <title>Re: AN2295 (HC08/S08 Developer's Serial Bootloader) updated for rev. 9</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-HC08-S08-Developer-s-Serial-Bootloader-updated-for-rev-9/m-p/193985#M15154</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Dears,&lt;BR /&gt;&lt;BR /&gt;new GUI is a simple Windows executable that actually invokes command line &lt;FONT face="Courier New"&gt;hc08sprg.exe&lt;/FONT&gt;. The calling convention of &lt;FONT face="Courier New"&gt;hc08sprg.exe&lt;/FONT&gt; has not changed, it all should be compatible. GUI was just made to make life easier, especially for those who like clicking &lt;SPAN&gt;&lt;IMG alt=":smileytongue:" class="emoticon emoticon-smileytongue" id="smileytongue" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-tongue.gif" title="Smiley Tongue" /&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;Also updated &lt;FONT face="Courier New"&gt;hc08sprg.exe&lt;/FONT&gt; is all compatible with all embedded codes. The update was required to support new variations of FC bootloader protocol, some newer devices do have a) larger adddress memory space or b) "non-binary" erase page size (DZ family has 768B erase page).&lt;BR /&gt;&lt;BR /&gt;Simply, replace all instances of &lt;FONT face="Courier New"&gt;hc08sprg.exe&lt;/FONT&gt; with the latest version and it all should be OK.&lt;BR /&gt;&lt;BR /&gt;Pavel&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;Message Edited by ok2ucx on &lt;SPAN class="date_text"&gt;2008-02-20&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;08:50 AM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Feb 2008 15:50:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-HC08-S08-Developer-s-Serial-Bootloader-updated-for-rev-9/m-p/193985#M15154</guid>
      <dc:creator>ok2ucx</dc:creator>
      <dc:date>2008-02-20T15:50:05Z</dc:date>
    </item>
    <item>
      <title>Re: AN2295 (HC08/S08 Developer's Serial Bootloader) updated for rev. 9</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-HC08-S08-Developer-s-Serial-Bootloader-updated-for-rev-9/m-p/193986#M15155</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;A couple quick questions:&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Are you planning to release a version for the JM60?&amp;nbsp; Even though there is a USB bootloader, I may want to bootload over serial in a future project that uses the JM.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Will you be posting the sourcecode for the GUI bootloader?&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks!&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Bob&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 08 Mar 2008 11:25:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-HC08-S08-Developer-s-Serial-Bootloader-updated-for-rev-9/m-p/193986#M15155</guid>
      <dc:creator>TurboBob</dc:creator>
      <dc:date>2008-03-08T11:25:22Z</dc:date>
    </item>
    <item>
      <title>Re: AN2295 (HC08/S08 Developer's Serial Bootloader) updated for rev. 9</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-HC08-S08-Developer-s-Serial-Bootloader-updated-for-rev-9/m-p/193987#M15156</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;A couple of quick answers:&lt;BR /&gt;&lt;BR /&gt;* just made alpha version for JM60. Briefly tested. Attached. Seems to work (just quickly tested CMX stack HID demo). If anyone downloads it &amp;amp; tests it (with any result), the feedback is very welcome.&lt;BR /&gt;&lt;BR /&gt;* regarding source code of so-called "GUI" is not planned to be released. It does not contain anything useful related to bootloading. It's just top-level application that justs enumerates COM ports, selects a file and launches command line hc08sprg.exe application. Nothing more. Is there anything particular that you're interested in?&lt;BR /&gt;&lt;BR /&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/files/community_files/8BITCOMM/hc08sprg-s08jm-alpha-1.exe.zip" rel="nofollow" target="_blank"&gt;http://www.freescale.com/files/community_files/8BITCOMM/hc08sprg-s08jm-alpha-1.exe.zip&lt;/A&gt;&lt;/P&gt;&lt;DIV class="message-edit-history"&gt;&lt;SPAN class="edit-author"&gt;Message Edited by t.dowe on&lt;/SPAN&gt; &lt;SPAN class="local-date"&gt;2009-08-18&lt;/SPAN&gt; &lt;SPAN class="local-time"&gt;11:21 AM&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Mar 2008 21:27:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-HC08-S08-Developer-s-Serial-Bootloader-updated-for-rev-9/m-p/193987#M15156</guid>
      <dc:creator>ok2ucx</dc:creator>
      <dc:date>2008-03-13T21:27:46Z</dc:date>
    </item>
    <item>
      <title>Re: AN2295 (HC08/S08 Developer's Serial Bootloader) updated for rev. 9</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-HC08-S08-Developer-s-Serial-Bootloader-updated-for-rev-9/m-p/193988#M15157</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I am just a real Windows rookie, and wanted to see how to enumerate the ports.&lt;BR /&gt;&lt;BR /&gt;Thanks for the JM bootloader.&amp;nbsp; I want to use the JM in a non-USB project.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Thanks!&lt;BR /&gt;&lt;BR /&gt;Bob&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Mar 2008 09:26:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-HC08-S08-Developer-s-Serial-Bootloader-updated-for-rev-9/m-p/193988#M15157</guid>
      <dc:creator>TurboBob</dc:creator>
      <dc:date>2008-03-14T09:26:47Z</dc:date>
    </item>
    <item>
      <title>Re: AN2295 (HC08/S08 Developer's Serial Bootloader) updated for rev. 9</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-HC08-S08-Developer-s-Serial-Bootloader-updated-for-rev-9/m-p/193989#M15158</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Bob,&lt;BR /&gt;&lt;BR /&gt;If you want some sample code to use a serial port go &lt;A href="http://www.lvr.com/serport.htm#example_code" rel="nofollow" target="_blank"&gt;here.&lt;/A&gt;&lt;BR /&gt;There is sample code for both VB and C# NET&lt;BR /&gt;The book is supposed to be very good as well.&lt;BR /&gt;Also search on code project as there is a C++ class there that I have used.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Mar 2008 10:20:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-HC08-S08-Developer-s-Serial-Bootloader-updated-for-rev-9/m-p/193989#M15158</guid>
      <dc:creator>JimDon</dc:creator>
      <dc:date>2008-03-14T10:20:32Z</dc:date>
    </item>
    <item>
      <title>Re: AN2295 (HC08/S08 Developer's Serial Bootloader) updated for rev. 9</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-HC08-S08-Developer-s-Serial-Bootloader-updated-for-rev-9/m-p/193990#M15159</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Thanks to all for the help.&lt;BR /&gt;&lt;BR /&gt;I use Borland C++ Builder 5, and built myself a GUI bootloader wrapper.&amp;nbsp; I used a 3rd party serial library that had built in port enumeration which works well.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;I will be testing the JM version in about a month, I will post back if I have troubles&lt;BR /&gt;&lt;BR /&gt;Bob&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 06 Apr 2008 23:57:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-HC08-S08-Developer-s-Serial-Bootloader-updated-for-rev-9/m-p/193990#M15159</guid>
      <dc:creator>TurboBob</dc:creator>
      <dc:date>2008-04-06T23:57:35Z</dc:date>
    </item>
    <item>
      <title>Re: AN2295 (HC08/S08 Developer's Serial Bootloader) updated for rev. 9</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-HC08-S08-Developer-s-Serial-Bootloader-updated-for-rev-9/m-p/193991#M15160</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Bob,&lt;BR /&gt;&lt;BR /&gt;Are you saying that you use a serial port, and that the CDC code is used on the JM board?&lt;BR /&gt;That is the JM board is a USB serial port.&lt;BR /&gt;&lt;BR /&gt;Or are you coming in via a serial port external to the JM board (meaning an SCI port on the JM)?&lt;BR /&gt;That is you would need an external USB to serial adaptor.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Apr 2008 00:18:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-HC08-S08-Developer-s-Serial-Bootloader-updated-for-rev-9/m-p/193991#M15160</guid>
      <dc:creator>JimDon</dc:creator>
      <dc:date>2008-04-07T00:18:25Z</dc:date>
    </item>
    <item>
      <title>Re: AN2295 (HC08/S08 Developer's Serial Bootloader) updated for rev. 9</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-HC08-S08-Developer-s-Serial-Bootloader-updated-for-rev-9/m-p/193992#M15161</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;no,&amp;nbsp; this particular project is using the JM, but not USB.&amp;nbsp; So I wanted to use the bootloader just like on my AW60 projects, with SCI communication via RS232 to a PC.&lt;BR /&gt;&lt;BR /&gt;My USB projects are coming up next.&amp;nbsp; At which point I will bug you a lot.....&amp;nbsp; &lt;IMG alt=":smileyhappy:" class="emoticon emoticon-smileyhappy" id="smileyhappy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif" title="Smiley Happy" /&gt;&lt;BR /&gt;&lt;BR /&gt;Bob&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Apr 2008 00:32:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-HC08-S08-Developer-s-Serial-Bootloader-updated-for-rev-9/m-p/193992#M15161</guid>
      <dc:creator>TurboBob</dc:creator>
      <dc:date>2008-04-07T00:32:08Z</dc:date>
    </item>
    <item>
      <title>Re: AN2295 (HC08/S08 Developer's Serial Bootloader) updated for rev. 9</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-HC08-S08-Developer-s-Serial-Bootloader-updated-for-rev-9/m-p/193993#M15162</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Bob,&lt;BR /&gt;Well, I have a POD (plain old dll) that give a nice interface to a hid device, and should work just fine with your code, regardless of the language.&lt;BR /&gt;Note also that the &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MCF51JM&amp;amp;nodeId=0162468rH3YTLC00M924B2" rel="nofollow" target="_blank"&gt;V1 JM is out now&lt;/A&gt;. If you have the DEMOJM with the 64 LQFP socket you should be able to drop it right in.&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;Message Edited by JimDon on &lt;SPAN class="date_text"&gt;2008-04-06&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;01:40 PM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Apr 2008 00:39:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-HC08-S08-Developer-s-Serial-Bootloader-updated-for-rev-9/m-p/193993#M15162</guid>
      <dc:creator>JimDon</dc:creator>
      <dc:date>2008-04-07T00:39:53Z</dc:date>
    </item>
    <item>
      <title>Re: AN2295 (HC08/S08 Developer's Serial Bootloader) updated for rev. 9</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-HC08-S08-Developer-s-Serial-Bootloader-updated-for-rev-9/m-p/193994#M15163</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;FONT size="3"&gt;both items are&lt;/FONT&gt; &lt;FONT size="5"&gt;Excellent &lt;FONT size="3"&gt;news!!!!&lt;BR /&gt;&lt;BR /&gt;Thanks!&lt;BR /&gt;&lt;BR /&gt;Bob&lt;BR /&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Apr 2008 00:42:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-HC08-S08-Developer-s-Serial-Bootloader-updated-for-rev-9/m-p/193994#M15163</guid>
      <dc:creator>TurboBob</dc:creator>
      <dc:date>2008-04-07T00:42:34Z</dc:date>
    </item>
    <item>
      <title>Re: AN2295 (HC08/S08 Developer's Serial Bootloader) updated for rev. 9</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-HC08-S08-Developer-s-Serial-Bootloader-updated-for-rev-9/m-p/193995#M15164</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hey,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I was hoping to look at some of the demos and DLL's you have working.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I plugged in my demo, and loaded up the HID demo, and my mouse pointer wiggles.....&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Can you direct me to your demos, I want to try them next.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks for all your help!!&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Bob&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 May 2008 07:14:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-HC08-S08-Developer-s-Serial-Bootloader-updated-for-rev-9/m-p/193995#M15164</guid>
      <dc:creator>TurboBob</dc:creator>
      <dc:date>2008-05-28T07:14:14Z</dc:date>
    </item>
    <item>
      <title>Re: AN2295 (HC08/S08 Developer's Serial Bootloader) updated for rev. 9</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-HC08-S08-Developer-s-Serial-Bootloader-updated-for-rev-9/m-p/193996#M15165</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Has anyone looked into porting AN2295 to use the HID interface on a JM60?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks!&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Bob&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Jul 2008 04:00:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-HC08-S08-Developer-s-Serial-Bootloader-updated-for-rev-9/m-p/193996#M15165</guid>
      <dc:creator>TurboBob</dc:creator>
      <dc:date>2008-07-30T04:00:57Z</dc:date>
    </item>
    <item>
      <title>Re: AN2295 (HC08/S08 Developer's Serial Bootloader) updated for rev. 9</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-HC08-S08-Developer-s-Serial-Bootloader-updated-for-rev-9/m-p/193997#M15166</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Hmmm, what do you mean?&lt;BR /&gt;&lt;BR /&gt;Porting AN2295 JM60 bootloader (currently SCI only) so it uses true USB interface (CDC class - Virtual Serial Port)? Just like with older HC08JW32? Is this what you want?&lt;BR /&gt;&lt;BR /&gt;If this is the case, such portation is in queue with no exact schedule. If there's some interest, we could increase the priority.&lt;BR /&gt;&lt;BR /&gt;Pavel, an2295 bootloader developer&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Jul 2008 15:48:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-HC08-S08-Developer-s-Serial-Bootloader-updated-for-rev-9/m-p/193997#M15166</guid>
      <dc:creator>ok2ucx</dc:creator>
      <dc:date>2008-07-30T15:48:00Z</dc:date>
    </item>
    <item>
      <title>Re: AN2295 (HC08/S08 Developer's Serial Bootloader) updated for rev. 9</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-HC08-S08-Developer-s-Serial-Bootloader-updated-for-rev-9/m-p/193998#M15167</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;My original thought was to make it HID, as my main application is HID,&amp;nbsp; so only one set of drivers and one VID/PID would be needed.&amp;nbsp; (HID using the CMX stack needs no extra driver,&amp;nbsp; which is a good thing in my opinion)&lt;BR /&gt;&lt;BR /&gt;CDC would work though...&lt;BR /&gt;&lt;BR /&gt;Let me know if I can help the process along.&lt;BR /&gt;&lt;BR /&gt;Bob&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Jul 2008 23:15:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-HC08-S08-Developer-s-Serial-Bootloader-updated-for-rev-9/m-p/193998#M15167</guid>
      <dc:creator>TurboBob</dc:creator>
      <dc:date>2008-07-30T23:15:41Z</dc:date>
    </item>
    <item>
      <title>Re: AN2295 (HC08/S08 Developer's Serial Bootloader) updated for rev. 9</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-HC08-S08-Developer-s-Serial-Bootloader-updated-for-rev-9/m-p/193999#M15168</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Another idea is the method that the FTF Badge-board used.&lt;BR /&gt;&lt;BR /&gt;When you put the unit into bootloader mode it apears as a USB hard-drive to the host computer.&amp;nbsp; You drop the S19 file in the drive window and the bootloader loads it.&lt;BR /&gt;&lt;BR /&gt;I believe thats how it worked,&amp;nbsp; I did not attend FTF.&lt;BR /&gt;&lt;BR /&gt;Bob&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Jul 2008 07:00:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-HC08-S08-Developer-s-Serial-Bootloader-updated-for-rev-9/m-p/193999#M15168</guid>
      <dc:creator>TurboBob</dc:creator>
      <dc:date>2008-07-31T07:00:47Z</dc:date>
    </item>
    <item>
      <title>Re: AN2295 (HC08/S08 Developer's Serial Bootloader) updated for rev. 9</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-HC08-S08-Developer-s-Serial-Bootloader-updated-for-rev-9/m-p/194000#M15169</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;BR /&gt;There was really no discussion of the badge board at FTF, but the web site has all the information.&lt;BR /&gt;&lt;BR /&gt;As I have mentioned on other threads, go to canyourbadgedothis.com and register so you can down load the sample code. It is certainly a sample of flashing for the V1.&lt;BR /&gt;&lt;BR /&gt;There was talk of making the badge boards available, but I don't know what came of that.&lt;BR /&gt;&lt;BR /&gt;BTW I would like to see a HID based boot loader as well, mainly because HID is easy in terms of no installation of any kind required.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Message Edited by JimDon on &lt;SPAN class="date_text"&gt;2008-07-31&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;09:04 AM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Jul 2008 20:02:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-HC08-S08-Developer-s-Serial-Bootloader-updated-for-rev-9/m-p/194000#M15169</guid>
      <dc:creator>JimDon</dc:creator>
      <dc:date>2008-07-31T20:02:03Z</dc:date>
    </item>
    <item>
      <title>Re: AN2295 (HC08/S08 Developer's Serial Bootloader) updated for rev. 9</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-HC08-S08-Developer-s-Serial-Bootloader-updated-for-rev-9/m-p/194001#M15170</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;BLOCKQUOTE&gt;&lt;FONT size="2"&gt;&lt;BR /&gt;BTW I would like to see a HID based boot loader as well, mainly because HID is easy in terms of no installation of any kind required.&lt;/FONT&gt;&lt;/BLOCKQUOTE&gt;Dears,&lt;BR /&gt;&lt;BR /&gt;could you, please, let me know, how this bootloader would work? &lt;SPAN&gt;&lt;IMG alt=":smileysurprised:" class="emoticon emoticon-smileysurprised" id="smileysurprised" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-surprised.gif" title="Smiley Surprised" /&gt;&lt;/SPAN&gt; In my understanding, HID USB device is something like mouse, keyboard, joystick, tablet, etc. Yes, for sure, it installs easily (on Windows) since Win HID driver is there by default and HID class is recognized properly. Despite of this, I have no idea how to feed data (S19 file) to/from such HID device?&lt;BR /&gt;&lt;BR /&gt;On the other side, I plan to have USB CDC class JM60 bootloader, just another port for existing AN2295 bootloader. After the JM60 resets in bootloader mode, it will appear as Virtual Serial Port (very possibly under the same PID/VID as existing JW32 bootloader = as the same COM port number). Then it is possible to send the boot data thru such COM port (just like it was standard SCI-based HC08/S08 AN2295 bootloader).&lt;BR /&gt;&lt;BR /&gt;Installation is one-time only process, not that well managed by Windows, since there's no specific .inf file for this PID/VID and Windows do not recognize CDC class by default (as HID class for example). Although usbser.sys (driver for CDC class in there), but there's no link for Windows to use that.&lt;BR /&gt;&lt;BR /&gt;Regards, Pavel&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Jul 2008 21:13:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-HC08-S08-Developer-s-Serial-Bootloader-updated-for-rev-9/m-p/194001#M15170</guid>
      <dc:creator>ok2ucx</dc:creator>
      <dc:date>2008-07-31T21:13:30Z</dc:date>
    </item>
    <item>
      <title>Re: AN2295 (HC08/S08 Developer's Serial Bootloader) updated for rev. 9</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-HC08-S08-Developer-s-Serial-Bootloader-updated-for-rev-9/m-p/194002#M15171</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;First of all, I should have been more specific.&lt;BR /&gt;There is a class called Generic HID (GHID). There are windows APIs to talk to to generic hid.&lt;BR /&gt;&lt;BR /&gt;The normal (mouse, keyboard etc) windows HID drivers will leave a GHID device alone, and only an app that knows about it can talk to it by VID/PID. But, windows will recognise with it no addtional files or drivers (for CDC you at least need an .inf file - even if you use the built in usn serial driver).&lt;BR /&gt;&lt;BR /&gt;I have a DLL that has a VC++ class that has sample code for this, which you are welcome to use as a sample. You can basicly use file I/O to talk to it.&lt;BR /&gt;&lt;BR /&gt;One nice thing about my code is you do not need anything from the DDK (WDK) as I manually export the entry points from the DLL.&lt;BR /&gt;&lt;BR /&gt;I have a new version of the DLL which I will post tonight if you are interested. I also have a sample app that talks to it. The CMX sample code (which it is based on) has a GHID device in and a sample app as well (but, the PC side code in thier sample is pretty limited).&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Aug 2008 01:46:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-HC08-S08-Developer-s-Serial-Bootloader-updated-for-rev-9/m-p/194002#M15171</guid>
      <dc:creator>JimDon</dc:creator>
      <dc:date>2008-08-01T01:46:28Z</dc:date>
    </item>
  </channel>
</rss>