<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: STOP2 and RTI Isr on QG8 in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/STOP2-and-RTI-Isr-on-QG8/m-p/193404#M15034</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jack,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It is my understanding that, when the RTI module is used to wakeup from STOP2 mode, the normal reset vector is used, rather than the RTI vector.&amp;nbsp; You would then need to test the SPMSC2_PPDF bit to determine when the reset is a result of STOP2 recovery.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 25 Jun 2009 09:41:05 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2009-06-25T09:41:05Z</dc:date>
    <item>
      <title>STOP2 and RTI Isr on QG8</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/STOP2-and-RTI-Isr-on-QG8/m-p/193403#M15033</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;in STOP3, when RTI wakes up the MCU, the RTI Isr is fired, executed (it increments a variable) and then the flow of the program return to the instruction after "asm stop".&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now: what happens with the STOP2 mode? the RTI Isr is executed or not? Because I use the RTI Isr (executed every 1024 msec) as "rough" clock because I need to do things every 30 sec, so the MCU wake up, increment a variable, check if it's less than 30 goes to sleep, else does some work.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks bye Jack&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jun 2009 13:57:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/STOP2-and-RTI-Isr-on-QG8/m-p/193403#M15033</guid>
      <dc:creator>jag</dc:creator>
      <dc:date>2009-06-24T13:57:53Z</dc:date>
    </item>
    <item>
      <title>Re: STOP2 and RTI Isr on QG8</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/STOP2-and-RTI-Isr-on-QG8/m-p/193404#M15034</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jack,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It is my understanding that, when the RTI module is used to wakeup from STOP2 mode, the normal reset vector is used, rather than the RTI vector.&amp;nbsp; You would then need to test the SPMSC2_PPDF bit to determine when the reset is a result of STOP2 recovery.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Jun 2009 09:41:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/STOP2-and-RTI-Isr-on-QG8/m-p/193404#M15034</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2009-06-25T09:41:05Z</dc:date>
    </item>
  </channel>
</rss>