<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Debug Interface for MC9S08DV60 in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Debug-Interface-for-MC9S08DV60/m-p/193402#M15032</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Thomas,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;HR /&gt;Thommi_Tulpe wrote:&lt;BR /&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have to design a board with the MC9S08DV60 8bit MC.&lt;/P&gt;&lt;P&gt;How can I connect the MC to the CodeWarrior Developmet Environment.&lt;/P&gt;&lt;P&gt;I looked in the schematic from the DEMO09S08DZ60. In this schematic the connection is done with an IC from P&amp;amp;E via USB.&lt;/P&gt;&lt;P&gt;Is there another way to program and debug the MC9S08DV60?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;HR /&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Programming and debug via 6-pin BDM connection.&amp;nbsp; Refer to the Reference Manual for the device.&amp;nbsp; This connection is compatible with P&amp;amp;E USB Multilink Interface, or other open source products.&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;HR /&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I also have a demoboard for the MCR9S08KA8 (DEMO9RS08KA8). On this Board there is a USB To BDM Interface. Can I connect this Interface to the BKG0 and RESET Pin of the MC9S08DV60 to download and debug porgramms with the CodeWarrior?&lt;/P&gt;&lt;HR /&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;BR /&gt;Once upon a time, the BDM interface associated with a demo board could be used to program devices&amp;nbsp;other than those for which the demo board was intended.&amp;nbsp; But apparently this is no longer the case.&amp;nbsp; There may be a workaround for some versions of CW, involving messing with DLL versions.&amp;nbsp; Refer to &lt;A href="https://community.freescale.com/message/49272#49272" title="https://community.freescale.com/message/49272#49272"&gt;https://community.freescale.com/message/49272#49272&lt;/A&gt;old thread.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The demo board for a 9RS08 product could be problematic for another reason, because it provides a programming voltage not needed by the 9S08 devices.&amp;nbsp; This voltage would need to be disabled.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;HR /&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it posible to design a gateway to the CodeWarrior without USB e. g. with the parallel or serial com port of the personal computer (PC)?&lt;/P&gt;&lt;P&gt;I did something like that for the DSP56F803, but this DSP has a JTAG-Interface.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;HR /&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;The BDM communications protocol is described within the Reference Manual or datasheet.&amp;nbsp; This would seem like a lot of hard work.&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;BLOCKQUOTE&gt;&lt;HR /&gt;Thommi_Tulpe wrote:&lt;BR /&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What is the easyest way to program the MC9S08DV60 ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;HR /&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;BR /&gt;&amp;nbsp;USB Multilink interface, IMHO.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 31 Aug 2012 13:47:52 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2012-08-31T13:47:52Z</dc:date>
    <item>
      <title>Debug Interface for MC9S08DV60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Debug-Interface-for-MC9S08DV60/m-p/193401#M15031</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have to design a board with the MC9S08DV60 8bit MC.&lt;/P&gt;&lt;P&gt;How can I connect the MC to the CodeWarrior Developmet Environment.&lt;/P&gt;&lt;P&gt;I looked in the schematic from the DEMO09S08DZ60. In this schematic the connection is done with an IC from P&amp;amp;E via USB.&lt;/P&gt;&lt;P&gt;Is there another way to program and debug the MC9S08DV60?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I also have a demoboard for the MCR9S08KA8 (DEMO9RS08KA8). On this Board there is a USB To BDM Interface. Can I connect this Interface to the BKG0 and RESET Pin of the MC9S08DV60 to download and debug porgramms with the CodeWarrior?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it posible to design a gateway to the CodeWarrior without USB e. g. with the parallel or serial com port of the personal computer (PC)?&lt;/P&gt;&lt;P&gt;I did something like that for the DSP56F803, but this DSP has a JTAG-Interface.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What is the easyest way to program the MC9S08DV60 ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope someon can help&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Aug 2012 03:38:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Debug-Interface-for-MC9S08DV60/m-p/193401#M15031</guid>
      <dc:creator>Thommi_Tulpe</dc:creator>
      <dc:date>2012-08-31T03:38:54Z</dc:date>
    </item>
    <item>
      <title>Re: Debug Interface for MC9S08DV60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Debug-Interface-for-MC9S08DV60/m-p/193402#M15032</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Thomas,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;HR /&gt;Thommi_Tulpe wrote:&lt;BR /&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have to design a board with the MC9S08DV60 8bit MC.&lt;/P&gt;&lt;P&gt;How can I connect the MC to the CodeWarrior Developmet Environment.&lt;/P&gt;&lt;P&gt;I looked in the schematic from the DEMO09S08DZ60. In this schematic the connection is done with an IC from P&amp;amp;E via USB.&lt;/P&gt;&lt;P&gt;Is there another way to program and debug the MC9S08DV60?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;HR /&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Programming and debug via 6-pin BDM connection.&amp;nbsp; Refer to the Reference Manual for the device.&amp;nbsp; This connection is compatible with P&amp;amp;E USB Multilink Interface, or other open source products.&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;HR /&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I also have a demoboard for the MCR9S08KA8 (DEMO9RS08KA8). On this Board there is a USB To BDM Interface. Can I connect this Interface to the BKG0 and RESET Pin of the MC9S08DV60 to download and debug porgramms with the CodeWarrior?&lt;/P&gt;&lt;HR /&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;BR /&gt;Once upon a time, the BDM interface associated with a demo board could be used to program devices&amp;nbsp;other than those for which the demo board was intended.&amp;nbsp; But apparently this is no longer the case.&amp;nbsp; There may be a workaround for some versions of CW, involving messing with DLL versions.&amp;nbsp; Refer to &lt;A href="https://community.freescale.com/message/49272#49272" title="https://community.freescale.com/message/49272#49272"&gt;https://community.freescale.com/message/49272#49272&lt;/A&gt;old thread.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The demo board for a 9RS08 product could be problematic for another reason, because it provides a programming voltage not needed by the 9S08 devices.&amp;nbsp; This voltage would need to be disabled.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;HR /&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it posible to design a gateway to the CodeWarrior without USB e. g. with the parallel or serial com port of the personal computer (PC)?&lt;/P&gt;&lt;P&gt;I did something like that for the DSP56F803, but this DSP has a JTAG-Interface.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;HR /&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;The BDM communications protocol is described within the Reference Manual or datasheet.&amp;nbsp; This would seem like a lot of hard work.&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;BLOCKQUOTE&gt;&lt;HR /&gt;Thommi_Tulpe wrote:&lt;BR /&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What is the easyest way to program the MC9S08DV60 ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;HR /&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;BR /&gt;&amp;nbsp;USB Multilink interface, IMHO.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Aug 2012 13:47:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Debug-Interface-for-MC9S08DV60/m-p/193402#M15032</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2012-08-31T13:47:52Z</dc:date>
    </item>
  </channel>
</rss>