<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックMC3PHAC with brushless motor</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC3PHAC-with-brushless-motor/m-p/193383#M15028</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I would like use MC3PHAC witch brushless motor :&amp;nbsp;&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.modelflight.com.au%2Fmanuals%2Fpdf%2Faxi_motors%2Faxi2808-14.pdf" rel="nofollow" target="_blank"&gt;http://www.modelflight.com.au/manuals/pdf/axi_motors/axi2808-14.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;But I am not sure if is MC3PHAC best way to control brushless motor.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Have anybody some experience with this?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you very much.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 30 Dec 2011 06:04:14 GMT</pubDate>
    <dc:creator>Seitec</dc:creator>
    <dc:date>2011-12-30T06:04:14Z</dc:date>
    <item>
      <title>MC3PHAC with brushless motor</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC3PHAC-with-brushless-motor/m-p/193383#M15028</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I would like use MC3PHAC witch brushless motor :&amp;nbsp;&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.modelflight.com.au%2Fmanuals%2Fpdf%2Faxi_motors%2Faxi2808-14.pdf" rel="nofollow" target="_blank"&gt;http://www.modelflight.com.au/manuals/pdf/axi_motors/axi2808-14.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;But I am not sure if is MC3PHAC best way to control brushless motor.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Have anybody some experience with this?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you very much.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Dec 2011 06:04:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC3PHAC-with-brushless-motor/m-p/193383#M15028</guid>
      <dc:creator>Seitec</dc:creator>
      <dc:date>2011-12-30T06:04:14Z</dc:date>
    </item>
    <item>
      <title>Re: MC3PHAC with brushless motor</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC3PHAC-with-brushless-motor/m-p/193384#M15029</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Seitec,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;No, the MC3PHAC would not be able to drive that motor. The MC3PHAC is designed for AC induction motors (think "washing machine"), and not for permanent-magnet motors. Also, the MC3PHAC is meant to drive motors at AC line voltages, and the motor you linked to is a low voltage / high-current battery-powered motor.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There are different ways to drive that motor, depending on the application. If you are driving a model aircraft propeller, as the motor was designed, then a single mosfet switched from some PWM controller would be appropriate (that would be "single-quadrant" operation). Other applications might need two or four quadrant operation. If you need precise speed regulation, or position control, then that motor may be a bad choice.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Dec 2011 13:39:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC3PHAC-with-brushless-motor/m-p/193384#M15029</guid>
      <dc:creator>rocco</dc:creator>
      <dc:date>2011-12-30T13:39:07Z</dc:date>
    </item>
    <item>
      <title>Re: MC3PHAC with brushless motor</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC3PHAC-with-brushless-motor/m-p/193385#M15030</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Oops, my mistake.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There is no way to drive a &lt;STRONG&gt;brushless&lt;/STRONG&gt; motor with a "single mosfet". I was thinking of a &lt;STRONG&gt;brushed&lt;/STRONG&gt; motor when I wrote that. Sorry.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The datasheet does not help in determining how many transistors you will need. If it is wired in a "wye" configuration with a center-tap (four wires), then you can get away with three switches. But more likely it is wired in a "delta" configuration (three wires), which means you will need six switches. Whether those switches are bipolar transistors or mosfet transistors would depend on the amount of current it will typically draw.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The hard part will be the commutation (knowing when to switch windings). That particular motor has no feedback, except for its back-emf. There may be ICs that can commutate using back-emf (it's not a difficult process), but I have not seen one. I have always used a DSP to do that.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Dec 2011 16:57:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC3PHAC-with-brushless-motor/m-p/193385#M15030</guid>
      <dc:creator>rocco</dc:creator>
      <dc:date>2011-12-30T16:57:46Z</dc:date>
    </item>
  </channel>
</rss>