<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: General purpose I/O voltage level problem</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/General-purpose-I-O-voltage-level-problem-Added-p-n-MC1321x/m-p/193270#M14995</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;Hello,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Is there any reason that you can't use a 74HC374 device?&amp;nbsp; This can operate from a 3 volt supply, and so would be compatible with the MC1321x device.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;An alternative approach to providing input or output expansion would be to use shift register devices, and to bit bang the SPI communications.&amp;nbsp; For input expansion, a suitable device might be the 74HC589 or 74HC597.&amp;nbsp; Multiple devices may be cascaded.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Mac&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;Message Edited by bigmac on &lt;SPAN class="date_text"&gt;2008-10-14&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;03:31 AM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 Oct 2008 00:28:33 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2008-10-14T00:28:33Z</dc:date>
    <item>
      <title>General purpose I/O voltage level problem - Added p/n MC1321x zigbee</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/General-purpose-I-O-voltage-level-problem-Added-p-n-MC1321x/m-p/193269#M14994</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;SPAN&gt;Hi all&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am working on MC1321x zigbee&amp;nbsp; wireless network.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I need more general purpose I/O than what is available on the board.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I used 74LS374 for adding more I/O ports.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The problem is that 74LS374 uses 5Volt Vcc. However its high output voltage is measured about 3.8Volt which is not too larger than 3Volt(high voltage level of the board). Can I connect this 3.8Volt directly to an input general purpose port of the board or I have to convert it to 3Volt. If so, how can I do that?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks alot&amp;nbsp;&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Message Edited by NLFSJ on &lt;/SPAN&gt;&lt;SPAN class="date_text"&gt;2008-10-13&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN class="time_text"&gt;12:59 PM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Oct 2008 20:52:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/General-purpose-I-O-voltage-level-problem-Added-p-n-MC1321x/m-p/193269#M14994</guid>
      <dc:creator>bitasobhani</dc:creator>
      <dc:date>2008-10-13T20:52:47Z</dc:date>
    </item>
    <item>
      <title>Re: General purpose I/O voltage level problem</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/General-purpose-I-O-voltage-level-problem-Added-p-n-MC1321x/m-p/193270#M14995</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;Hello,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Is there any reason that you can't use a 74HC374 device?&amp;nbsp; This can operate from a 3 volt supply, and so would be compatible with the MC1321x device.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;An alternative approach to providing input or output expansion would be to use shift register devices, and to bit bang the SPI communications.&amp;nbsp; For input expansion, a suitable device might be the 74HC589 or 74HC597.&amp;nbsp; Multiple devices may be cascaded.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Mac&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;Message Edited by bigmac on &lt;SPAN class="date_text"&gt;2008-10-14&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;03:31 AM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Oct 2008 00:28:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/General-purpose-I-O-voltage-level-problem-Added-p-n-MC1321x/m-p/193270#M14995</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2008-10-14T00:28:33Z</dc:date>
    </item>
  </channel>
</rss>