<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 graphic LCD interfacing</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/graphic-LCD-interfacing/m-p/193090#M14953</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all&lt;/P&gt;&lt;P&gt;has anyone tried connecting one of the graphic LCD modules from KENTEC, such as &lt;SPAN&gt;K350QVG-V2-F&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;to a S908 micro&amp;nbsp;(using the port lines to generate data lines. WR, CS, &amp;nbsp;of course) ?&lt;/P&gt;&lt;P&gt;The driver IC HX8347-D&amp;nbsp;docs are hard to follow (asian!)...&lt;/P&gt;&lt;P&gt;I don't need fast grahics (text only), so update speed should not be a problem.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Dec 2011 04:29:17 GMT</pubDate>
    <dc:creator>donw</dc:creator>
    <dc:date>2011-12-29T04:29:17Z</dc:date>
    <item>
      <title>graphic LCD interfacing</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/graphic-LCD-interfacing/m-p/193090#M14953</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all&lt;/P&gt;&lt;P&gt;has anyone tried connecting one of the graphic LCD modules from KENTEC, such as &lt;SPAN&gt;K350QVG-V2-F&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;to a S908 micro&amp;nbsp;(using the port lines to generate data lines. WR, CS, &amp;nbsp;of course) ?&lt;/P&gt;&lt;P&gt;The driver IC HX8347-D&amp;nbsp;docs are hard to follow (asian!)...&lt;/P&gt;&lt;P&gt;I don't need fast grahics (text only), so update speed should not be a problem.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Dec 2011 04:29:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/graphic-LCD-interfacing/m-p/193090#M14953</guid>
      <dc:creator>donw</dc:creator>
      <dc:date>2011-12-29T04:29:17Z</dc:date>
    </item>
    <item>
      <title>Re: graphic LCD interfacing</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/graphic-LCD-interfacing/m-p/193091#M14954</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;not yet, but the next project in the pipeline will most likely have a small graphical LCD or OLED. Once I get started, I'll post back.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Bob&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Dec 2011 04:51:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/graphic-LCD-interfacing/m-p/193091#M14954</guid>
      <dc:creator>TurboBob</dc:creator>
      <dc:date>2011-12-29T04:51:47Z</dc:date>
    </item>
  </channel>
</rss>