<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: internal watchdog in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/internal-watchdog/m-p/192704#M14885</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;You do not say which HCS08 device you are using.&amp;nbsp; The variation of COP timeout period will depend entirely on the oscillator source that increments the COP counter.&amp;nbsp; If an internal&amp;nbsp;RC oscillator is used, this will generally have a wide frequency tolerance unit-to-unit, and&amp;nbsp;for variation of voltage and temperature.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Normally the minimum interval is the critical period because it determines how frequently COP counter reset must occur to prevent timeout.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Mac&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Feb 2008 19:11:12 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2008-02-21T19:11:12Z</dc:date>
    <item>
      <title>internal watchdog</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/internal-watchdog/m-p/192703#M14884</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I am&amp;nbsp;working on&amp;nbsp;Freescale HCS08 microcontroller.&lt;/DIV&gt;&lt;DIV&gt;and i am using internal watchdog provided by it ,Datasheet says its refresh time is 32msec but when i checked through CRO it showed me 37msec.Is there any chance that at cold temperatures it will take more time than that.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Feb 2008 18:05:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/internal-watchdog/m-p/192703#M14884</guid>
      <dc:creator>ramabh</dc:creator>
      <dc:date>2008-02-21T18:05:27Z</dc:date>
    </item>
    <item>
      <title>Re: internal watchdog</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/internal-watchdog/m-p/192704#M14885</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;You do not say which HCS08 device you are using.&amp;nbsp; The variation of COP timeout period will depend entirely on the oscillator source that increments the COP counter.&amp;nbsp; If an internal&amp;nbsp;RC oscillator is used, this will generally have a wide frequency tolerance unit-to-unit, and&amp;nbsp;for variation of voltage and temperature.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Normally the minimum interval is the critical period because it determines how frequently COP counter reset must occur to prevent timeout.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Mac&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Feb 2008 19:11:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/internal-watchdog/m-p/192704#M14885</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2008-02-21T19:11:12Z</dc:date>
    </item>
    <item>
      <title>Re: internal watchdog</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/internal-watchdog/m-p/192705#M14886</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi&lt;/DIV&gt;&lt;DIV&gt;i am using MC9S08DZ60 microcontroller.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;With your message it is clear that with temperature even internal watchdog timeout period will increase.&lt;/DIV&gt;&lt;DIV&gt;I mentioned watchdog time out period to be 32msec but its varying between 32 to 40msec,Is there any chance that at cold temperatures like -40 the timeout will increaase more than 50msec&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Feb 2008 19:33:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/internal-watchdog/m-p/192705#M14886</guid>
      <dc:creator>ramabh</dc:creator>
      <dc:date>2008-02-21T19:33:30Z</dc:date>
    </item>
    <item>
      <title>Re: internal watchdog</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/internal-watchdog/m-p/192706#M14887</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;According to the data sheet for the DZ60, the internal low power oscillator may have a period between the limits 0.7 to 1.3 milliseconds.&amp;nbsp; When this is used as the source for the COP timer, and&amp;nbsp;using the shortest threshold setting, the COP timeout period should lie somewhere between 22 and 42 ms.&amp;nbsp; Since there doesn't appear to be a published temperature curve for the oscillator, it is unclear whether these limits would apply over the full range of temperatures.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;If it is important for your application that the COP timeout period be more closely controlled, you will need to alternatively consider the bus frequency as the COP timeout source.&amp;nbsp; Refer to table 5.6 in the data sheet.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Mac&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Feb 2008 20:02:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/internal-watchdog/m-p/192706#M14887</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2008-02-21T20:02:58Z</dc:date>
    </item>
  </channel>
</rss>