<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Mitigating Double Interrupt Using Mechanical Switch and IRQ / KBI</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Mitigating-Double-Interrupt-Using-Mechanical-Switch-and-IRQ-KBI/m-p/192593#M14869</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;A problem which I'm sure others have had, but which is difficult to find mentioned in past discussion:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Using a mechanical (tactile SPST momentary) switch to trigger interrupts using the IRQ or KBI modules, I often get "double clicks."&amp;nbsp; I am using falling-edge-only detection, so with a perfect switch, this should not happen.&amp;nbsp; But no mechanical switch is perfect, and the typical 6mm x 6mm tactile switch PCB-mount switch ubiquitous in consumer electronics seems to routinely switch not-so-cleanly, causing multiple pulses instead of a single edge, particularly as pressure is removed from the switch as it returns to "open" position.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there a pre-existing primer on dealing with this issue in in the MCU realm?&amp;nbsp; I'm new.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So far I've implemented a timer that simply skips the interrupt routine if it is called within 250 ms of a previous interrupt.&amp;nbsp; This works sometimes, but sometimes the user holds the button down longer than 250 ms, and increasing to 500 ms is bad for usability, because people want to click faster than that.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Patrick&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Feb 2008 14:14:37 GMT</pubDate>
    <dc:creator>PatrickW</dc:creator>
    <dc:date>2008-02-21T14:14:37Z</dc:date>
    <item>
      <title>Mitigating Double Interrupt Using Mechanical Switch and IRQ / KBI</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Mitigating-Double-Interrupt-Using-Mechanical-Switch-and-IRQ-KBI/m-p/192593#M14869</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;A problem which I'm sure others have had, but which is difficult to find mentioned in past discussion:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Using a mechanical (tactile SPST momentary) switch to trigger interrupts using the IRQ or KBI modules, I often get "double clicks."&amp;nbsp; I am using falling-edge-only detection, so with a perfect switch, this should not happen.&amp;nbsp; But no mechanical switch is perfect, and the typical 6mm x 6mm tactile switch PCB-mount switch ubiquitous in consumer electronics seems to routinely switch not-so-cleanly, causing multiple pulses instead of a single edge, particularly as pressure is removed from the switch as it returns to "open" position.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there a pre-existing primer on dealing with this issue in in the MCU realm?&amp;nbsp; I'm new.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So far I've implemented a timer that simply skips the interrupt routine if it is called within 250 ms of a previous interrupt.&amp;nbsp; This works sometimes, but sometimes the user holds the button down longer than 250 ms, and increasing to 500 ms is bad for usability, because people want to click faster than that.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Patrick&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Feb 2008 14:14:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Mitigating-Double-Interrupt-Using-Mechanical-Switch-and-IRQ-KBI/m-p/192593#M14869</guid>
      <dc:creator>PatrickW</dc:creator>
      <dc:date>2008-02-21T14:14:37Z</dc:date>
    </item>
    <item>
      <title>Re: Mitigating Double Interrupt Using Mechanical Switch and IRQ / KBI</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Mitigating-Double-Interrupt-Using-Mechanical-Switch-and-IRQ-KBI/m-p/192594#M14870</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Hello Patrick,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;There should be numerous discussions on this forum - perhaps try the forum search engine at the bottom of this page.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;It may be possible to use polling of the pin to which the pushbutton is connected.&amp;nbsp; However, assuming that you use the KBI module, perhaps to provide wake-up from STOP mode, you might consider the following sequence of events.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;OL&gt;&lt;LI&gt;&lt;FONT size="2"&gt;Within the KBI ISR code:&lt;BR /&gt;&lt;/FONT&gt;&lt;FONT size="2"&gt;Check which switch is active (if more than one), and start a debounce timeout period for that switch, and initiate the action required for the keypress.&amp;nbsp; Disable further interrupts for that input, clear the interrupt flag, and exit the ISR.&amp;nbsp; Incidently, a debounce period of 50 ms will probably be adequate for most tactile switches.&lt;/FONT&gt;&lt;/LI&gt;&lt;LI&gt;&lt;FONT size="2"&gt;Monitor the timeout condition, by means of polling, or maybe a timer interrupt.&amp;nbsp; When timeout is detected, test whether the switch is still closed.&lt;/FONT&gt;&lt;/LI&gt;&lt;LI&gt;&lt;FONT size="2"&gt;If not released, commence another timeout period, and continue.&amp;nbsp; If the switch is now open, re-enable the KBI&amp;nbsp;interrupt for the switch input.&lt;/FONT&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;A very simple way to generate the required delay (which does not have to be particularly accurate), is to utilise the overflow condition of the TIM or TPM timer module.&amp;nbsp; The overflow period needs to be short compared with the timeout period, so that multiple overflow events can be counted to determine the timeout.&amp;nbsp; If you have more than one switch, a separate counter might be used for each switch.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Within the timer overflow ISR, each counter could be handled in the following manner -&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Courier New" size="2"&gt;unsigned char count1, count2;&amp;nbsp;&amp;nbsp; // Global counter variables&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Courier New" size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Courier New" size="2"&gt;// Within the ISR code -&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Courier New" size="2"&gt;if (count1)&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Courier New" size="2"&gt;&amp;nbsp;&amp;nbsp; count1--;&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Courier New" size="2"&gt;if (count2)&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Courier New" size="2"&gt;&amp;nbsp;&amp;nbsp; count2--;&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT face="Courier New" size="2"&gt;// etc.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;To&amp;nbsp;start a&amp;nbsp;timeout period, write the requred timeout value to the counter.&amp;nbsp; When timeout&amp;nbsp;has occurred, the counter will become zero, and will remain at zero.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Regards,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Mac&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Feb 2008 15:45:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Mitigating-Double-Interrupt-Using-Mechanical-Switch-and-IRQ-KBI/m-p/192594#M14870</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2008-02-21T15:45:56Z</dc:date>
    </item>
    <item>
      <title>Re: Mitigating Double Interrupt Using Mechanical Switch and IRQ / KBI</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Mitigating-Double-Interrupt-Using-Mechanical-Switch-and-IRQ-KBI/m-p/192595#M14871</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi Patrick,&lt;BR /&gt;&lt;BR /&gt;First of all you need to ask yourself if you really need to use interrupts just to detect a finger operated switch.&lt;BR /&gt;No one will notice if its polled or interrupt.&lt;BR /&gt;Then the basic idea is.&lt;BR /&gt;Detect switch is closed, then mark as maybe closed.&lt;BR /&gt;Re-test after a debounce time.&lt;BR /&gt;If its closed mark as really closed, if open clear the maybe closed.&lt;BR /&gt;Debounce time should be from 15 to 50ms. If you need longer than 50ms get a better switch.&lt;BR /&gt;Simple as that!&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Feb 2008 16:08:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Mitigating-Double-Interrupt-Using-Mechanical-Switch-and-IRQ-KBI/m-p/192595#M14871</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2008-02-21T16:08:53Z</dc:date>
    </item>
    <item>
      <title>Re: Mitigating Double Interrupt Using Mechanical Switch and IRQ / KBI</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Mitigating-Double-Interrupt-Using-Mechanical-Switch-and-IRQ-KBI/m-p/192596#M14872</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Peg and Mac:&lt;BR /&gt;&lt;BR /&gt;Thanks very much for your help.&amp;nbsp; I knew it had to be an old question, but my searches weren't turning up anything.&amp;nbsp; Now I know the words you folks use, like "debounce," and I can phrase a decent search.&amp;nbsp; Your explanations are full and clear enough that I don't need to, however.&lt;BR /&gt;&lt;BR /&gt;Thanks,&lt;BR /&gt;Patrick&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Feb 2008 16:44:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Mitigating-Double-Interrupt-Using-Mechanical-Switch-and-IRQ-KBI/m-p/192596#M14872</guid>
      <dc:creator>PatrickW</dc:creator>
      <dc:date>2008-02-21T16:44:39Z</dc:date>
    </item>
  </channel>
</rss>