<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Program/Erase Flash Using LAP register on QE128/64</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Program-Erase-Flash-Using-LAP-register-on-QE128-64/m-p/192365#M14828</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am trying to erase/program the flash on the QE164 device. For either operation I need to write to a flash memory location before I launch the command. I write to a flash location by using the linear address pointer registers LAP[2:0] defined in the QE128 Reference Manual at paragraph 4.4.2.2. I am not getting the results I want evidently.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What is the value to write in the LAP[2:0] registers for each page I want to program/erase?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I thought I had to write a value in the range 0xP8000- 0xPBFFF (where P is the PPAGE of flash I want to access from 0 to 3 on the QE64). So if wanted to write to flash location 0x2080 I would have to write the value 0x0A080 in the LAP registers.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What is it that I don't understand?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you all!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 15 Apr 2010 22:51:38 GMT</pubDate>
    <dc:creator>pbouf</dc:creator>
    <dc:date>2010-04-15T22:51:38Z</dc:date>
    <item>
      <title>Program/Erase Flash Using LAP register on QE128/64</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Program-Erase-Flash-Using-LAP-register-on-QE128-64/m-p/192365#M14828</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am trying to erase/program the flash on the QE164 device. For either operation I need to write to a flash memory location before I launch the command. I write to a flash location by using the linear address pointer registers LAP[2:0] defined in the QE128 Reference Manual at paragraph 4.4.2.2. I am not getting the results I want evidently.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What is the value to write in the LAP[2:0] registers for each page I want to program/erase?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I thought I had to write a value in the range 0xP8000- 0xPBFFF (where P is the PPAGE of flash I want to access from 0 to 3 on the QE64). So if wanted to write to flash location 0x2080 I would have to write the value 0x0A080 in the LAP registers.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What is it that I don't understand?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you all!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Apr 2010 22:51:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Program-Erase-Flash-Using-LAP-register-on-QE128-64/m-p/192365#M14828</guid>
      <dc:creator>pbouf</dc:creator>
      <dc:date>2010-04-15T22:51:38Z</dc:date>
    </item>
    <item>
      <title>Re: Program/Erase Flash Using LAP register on QE128/64</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Program-Erase-Flash-Using-LAP-register-on-QE128-64/m-p/192366#M14829</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;FONT face="Arial, Helvetica, sans-serif" size="2"&gt;Hi,&lt;BR /&gt;I am also attempting to read and write into PPAGE0,PPAGE2,PPAGE4,PPAGE5,PPAGE6 and PPAGE7 using assembly, I am able to write into Linear Address Pointer Registers 2:0 (LAP2:LAP0). However, I am not able to do so with Linear Byte Register (LB).&lt;BR /&gt;&lt;BR /&gt;The LB register appears to be READ_ONLY, is there a document of an asm set up routine for this?&amp;nbsp;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="Arial, Helvetica, sans-serif" size="2"&gt;&lt;BR /&gt;Thanks.&lt;/FONT&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 24 Apr 2010 23:01:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Program-Erase-Flash-Using-LAP-register-on-QE128-64/m-p/192366#M14829</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2010-04-24T23:01:27Z</dc:date>
    </item>
  </channel>
</rss>