<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックLocating varibles in flash. MC9RS08KA2</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Locating-varibles-in-flash-MC9RS08KA2/m-p/191868#M14760</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I´m using&amp;nbsp; MC9RS08KA2 with codewarrior&amp;nbsp; 6.3. The RAM memory in MC9RS08KA2 is only 64 bytes so i need to store some only read varibles in the flash memory. how can i program it?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have read some messages in the forum but they didn´t help&amp;nbsp; me.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Some body can help me?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you very much.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 Apr 2010 18:29:23 GMT</pubDate>
    <dc:creator>josep</dc:creator>
    <dc:date>2010-04-14T18:29:23Z</dc:date>
    <item>
      <title>Locating varibles in flash. MC9RS08KA2</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Locating-varibles-in-flash-MC9RS08KA2/m-p/191868#M14760</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I´m using&amp;nbsp; MC9RS08KA2 with codewarrior&amp;nbsp; 6.3. The RAM memory in MC9RS08KA2 is only 64 bytes so i need to store some only read varibles in the flash memory. how can i program it?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have read some messages in the forum but they didn´t help&amp;nbsp; me.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Some body can help me?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you very much.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Apr 2010 18:29:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Locating-varibles-in-flash-MC9RS08KA2/m-p/191868#M14760</guid>
      <dc:creator>josep</dc:creator>
      <dc:date>2010-04-14T18:29:23Z</dc:date>
    </item>
    <item>
      <title>Re: Locating variables in flash. MC9RS08KA2</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Locating-varibles-in-flash-MC9RS08KA2/m-p/191869#M14761</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;To get read only variables allocated in Flash , just define them as constants with the const keyword.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Example&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;const int myTab[4] = {0x123, 0x4567, 0x6789, 0x89AB};&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Apr 2010 20:00:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Locating-varibles-in-flash-MC9RS08KA2/m-p/191869#M14761</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2010-04-14T20:00:34Z</dc:date>
    </item>
  </channel>
</rss>