<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: MC9S08SH8 with 20MHz bus clock???</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08SH8-with-20MHz-bus-clock/m-p/191659#M14755</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello Roger,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;From the datasheet, it would appear that the trimmed frequency range for the internal reference must lie within the limits 31.25kHz to 39.0625kHz.&amp;nbsp; I would presume that trimming&amp;nbsp;for operation outside these limits&amp;nbsp;limits would not be guaranteed.&amp;nbsp; Therefore, the corresponding frequency range of the DCO would be 32 to 40MHz.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The bus frequency will depend on the BDIV setting.&amp;nbsp; For the reset default division by 2, the bus frequency range would be 8-10MHz.&amp;nbsp; If the BDIV setting is changed to division by 1, the bus frequency range would be 16-20MHz.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I would make two observations -&lt;/DIV&gt;&lt;OL&gt;&lt;LI&gt;A bus frequency of 12MHz is not&amp;nbsp;valid&amp;nbsp;using the internal reference.&lt;/LI&gt;&lt;LI&gt;If the BDIV setting is changed from 2 to 1, this should be done after frequency trimming has taken place within the above frequency&amp;nbsp;limits.&amp;nbsp; Otherwise the maximum bus frequency limit may be exceeded.&lt;/LI&gt;&lt;/OL&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Mac&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 Oct 2008 19:37:03 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2008-10-07T19:37:03Z</dc:date>
    <item>
      <title>MC9S08SH8 with 20MHz bus clock???</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08SH8-with-20MHz-bus-clock/m-p/191658#M14754</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello,&lt;/DIV&gt;&lt;DIV&gt;The flyleaf page of the MC9S08SH8 data book says that with the internal clock source the MPU should "support bus frequencies from 2 MHz to 20 MHz".&amp;nbsp; When I tried setting the ICSTRM to get 20 or 16 MHz the chip failed.&amp;nbsp; No problem setting to 8 MHz.&amp;nbsp; When I tried to load a simple test program into the chip at a 12 MHz it seemed to work.&amp;nbsp; At 8 MHz the ICSTRM value for this particular chip was $BC and to get 12 MHz the value need was $3E.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The little test program&amp;nbsp; sends out a message at 9600 baud and blinks a LED works at 12 MHz but now I can no longer communicate with the chip with my OSBDM.&amp;nbsp; Does anyone have any idea why that may be?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Has anyone got the faster bus frequencies with the SH8?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Roger&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Oct 2008 21:14:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08SH8-with-20MHz-bus-clock/m-p/191658#M14754</guid>
      <dc:creator>RogerSchaefer</dc:creator>
      <dc:date>2008-10-06T21:14:30Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08SH8 with 20MHz bus clock???</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08SH8-with-20MHz-bus-clock/m-p/191659#M14755</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello Roger,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;From the datasheet, it would appear that the trimmed frequency range for the internal reference must lie within the limits 31.25kHz to 39.0625kHz.&amp;nbsp; I would presume that trimming&amp;nbsp;for operation outside these limits&amp;nbsp;limits would not be guaranteed.&amp;nbsp; Therefore, the corresponding frequency range of the DCO would be 32 to 40MHz.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The bus frequency will depend on the BDIV setting.&amp;nbsp; For the reset default division by 2, the bus frequency range would be 8-10MHz.&amp;nbsp; If the BDIV setting is changed to division by 1, the bus frequency range would be 16-20MHz.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I would make two observations -&lt;/DIV&gt;&lt;OL&gt;&lt;LI&gt;A bus frequency of 12MHz is not&amp;nbsp;valid&amp;nbsp;using the internal reference.&lt;/LI&gt;&lt;LI&gt;If the BDIV setting is changed from 2 to 1, this should be done after frequency trimming has taken place within the above frequency&amp;nbsp;limits.&amp;nbsp; Otherwise the maximum bus frequency limit may be exceeded.&lt;/LI&gt;&lt;/OL&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Mac&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Oct 2008 19:37:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08SH8-with-20MHz-bus-clock/m-p/191659#M14755</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2008-10-07T19:37:03Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08SH8 with 20MHz bus clock???</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08SH8-with-20MHz-bus-clock/m-p/191660#M14756</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Thanks Mac,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I had forgotten about BDIV.&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I had a S08SH8 running at 8 MHz and I changed BDIV to divide by 1.&amp;nbsp; The bus speed jumped to 16 MHz.&amp;nbsp; I knew this because I had to change my terminal program from 9600 to 19200.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;So to get 20 MHz the thing to do is set my trim program to find the proper trim at 10 MHz then change BDIV in the application program.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Roger&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;PS&amp;nbsp; It wouldn't hurt Freescale to put in a few example programs in their data books&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Oct 2008 21:33:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08SH8-with-20MHz-bus-clock/m-p/191660#M14756</guid>
      <dc:creator>RogerSchaefer</dc:creator>
      <dc:date>2008-10-07T21:33:27Z</dc:date>
    </item>
  </channel>
</rss>