<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MC13192 and CRC calculation question in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC13192-and-CRC-calculation-question/m-p/191455#M14733</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Besides the CRC calculation question, i could solve the TX an RX problem.&lt;/P&gt;&lt;P&gt;The issue was on the TX routine. The last 2 bytes of the recursive SPI must be Dummy and then the Character. I was sending first the Character and then the Dummy.&lt;/P&gt;&lt;P&gt;Gustavo.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 23 Jan 2012 10:13:52 GMT</pubDate>
    <dc:creator>GusPS</dc:creator>
    <dc:date>2012-01-23T10:13:52Z</dc:date>
    <item>
      <title>MC13192 and CRC calculation question</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC13192-and-CRC-calculation-question/m-p/191454#M14732</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Reading the MC13192RM I coulnd't find the details about the CRC calculation used on every TX of the MC13192 chip.&lt;/P&gt;&lt;P&gt;I'm having an issue with TX and RX with odd packets. Even packets are fine, but surely some bug is in the odd routine I made, and if I could know how the CRC is calculated it can help me to track down the problem.&lt;/P&gt;&lt;P&gt;I'm sending from&amp;nbsp;a node, for example, four bytes as the payload: "PEPE". The other node receving this payload reports that CRC is 0x5891.&lt;/P&gt;&lt;P&gt;So, I went to&amp;nbsp;&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.lammertbies.nl%2Fcomm%2Finfo%2Fcrc-calculation.html" rel="nofollow" target="_blank"&gt;http://www.lammertbies.nl/comm/info/crc-calculation.html&lt;/A&gt;&amp;nbsp;and typed "PEPE", and any result is not equal to 0x5891.&lt;/P&gt;&lt;P&gt;The problem with odds packets is that sending for example "GUSTAVO", I'm receving "GUSTAVA", with a CRC = to 0x4E31. So, I would like to use the CRC to help me check to determine is the error is in the TX routine or the RX routine.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If anyone has deatils about the CRC calculation used in MC13192, please let me know.&lt;/P&gt;&lt;P&gt;Thank you very much.&lt;/P&gt;&lt;P&gt;Gustavo.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Dec 2011 20:44:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC13192-and-CRC-calculation-question/m-p/191454#M14732</guid>
      <dc:creator>GusPS</dc:creator>
      <dc:date>2011-12-20T20:44:59Z</dc:date>
    </item>
    <item>
      <title>Re: MC13192 and CRC calculation question</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC13192-and-CRC-calculation-question/m-p/191455#M14733</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Besides the CRC calculation question, i could solve the TX an RX problem.&lt;/P&gt;&lt;P&gt;The issue was on the TX routine. The last 2 bytes of the recursive SPI must be Dummy and then the Character. I was sending first the Character and then the Dummy.&lt;/P&gt;&lt;P&gt;Gustavo.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Jan 2012 10:13:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC13192-and-CRC-calculation-question/m-p/191455#M14733</guid>
      <dc:creator>GusPS</dc:creator>
      <dc:date>2012-01-23T10:13:52Z</dc:date>
    </item>
  </channel>
</rss>