<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: HCS08 : 9S08QG8 + RDIV in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-9S08QG8-RDIV/m-p/190860#M14622</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;I don't think you should use RDIV in this manner.&lt;BR /&gt;If you set it to 2, this results in a Divided ref. clock frequency is 15.625K which is not in spec.&lt;BR /&gt;(31.25/2). If set to 4 7.815K etc.&lt;BR /&gt;&lt;BR /&gt;So it must remain at 1 in this mode.&lt;BR /&gt;&lt;BR /&gt;You can use the BDIV bits in in ICSC2 to divide down the resulting 8Mhz bus clock if you want a lower clock.&lt;BR /&gt;&lt;BR /&gt;If you want to experiment with these settings, use Processor Expert in Device Initialization mode.&lt;BR /&gt;Click on CPU. Then you can experiment with different settings. PE will tell you when you are wrong.&lt;BR /&gt;&lt;BR /&gt;&lt;B&gt;"If FLL is enabled (FLL mode property is set to 'Engaged' or 'Bypassed Low Power') , this frequency shall be in range of 31.25 kHz to 39.0625 kHz. This property cannot by directly modified if FLL is engaged."&lt;/B&gt;&lt;BR /&gt;(Means leave RDIV alone).&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Message Edited by JimDon on &lt;SPAN class="date_text"&gt;2008-02-19&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;10:44 AM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 Feb 2008 23:43:50 GMT</pubDate>
    <dc:creator>JimDon</dc:creator>
    <dc:date>2008-02-19T23:43:50Z</dc:date>
    <item>
      <title>HCS08 : 9S08QG8 + RDIV</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-9S08QG8-RDIV/m-p/190856#M14618</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I'm&amp;nbsp;currently starting with the HCS08 family and I have a question about the ICS module. (Internal Clock Source)&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;After a reset, the operating mode of the ICS module is set as FLL engaged Internal (FEI).&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I would like to know if I can use the RDIV bits of ICSC1 register in the FEI mode ? How does the RDIV bits works in the FEI mode ?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Is that right to say the following ? :&lt;/DIV&gt;&lt;DIV&gt;RDIV = 000&amp;nbsp;-&amp;gt; fIRC = 31.25 k Hz&lt;/DIV&gt;&lt;DIV&gt;RDIV = 001 -&amp;gt; fIRC =&amp;nbsp;32.37 k Hz&lt;/DIV&gt;&lt;DIV&gt;RDIV = 010 -&amp;gt; fIRC =&amp;nbsp;33.48 k Hz&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;RDIV = 011 -&amp;gt; fIRC =&amp;nbsp;34.60 k Hz&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;RDIV = 100 -&amp;gt; fIRC =&amp;nbsp;35.71 k Hz&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;RDIV = 101 -&amp;gt; fIRC =&amp;nbsp;36.830 k Hz&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;RDIV = 110 -&amp;gt; fIRC =&amp;nbsp;37.95 k Hz&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;RDIV = 111 -&amp;gt; fIRC =&amp;nbsp;39.0625 k Hz&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Where&amp;nbsp;each bit of RDIV&amp;nbsp;adds : (39.0625 k - 31.25 k) / 7 = 1.11 K Hz&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Note :&lt;/DIV&gt;&lt;DIV&gt;The definition of the RDIV from the datasheet is :&lt;/DIV&gt;&lt;DIV&gt;Reference Divider — Selects the amount to divide down the FLL reference clock selected by the IREFS bits. Resulting frequency must be in the range 31.25 kHz to 39.0625 kHz.&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks for your answer.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Feb 2008 13:47:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-9S08QG8-RDIV/m-p/190856#M14618</guid>
      <dc:creator>ssinfod</dc:creator>
      <dc:date>2008-02-19T13:47:54Z</dc:date>
    </item>
    <item>
      <title>Re: HCS08 : 9S08QG8 + RDIV</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-9S08QG8-RDIV/m-p/190857#M14619</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi,&lt;/DIV&gt;&lt;DIV&gt;The values in the regisers are setup at powerup to generate a fBUS clock of about 4 MHz.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Ake&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Feb 2008 16:35:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-9S08QG8-RDIV/m-p/190857#M14619</guid>
      <dc:creator>Ake</dc:creator>
      <dc:date>2008-02-19T16:35:55Z</dc:date>
    </item>
    <item>
      <title>Re: HCS08 : 9S08QG8 + RDIV</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-9S08QG8-RDIV/m-p/190858#M14620</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Hello,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;My understanding is that variation of RDIV would be applicable to FEE mode, where a higher frequency crystal might be used.&amp;nbsp; The RDIV value should be selected so that the resulting frequency applied to the FLL is within the range 31.25 to 39.0625 kHz.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;For example, if you wish to use a 4.00 MHz crystal, the division ratio would need to be 128 (RDIV = 7).&amp;nbsp; This would produce a reference frequency of 31.25 kHz, and a bus frequency of 8 MHz, or a sub-multiple, depending on the BDIV setting.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Regards,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Mac&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Feb 2008 22:21:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-9S08QG8-RDIV/m-p/190858#M14620</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2008-02-19T22:21:45Z</dc:date>
    </item>
    <item>
      <title>Re: HCS08 : 9S08QG8 + RDIV</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-9S08QG8-RDIV/m-p/190859#M14621</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I agree with MAC.&lt;BR /&gt;&lt;BR /&gt;Regarding to &lt;FONT size="2"&gt;the range from 31.25 to 39.0625 kHz, note that it is actually trimmed using the ICSTRM register and the FTRIM bit.&lt;BR /&gt;&lt;BR /&gt;The RDIV is the reference dividing factor and can be 1, 2, 4, 8, 16, 32, 64 or 128.&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;&lt;/FONT&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Feb 2008 23:14:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-9S08QG8-RDIV/m-p/190859#M14621</guid>
      <dc:creator>fabio</dc:creator>
      <dc:date>2008-02-19T23:14:05Z</dc:date>
    </item>
    <item>
      <title>Re: HCS08 : 9S08QG8 + RDIV</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-9S08QG8-RDIV/m-p/190860#M14622</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;I don't think you should use RDIV in this manner.&lt;BR /&gt;If you set it to 2, this results in a Divided ref. clock frequency is 15.625K which is not in spec.&lt;BR /&gt;(31.25/2). If set to 4 7.815K etc.&lt;BR /&gt;&lt;BR /&gt;So it must remain at 1 in this mode.&lt;BR /&gt;&lt;BR /&gt;You can use the BDIV bits in in ICSC2 to divide down the resulting 8Mhz bus clock if you want a lower clock.&lt;BR /&gt;&lt;BR /&gt;If you want to experiment with these settings, use Processor Expert in Device Initialization mode.&lt;BR /&gt;Click on CPU. Then you can experiment with different settings. PE will tell you when you are wrong.&lt;BR /&gt;&lt;BR /&gt;&lt;B&gt;"If FLL is enabled (FLL mode property is set to 'Engaged' or 'Bypassed Low Power') , this frequency shall be in range of 31.25 kHz to 39.0625 kHz. This property cannot by directly modified if FLL is engaged."&lt;/B&gt;&lt;BR /&gt;(Means leave RDIV alone).&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Message Edited by JimDon on &lt;SPAN class="date_text"&gt;2008-02-19&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;10:44 AM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Feb 2008 23:43:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-9S08QG8-RDIV/m-p/190860#M14622</guid>
      <dc:creator>JimDon</dc:creator>
      <dc:date>2008-02-19T23:43:50Z</dc:date>
    </item>
  </channel>
</rss>