<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRS08 flash protect</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/RS08-flash-protect/m-p/190487#M14595</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I have a working RS08 project that needs to be released to production. Looking at the data sheet I need to set FOPT. Because this is tied to flash should it be set in my code (c) or as part of the programming?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 16 Dec 2011 02:58:29 GMT</pubDate>
    <dc:creator>barbercolman</dc:creator>
    <dc:date>2011-12-16T02:58:29Z</dc:date>
    <item>
      <title>RS08 flash protect</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/RS08-flash-protect/m-p/190487#M14595</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I have a working RS08 project that needs to be released to production. Looking at the data sheet I need to set FOPT. Because this is tied to flash should it be set in my code (c) or as part of the programming?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Dec 2011 02:58:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/RS08-flash-protect/m-p/190487#M14595</guid>
      <dc:creator>barbercolman</dc:creator>
      <dc:date>2011-12-16T02:58:29Z</dc:date>
    </item>
    <item>
      <title>Re: RS08 flash protect</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/RS08-flash-protect/m-p/190488#M14596</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You actually need to program the location NVOPT in flash memory.&amp;nbsp; Whenever a reset occurs, this value is automatically written to FOPT.&amp;nbsp; If your programming tool is capable of separately programming NVOPT, this method can be used.&amp;nbsp; However, this register can alternatively&amp;nbsp;be cleared as part of the normal MCU flash programming procedure.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If the latter method is used, this is one less process that can potentially be forgotten during production.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If using the internal reference oscillator, calibration of the trim value is another process required during programming.&amp;nbsp; Your code might include a check that this has been done, and to&amp;nbsp;provide some sort of external error indication during production testing, if&amp;nbsp;forgotten.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Dec 2011 10:29:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/RS08-flash-protect/m-p/190488#M14596</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2011-12-16T10:29:56Z</dc:date>
    </item>
  </channel>
</rss>