<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックCommunication problem with  DEMO09S08QG8 board</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Communication-problem-with-DEMO09S08QG8-board/m-p/190357#M14586</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I got a DEMO09S08QG8 board and I already programmed a M9S08QG8 chip using the&amp;nbsp;integrated USB-to-BDM interface&amp;nbsp;of the board in an external target. Now I want to do the same with a MC9S08SE8CRL chip but there is no communiation with the target when I run the debug mode in CodeWarrior V6.3.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My question is, what I need to change in the board configuration? Could it be the 3.3V power of the BDM Port and change it for an external 5v power??&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thak you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 11 Mar 2011 03:56:10 GMT</pubDate>
    <dc:creator>israel_voli</dc:creator>
    <dc:date>2011-03-11T03:56:10Z</dc:date>
    <item>
      <title>Communication problem with  DEMO09S08QG8 board</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Communication-problem-with-DEMO09S08QG8-board/m-p/190357#M14586</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I got a DEMO09S08QG8 board and I already programmed a M9S08QG8 chip using the&amp;nbsp;integrated USB-to-BDM interface&amp;nbsp;of the board in an external target. Now I want to do the same with a MC9S08SE8CRL chip but there is no communiation with the target when I run the debug mode in CodeWarrior V6.3.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My question is, what I need to change in the board configuration? Could it be the 3.3V power of the BDM Port and change it for an external 5v power??&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thak you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Mar 2011 03:56:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Communication-problem-with-DEMO09S08QG8-board/m-p/190357#M14586</guid>
      <dc:creator>israel_voli</dc:creator>
      <dc:date>2011-03-11T03:56:10Z</dc:date>
    </item>
    <item>
      <title>Re: Communication problem with  DEMO09S08QG8 board</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Communication-problem-with-DEMO09S08QG8-board/m-p/190358#M14587</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello and welcome to the fora,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In the interest of making more money this sort of functionality has been disabled.&lt;/P&gt;&lt;P&gt;Refer to&lt;A href="https://community.freescale.com/message/49272#49272" title="https://community.freescale.com/message/49272#49272"&gt;https://community.freescale.com/message/49272#49272&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Mar 2011 04:37:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Communication-problem-with-DEMO09S08QG8-board/m-p/190358#M14587</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2011-03-11T04:37:28Z</dc:date>
    </item>
  </channel>
</rss>