<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: Adding an LCD to a SRB</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Adding-an-LCD-to-a-SRB/m-p/190268#M14565</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;You can use PTB port for connecting a LCD display to SRB board (pins 19 - 26 on J103 connector). NCB board use the same port for connecting LCD display.&lt;BR /&gt;&lt;BR /&gt;Adrian&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Feb 2008 23:31:35 GMT</pubDate>
    <dc:creator>addiyi</dc:creator>
    <dc:date>2008-02-21T23:31:35Z</dc:date>
    <item>
      <title>Adding an LCD to a SRB</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Adding-an-LCD-to-a-SRB/m-p/190266#M14563</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;We are using the MC13213 EVK (1x NCB 2xSRBs) to&amp;nbsp;design a wireless secuity system for our building.&lt;/DIV&gt;&lt;DIV&gt;We will need to add an LCD to the SRBs is this possible w/o adding more circuitry besides the LCD? Or do will we need to add additional driver chips?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 16 Feb 2008 06:58:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Adding-an-LCD-to-a-SRB/m-p/190266#M14563</guid>
      <dc:creator>flyingasics</dc:creator>
      <dc:date>2008-02-16T06:58:07Z</dc:date>
    </item>
    <item>
      <title>Re: Adding an LCD to a SRB</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Adding-an-LCD-to-a-SRB/m-p/190267#M14564</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;If you have 6 outputs left, you can use a "standard" 16x2, 20x3 &lt;A href="http://www.sparkfun.com/commerce/product_info.php?products_id=256" rel="nofollow" target="_blank"&gt;20x4&lt;/A&gt; LCD.&lt;BR /&gt;The link shows one from sparkfun. There are very common.&lt;BR /&gt;You can also get it with a serial interface if you have a port left.&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 16 Feb 2008 08:04:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Adding-an-LCD-to-a-SRB/m-p/190267#M14564</guid>
      <dc:creator>JimDon</dc:creator>
      <dc:date>2008-02-16T08:04:19Z</dc:date>
    </item>
    <item>
      <title>Re: Adding an LCD to a SRB</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Adding-an-LCD-to-a-SRB/m-p/190268#M14565</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;You can use PTB port for connecting a LCD display to SRB board (pins 19 - 26 on J103 connector). NCB board use the same port for connecting LCD display.&lt;BR /&gt;&lt;BR /&gt;Adrian&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Feb 2008 23:31:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Adding-an-LCD-to-a-SRB/m-p/190268#M14565</guid>
      <dc:creator>addiyi</dc:creator>
      <dc:date>2008-02-21T23:31:35Z</dc:date>
    </item>
  </channel>
</rss>