<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックAW60 RTI with external crystal - does it work ?</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AW60-RTI-with-external-crystal-does-it-work/m-p/127711#M1454</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;SPAN style="font-family: Verdana; font-size: 2;"&gt;Does anyone have any experience in getting the RTI to work with the external crystal (32k specifically) on the AW60?&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN style="font-family: Verdana; font-size: 2;"&gt;We can't seem to get the AW60's RTI&amp;nbsp;create any periodic interrupts with the external crystal, the internal clock source seems to work. I'm using CW5. Any response yae or ney would be helpful.&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN style="font-family: Verdana; font-size: 2;"&gt;Thanks in advance...&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN style="font-family: Verdana; font-size: 2;"&gt;Sundar&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Mar 2006 03:31:54 GMT</pubDate>
    <dc:creator>Caligold</dc:creator>
    <dc:date>2006-03-02T03:31:54Z</dc:date>
    <item>
      <title>AW60 RTI with external crystal - does it work ?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AW60-RTI-with-external-crystal-does-it-work/m-p/127711#M1454</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;SPAN style="font-family: Verdana; font-size: 2;"&gt;Does anyone have any experience in getting the RTI to work with the external crystal (32k specifically) on the AW60?&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN style="font-family: Verdana; font-size: 2;"&gt;We can't seem to get the AW60's RTI&amp;nbsp;create any periodic interrupts with the external crystal, the internal clock source seems to work. I'm using CW5. Any response yae or ney would be helpful.&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN style="font-family: Verdana; font-size: 2;"&gt;Thanks in advance...&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN style="font-family: Verdana; font-size: 2;"&gt;Sundar&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Mar 2006 03:31:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AW60-RTI-with-external-crystal-does-it-work/m-p/127711#M1454</guid>
      <dc:creator>Caligold</dc:creator>
      <dc:date>2006-03-02T03:31:54Z</dc:date>
    </item>
    <item>
      <title>Re: AW60 RTI with external crystal - does it work ?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AW60-RTI-with-external-crystal-does-it-work/m-p/127712#M1455</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi:&lt;BR /&gt;&lt;BR /&gt;Do you have the External Clock available and active, as the datasheet specifies?&lt;BR /&gt;&lt;BR /&gt;Which divider are you using (this will set up the interrupt timing)?&lt;BR /&gt;&lt;BR /&gt;Are you in run mode or wait, or stop modes?&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;&lt;BR /&gt;Alex&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Mar 2006 06:19:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AW60-RTI-with-external-crystal-does-it-work/m-p/127712#M1455</guid>
      <dc:creator>alex_spotw</dc:creator>
      <dc:date>2006-03-02T06:19:48Z</dc:date>
    </item>
    <item>
      <title>Re: AW60 RTI with external crystal - does it work ?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AW60-RTI-with-external-crystal-does-it-work/m-p/127713#M1456</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;&lt;FONT face="Verdana" size="2"&gt;Hi Alex,&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Verdana" size="2"&gt;Yes, I do have an external crystal (32.768k) and it is set active. The prescalar (divider) is set to 16384 to get a 500ms interrupt. I am in run mode.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Verdana" size="2"&gt;Neither any of the FAEs or anyone I know can get it to work on any board. I would like to know if there are any secrets or if anyone has got it to work yet !!&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Verdana" size="2"&gt;Have you used the AW60's RTI ? I can get the GB60's RTI to work without much of a problem...&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Verdana" size="2"&gt;Thanks,&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Verdana" size="2"&gt;Sundar&lt;/FONT&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Mar 2006 11:16:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AW60-RTI-with-external-crystal-does-it-work/m-p/127713#M1456</guid>
      <dc:creator>Caligold</dc:creator>
      <dc:date>2006-03-02T11:16:09Z</dc:date>
    </item>
    <item>
      <title>Re: AW60 RTI with external crystal - does it work ?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AW60-RTI-with-external-crystal-does-it-work/m-p/127714#M1457</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi Sundar:&lt;BR /&gt;&lt;BR /&gt;I have a GT60 running the RTI from the External Clock in run mode, no problem. However, in the GT60, it does not run from the Internal Clock in Run mode.&lt;BR /&gt;&lt;BR /&gt;I don't have access to a AW60 to verify it is not running from the external clock, though.&lt;BR /&gt;&lt;BR /&gt;Did you check the erratas for the AW60 mask that you're using? It might be that it doesn't run from the External Clock due to a problem in the mask.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;&lt;BR /&gt;Alex R.&lt;P&gt;Message Edited by alex_spotw on &lt;SPAN class="date_text"&gt;03-02-2006&lt;/SPAN&gt;&lt;SPAN class="time_text"&gt;09:44 AM&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Mar 2006 23:43:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AW60-RTI-with-external-crystal-does-it-work/m-p/127714#M1457</guid>
      <dc:creator>alex_spotw</dc:creator>
      <dc:date>2006-03-02T23:43:16Z</dc:date>
    </item>
  </channel>
</rss>