<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 9S08AC16 Temperature Sensor Voltage</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08AC16-Temperature-Sensor-Voltage/m-p/190019#M14507</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;SPAN&gt;Hi All&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I've just migrated up from an 08QG8 to an 08AC16 part and was wondering why i was getting wildly inaccurate temperature readings from the internal temperature sensor using imported 08QG8 code.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Anyway, i found out the reason - there's been a subtle change in the temperature sensor reference voltage @25°C from 0.7012 to 1.41mV.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;However, the footnote for this value states "Typical values assume VDDAD = 5.0V, Temp = 25C, fADCK=1.0 MHz unless otherwise stated. Typical values are for reference only and are not tested in production".&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So my question is this, has this value been definitively determined yet for various values of VCC&amp;nbsp; etc. I based my original 08QG8 code around AN3031, unfortunately, this now appears obsolete for 08AC16 use.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Gary&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 01 Oct 2008 20:31:45 GMT</pubDate>
    <dc:creator>airbusboy</dc:creator>
    <dc:date>2008-10-01T20:31:45Z</dc:date>
    <item>
      <title>9S08AC16 Temperature Sensor Voltage</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08AC16-Temperature-Sensor-Voltage/m-p/190019#M14507</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;SPAN&gt;Hi All&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I've just migrated up from an 08QG8 to an 08AC16 part and was wondering why i was getting wildly inaccurate temperature readings from the internal temperature sensor using imported 08QG8 code.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Anyway, i found out the reason - there's been a subtle change in the temperature sensor reference voltage @25°C from 0.7012 to 1.41mV.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;However, the footnote for this value states "Typical values assume VDDAD = 5.0V, Temp = 25C, fADCK=1.0 MHz unless otherwise stated. Typical values are for reference only and are not tested in production".&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So my question is this, has this value been definitively determined yet for various values of VCC&amp;nbsp; etc. I based my original 08QG8 code around AN3031, unfortunately, this now appears obsolete for 08AC16 use.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Gary&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Oct 2008 20:31:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08AC16-Temperature-Sensor-Voltage/m-p/190019#M14507</guid>
      <dc:creator>airbusboy</dc:creator>
      <dc:date>2008-10-01T20:31:45Z</dc:date>
    </item>
    <item>
      <title>Re: 9S08AC16 Temperature Sensor Voltage</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08AC16-Temperature-Sensor-Voltage/m-p/190020#M14508</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello Gary,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The temperature sensor for the 'QG8 consists of a single diode, presumably&amp;nbsp;fed by a constant current source.&amp;nbsp; The voltage drop across the diode is measured.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;For the 'AC16 device, it would be reasonable to assume that the sensor now consists of two diodes connected in series, to effectively double the resolution of the temperature measurement.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The calibration processes described in AN3031 should still be applicable to the later device.&amp;nbsp; Note that the variation of the readings&amp;nbsp;for different&amp;nbsp;Vdd voltages, as&amp;nbsp;graphed in the application note,&amp;nbsp;is primarily because of the similar variation of Vref for the ADC module (Vref = Vdd).&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Mac&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Oct 2008 21:22:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08AC16-Temperature-Sensor-Voltage/m-p/190020#M14508</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2008-10-01T21:22:39Z</dc:date>
    </item>
  </channel>
</rss>