<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックXtal frequency, baud rate, in-circuit programming.</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Xtal-frequency-baud-rate-in-circuit-programming/m-p/189976#M14495</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Going to use a HC08 of some description in a new project, and this will have an SMD and use in-circuit programming. I have never done one like this before and the problem is this: I will be using an 8 MHz xtal but for programming, according to the datasheet it needs a 9.8304 MHz xtal for the sake of the correct baud rate between the pc and board. Can I just use my 8 MHz xtal and somehow use a non-standard baud rate or is there some other way?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 13 Dec 2011 10:03:52 GMT</pubDate>
    <dc:creator>JimDandy</dc:creator>
    <dc:date>2011-12-13T10:03:52Z</dc:date>
    <item>
      <title>Xtal frequency, baud rate, in-circuit programming.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Xtal-frequency-baud-rate-in-circuit-programming/m-p/189976#M14495</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Going to use a HC08 of some description in a new project, and this will have an SMD and use in-circuit programming. I have never done one like this before and the problem is this: I will be using an 8 MHz xtal but for programming, according to the datasheet it needs a 9.8304 MHz xtal for the sake of the correct baud rate between the pc and board. Can I just use my 8 MHz xtal and somehow use a non-standard baud rate or is there some other way?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Dec 2011 10:03:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Xtal-frequency-baud-rate-in-circuit-programming/m-p/189976#M14495</guid>
      <dc:creator>JimDandy</dc:creator>
      <dc:date>2011-12-13T10:03:52Z</dc:date>
    </item>
    <item>
      <title>Re: Xtal frequency, baud rate, in-circuit programming.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Xtal-frequency-baud-rate-in-circuit-programming/m-p/189977#M14496</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello JD,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For a new project, I would strongly suggest that you consider using one of the MC9S08 family, in lieu of a MC908 device, which have largely been&amp;nbsp;superceded.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The purchase of a demo board for the selected device will provide programming and debug capability via a USB connection.&amp;nbsp; ICP can usually be achieved with the fitment of an additional header, and 6-way ribbon cable assembly, and the removal of the resident MCU from the demo board (usually socketed).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Other low cost programming/debug solutions are also available from third party sources.&amp;nbsp; Also refer to OSBDM forum.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Dec 2011 23:01:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Xtal-frequency-baud-rate-in-circuit-programming/m-p/189977#M14496</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2011-12-13T23:01:51Z</dc:date>
    </item>
    <item>
      <title>Re: Xtal frequency, baud rate, in-circuit programming.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Xtal-frequency-baud-rate-in-circuit-programming/m-p/189978#M14497</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So the demo board can connect and download to the project board? Okay...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;That might be the simplest thing you have said to anybody all year, but you have no idea how much help that is to me &lt;IMG alt=":smileyhappy:" class="emoticon emoticon-smileyhappy" id="smileyhappy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif" title="Smiley Happy" /&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks a lot Mac&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Dec 2011 07:32:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Xtal-frequency-baud-rate-in-circuit-programming/m-p/189978#M14497</guid>
      <dc:creator>JimDandy</dc:creator>
      <dc:date>2011-12-14T07:32:43Z</dc:date>
    </item>
  </channel>
</rss>