<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Re: MC9s08JM32 clock initialisation</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9s08JM32-clock-initialisation/m-p/189572#M14470</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi pgo,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for the link. Looks like it's what I need.&lt;/P&gt;&lt;P&gt;I'm a bit concerned about the reference to BDM speed. Something else I shall have to check out! I'm using a P&amp;amp;E MultiLink Interface. I've just found it works with a bus speed of up to 35MHz so I should be ok.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Steve&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 12 Jun 2009 13:47:22 GMT</pubDate>
    <dc:creator>stevec</dc:creator>
    <dc:date>2009-06-12T13:47:22Z</dc:date>
    <item>
      <title>MC9s08JM32 clock initialisation</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9s08JM32-clock-initialisation/m-p/189570#M14468</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have just decided to use the JM32 device because of its 24MHz max bus speed and 12 bit A/D, having used the 9S08RE16 device before. I am having problems understanding how to achieve this maximum bus speed. When I was selecting the device I thought it was just a simple job of running off a 48MHz crystal! Can someone point me in the right direction here. I wish to use an external crystal and have all internal processes working off 24MHz. I have tried using Device Initialiser within Codewarrior but to no avail.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Steve&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jun 2009 21:02:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9s08JM32-clock-initialisation/m-p/189570#M14468</guid>
      <dc:creator>stevec</dc:creator>
      <dc:date>2009-06-11T21:02:56Z</dc:date>
    </item>
    <item>
      <title>Re: MC9s08JM32 clock initialisation</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9s08JM32-clock-initialisation/m-p/189571#M14469</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear stevec,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;See this thread for some example code:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="http://forums.freescale.com/freescale/board/message?board.id=8BITCOMM&amp;amp;message.id=13898#M13898" target="test_blank"&gt;http://forums.freescale.com/freescale/board/message?board.id=8BITCOMM&amp;amp;message.id=13898#M13898&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Jun 2009 09:21:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9s08JM32-clock-initialisation/m-p/189571#M14469</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2009-06-12T09:21:43Z</dc:date>
    </item>
    <item>
      <title>Re: MC9s08JM32 clock initialisation</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9s08JM32-clock-initialisation/m-p/189572#M14470</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi pgo,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for the link. Looks like it's what I need.&lt;/P&gt;&lt;P&gt;I'm a bit concerned about the reference to BDM speed. Something else I shall have to check out! I'm using a P&amp;amp;E MultiLink Interface. I've just found it works with a bus speed of up to 35MHz so I should be ok.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Steve&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Jun 2009 13:47:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9s08JM32-clock-initialisation/m-p/189572#M14470</guid>
      <dc:creator>stevec</dc:creator>
      <dc:date>2009-06-12T13:47:22Z</dc:date>
    </item>
  </channel>
</rss>