<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックCommissioning: Startup Control - BeeKit-code and Home Automation Profile differences</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Commissioning-Startup-Control-BeeKit-code-and-Home-Automation/m-p/189410#M14462</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I found a difference between the standard definition of Startup Control from the Home Automation Profile and the implementation by the BeeKit-generated-cod. In this code, in files ApplicationConf.h and ZdoApsInterface.h, the 3 Startup Control mode bit can assume values other than the two ones specified by the ZigBee Document 053520r25. I also found that those values do not refer to the same function: "zero" means the device "will not perform any explicit join or rejoin" by the standard but "0x00" means "use association (ZR, ZED only), or form (ZC)" by the Beekit-generate-code; as the same, "three" means the device "will join network by association when join command is indicated by button press sequence" by the standard but "0x03" means silent join by the code.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm working to implement the commissioning procedure in my BeeKit Codebase 3.0.2 based application, so I need more info about the existing code and the code that I have to add.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;ApplicationConf.h:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;/*&lt;BR /&gt;&amp;nbsp; Start mode to use if this node receives an over-the-air NLME-LEAVE command. See&lt;BR /&gt;&amp;nbsp; ZdoStopMode_t in ApsZdoInterface.h. Note: the restart bit is chosen by the&lt;BR /&gt;&amp;nbsp; over-the-air command, but whether to announce or reset tables is chosen by the&lt;BR /&gt;&amp;nbsp; application. See also ZDO_StartEx().&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp; DDDx xxxx&amp;nbsp;&amp;nbsp; - Device type&lt;BR /&gt;&amp;nbsp; xxxS Sxxx&amp;nbsp;&amp;nbsp; - Startup set&lt;BR /&gt;&amp;nbsp; xxxx xCCC&amp;nbsp;&amp;nbsp; - Startup control mode&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp; Default: 0x02 (NVM set, gZdoStartMode_NwkRejoin_c)&lt;BR /&gt;*/&lt;BR /&gt;#ifndef gZdoStartModeDefault_c&lt;BR /&gt;#define gZdoStartModeDefault_c&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x02&lt;BR /&gt;#endif&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;ZdoApsInterface.h:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;#define gZdoStartMode_Associate_c&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x00 // (default) use association (ZR, ZED only), or form (ZC)&lt;BR /&gt;#define gZdoStartMode_OrphanRejoin_c&amp;nbsp; 0x01 // FS specific: use orphan rejoin (ZR, ZED only)&lt;BR /&gt;#define gZdoStartMode_NwkRejoin_c&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x02 // use NWK rejoin (ZR, ZED only)&lt;BR /&gt;#define gZdoStartMode_FindAndRejoin_c 0x03 // valid for ZR, ZED only, search for network on this and&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // other channels, then silent join&lt;BR /&gt;#define gZdoStartMode_SilentStart_c&amp;nbsp;&amp;nbsp; 0x04 // already part of the network (no form/join needed)&lt;BR /&gt;#define gZdoStartMode_StartMask_c&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x07 // mask for above fields&lt;BR /&gt;&lt;BR /&gt;// form (ZC) or associate join (if ZR or ZED), using NVM if available&lt;BR /&gt;#define gZdoStartMode_Default_c&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (gZdoStartMode_Associate_c | gZdoStartMode_NvmSet_c)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;ZigBee Document 053520r25 (ZIGBEE HOME AUTOMATION PUBLIC APPLICATION PROFILE):&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Startup Control:&lt;BR /&gt;3 (three) if un-commissioned, so it will join network by association when join&lt;BR /&gt;command is indicated by button press sequence.&lt;BR /&gt;0 (Zero) if commissioned. Indicates that the device should consider itself a part of&lt;BR /&gt;the network indicated by the ExtendedPANId attribute. In this case it will not&lt;BR /&gt;perform any explicit join or rejoin operation.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 11 Jun 2009 16:30:31 GMT</pubDate>
    <dc:creator>Devitt</dc:creator>
    <dc:date>2009-06-11T16:30:31Z</dc:date>
    <item>
      <title>Commissioning: Startup Control - BeeKit-code and Home Automation Profile differences</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Commissioning-Startup-Control-BeeKit-code-and-Home-Automation/m-p/189410#M14462</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I found a difference between the standard definition of Startup Control from the Home Automation Profile and the implementation by the BeeKit-generated-cod. In this code, in files ApplicationConf.h and ZdoApsInterface.h, the 3 Startup Control mode bit can assume values other than the two ones specified by the ZigBee Document 053520r25. I also found that those values do not refer to the same function: "zero" means the device "will not perform any explicit join or rejoin" by the standard but "0x00" means "use association (ZR, ZED only), or form (ZC)" by the Beekit-generate-code; as the same, "three" means the device "will join network by association when join command is indicated by button press sequence" by the standard but "0x03" means silent join by the code.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm working to implement the commissioning procedure in my BeeKit Codebase 3.0.2 based application, so I need more info about the existing code and the code that I have to add.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;ApplicationConf.h:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;/*&lt;BR /&gt;&amp;nbsp; Start mode to use if this node receives an over-the-air NLME-LEAVE command. See&lt;BR /&gt;&amp;nbsp; ZdoStopMode_t in ApsZdoInterface.h. Note: the restart bit is chosen by the&lt;BR /&gt;&amp;nbsp; over-the-air command, but whether to announce or reset tables is chosen by the&lt;BR /&gt;&amp;nbsp; application. See also ZDO_StartEx().&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp; DDDx xxxx&amp;nbsp;&amp;nbsp; - Device type&lt;BR /&gt;&amp;nbsp; xxxS Sxxx&amp;nbsp;&amp;nbsp; - Startup set&lt;BR /&gt;&amp;nbsp; xxxx xCCC&amp;nbsp;&amp;nbsp; - Startup control mode&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp; Default: 0x02 (NVM set, gZdoStartMode_NwkRejoin_c)&lt;BR /&gt;*/&lt;BR /&gt;#ifndef gZdoStartModeDefault_c&lt;BR /&gt;#define gZdoStartModeDefault_c&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x02&lt;BR /&gt;#endif&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;ZdoApsInterface.h:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;#define gZdoStartMode_Associate_c&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x00 // (default) use association (ZR, ZED only), or form (ZC)&lt;BR /&gt;#define gZdoStartMode_OrphanRejoin_c&amp;nbsp; 0x01 // FS specific: use orphan rejoin (ZR, ZED only)&lt;BR /&gt;#define gZdoStartMode_NwkRejoin_c&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x02 // use NWK rejoin (ZR, ZED only)&lt;BR /&gt;#define gZdoStartMode_FindAndRejoin_c 0x03 // valid for ZR, ZED only, search for network on this and&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // other channels, then silent join&lt;BR /&gt;#define gZdoStartMode_SilentStart_c&amp;nbsp;&amp;nbsp; 0x04 // already part of the network (no form/join needed)&lt;BR /&gt;#define gZdoStartMode_StartMask_c&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x07 // mask for above fields&lt;BR /&gt;&lt;BR /&gt;// form (ZC) or associate join (if ZR or ZED), using NVM if available&lt;BR /&gt;#define gZdoStartMode_Default_c&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (gZdoStartMode_Associate_c | gZdoStartMode_NvmSet_c)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;ZigBee Document 053520r25 (ZIGBEE HOME AUTOMATION PUBLIC APPLICATION PROFILE):&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Startup Control:&lt;BR /&gt;3 (three) if un-commissioned, so it will join network by association when join&lt;BR /&gt;command is indicated by button press sequence.&lt;BR /&gt;0 (Zero) if commissioned. Indicates that the device should consider itself a part of&lt;BR /&gt;the network indicated by the ExtendedPANId attribute. In this case it will not&lt;BR /&gt;perform any explicit join or rejoin operation.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jun 2009 16:30:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Commissioning-Startup-Control-BeeKit-code-and-Home-Automation/m-p/189410#M14462</guid>
      <dc:creator>Devitt</dc:creator>
      <dc:date>2009-06-11T16:30:31Z</dc:date>
    </item>
    <item>
      <title>Re: Commissioning: Startup Control - BeeKit-code and Home Automation Profile differences</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Commissioning-Startup-Control-BeeKit-code-and-Home-Automation/m-p/189411#M14463</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;Devitt,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You can not compare the starting primitives with the HA spec directly.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you e.g use the ZDO_Start(gSilentRejoinWithNVM_c) which most of the demo applications uses you will see the following behavior:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. if the node has never been on the a network before it will do a discovery and an association join.&lt;/P&gt;&lt;P&gt;2. if the node has valid NVM information (e.g. power cycled while participating in the network) it will silently resume its role in the network.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Start up control mode 0 requires a full commisisoning of a the SAS which normally is done through a commissioning cluster, however this cluster is not used in HA. the test is "generic text based on the SAS.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Br,&lt;/P&gt;&lt;P&gt;Mads&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jun 2009 23:18:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Commissioning-Startup-Control-BeeKit-code-and-Home-Automation/m-p/189411#M14463</guid>
      <dc:creator>Mads</dc:creator>
      <dc:date>2009-06-16T23:18:32Z</dc:date>
    </item>
  </channel>
</rss>