<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: MC9S08LG32 LCD Module Voltage?</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08LG32-LCD-Module-Voltage/m-p/188866#M14423</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello sandeepnaik,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The LG32 has an integrated LCD driver that can supply LCD waveforms for 5 V glass.&amp;nbsp; You can use the on-chip charge pump to create the 5V source needed to drive the LCD when operating the MCU at 3.3V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The only time you should connect VLL3 to 5 V is when the MCU voltage is set at 5 V.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The externally supplied voltages MUST NOT EXCEED VDD :smileysad:.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Check out the reference manual, LCD section&amp;nbsp; &lt;STRONG&gt;&lt;STRONG style="font-size: 10pt; font-family: Helvetica-Bold;"&gt;&lt;STRONG style="font-size: 10pt; font-family: Helvetica-Bold;"&gt; &lt;/STRONG&gt;&lt;/STRONG&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Table 9-19. LCD Power Supply Options.&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/microcontrollers/doc/ref_manual/MC9S08LG32RM.pdf?fpsp=1"&gt;http://cache.freescale.com/files/microcontrollers/doc/ref_manual/MC9S08LG32RM.pdf?fpsp=1&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Philip :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 10 Sep 2012 15:41:44 GMT</pubDate>
    <dc:creator>philip_drake</dc:creator>
    <dc:date>2012-09-10T15:41:44Z</dc:date>
    <item>
      <title>MC9S08LG32 LCD Module Voltage?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08LG32-LCD-Module-Voltage/m-p/188865#M14422</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using MC9S08LG32 (LQFP-80 package) with inbuilt LCD Module.&lt;/P&gt;&lt;P&gt;I am operating my core and other peripherals at 3.3 VDC.&lt;/P&gt;&lt;P&gt;Can I still operate my LCD Module from 5 VDC power-rail without damaging the controller.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Aug 2012 18:10:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08LG32-LCD-Module-Voltage/m-p/188865#M14422</guid>
      <dc:creator>sandeepnaik</dc:creator>
      <dc:date>2012-08-14T18:10:42Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08LG32 LCD Module Voltage?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08LG32-LCD-Module-Voltage/m-p/188866#M14423</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello sandeepnaik,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The LG32 has an integrated LCD driver that can supply LCD waveforms for 5 V glass.&amp;nbsp; You can use the on-chip charge pump to create the 5V source needed to drive the LCD when operating the MCU at 3.3V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The only time you should connect VLL3 to 5 V is when the MCU voltage is set at 5 V.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The externally supplied voltages MUST NOT EXCEED VDD :smileysad:.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Check out the reference manual, LCD section&amp;nbsp; &lt;STRONG&gt;&lt;STRONG style="font-size: 10pt; font-family: Helvetica-Bold;"&gt;&lt;STRONG style="font-size: 10pt; font-family: Helvetica-Bold;"&gt; &lt;/STRONG&gt;&lt;/STRONG&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Table 9-19. LCD Power Supply Options.&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/microcontrollers/doc/ref_manual/MC9S08LG32RM.pdf?fpsp=1"&gt;http://cache.freescale.com/files/microcontrollers/doc/ref_manual/MC9S08LG32RM.pdf?fpsp=1&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Philip :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Sep 2012 15:41:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08LG32-LCD-Module-Voltage/m-p/188866#M14423</guid>
      <dc:creator>philip_drake</dc:creator>
      <dc:date>2012-09-10T15:41:44Z</dc:date>
    </item>
  </channel>
</rss>