<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: Problem with Freescale Compiler</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Problem-with-Freescale-Compiler/m-p/187751#M14210</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As Markus already explained, you are using a integral only library.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Check if you do need indeed floating point numbers, for a small 8 bit chip using integers (including longs) is much efficient.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also&lt;/P&gt;&lt;P&gt;voltage = 4096/1023*result;&lt;/P&gt;&lt;P&gt;is not actually performing the computation in floating point arithmetic, instead it computes&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;voltage = 4*result;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;4096/1023 is 4 (int type), and not 4.0039100684...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;Daniel&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 05 Jun 2009 09:54:56 GMT</pubDate>
    <dc:creator>CompilerGuru</dc:creator>
    <dc:date>2009-06-05T09:54:56Z</dc:date>
    <item>
      <title>Problem with Freescale Compiler</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Problem-with-Freescale-Compiler/m-p/187749#M14208</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, i have some trouble with my programm an i hop you can help me.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Her my code&amp;nbsp;&lt;/P&gt;&lt;P&gt;for(;&lt;A href="http://freescale.i.lithium.com/i/smilies/16x16_smiley-wink.gif"&gt;&lt;IMG alt=":smileywink:" class="emoticon emoticon-smileywink" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-wink.gif" title="Smiley Wink" /&gt;&lt;/A&gt;&lt;BR /&gt;&amp;nbsp; {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; int result;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; float voltage;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ACMP1SC = 0x00; //Analog Comperator ausschalten&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ADCSC1 = 0x22;&amp;nbsp; //Kanal 1 Messung jede Sekunde&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; while (!(ADCSC1 &amp;amp; 0x80))&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; result = ~ADCRL;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; voltage = 4096/1023*result;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp; }&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The Compiler error is&lt;/P&gt;&lt;P&gt;"Link Error&amp;nbsp;&amp;nbsp; : L1822: Symbol _FSFLOAT in file C:\Users\Markus\Desktop\BAUVORHABEN\BUS_SYSTEM\SOFTWARE\EINFACHE_ROUTINEN\Analog\Analog_Data\Standard\ObjectCode\main.c.o&lt;BR /&gt;is undefined&lt;BR /&gt;Link Error&amp;nbsp;&amp;nbsp; : Link failed"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What´s wrong with this code??&lt;/P&gt;&lt;P&gt;Thanks Markus&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jun 2009 02:55:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Problem-with-Freescale-Compiler/m-p/187749#M14208</guid>
      <dc:creator>MarkusWimmer</dc:creator>
      <dc:date>2009-06-05T02:55:33Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with Freescale Compiler</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Problem-with-Freescale-Compiler/m-p/187750#M14209</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Markus,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It looks like the floating point library is missing.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When you created the project did you select the floating point option?&amp;nbsp; It appears at the bottom of&lt;/P&gt;&lt;P&gt;&amp;nbsp; one of the &lt;STRONG&gt;&lt;EM&gt;New Project Wizard&lt;/EM&gt;&lt;/STRONG&gt; dialogues.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jun 2009 09:31:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Problem-with-Freescale-Compiler/m-p/187750#M14209</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2009-06-05T09:31:30Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with Freescale Compiler</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Problem-with-Freescale-Compiler/m-p/187751#M14210</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As Markus already explained, you are using a integral only library.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Check if you do need indeed floating point numbers, for a small 8 bit chip using integers (including longs) is much efficient.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also&lt;/P&gt;&lt;P&gt;voltage = 4096/1023*result;&lt;/P&gt;&lt;P&gt;is not actually performing the computation in floating point arithmetic, instead it computes&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;voltage = 4*result;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;4096/1023 is 4 (int type), and not 4.0039100684...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;Daniel&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jun 2009 09:54:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Problem-with-Freescale-Compiler/m-p/187751#M14210</guid>
      <dc:creator>CompilerGuru</dc:creator>
      <dc:date>2009-06-05T09:54:56Z</dc:date>
    </item>
  </channel>
</rss>