<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックCAN bus - To ground or not to ground</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/CAN-bus-To-ground-or-not-to-ground/m-p/187339#M14143</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is it necessary to pass a a third wire on the bus to connect node signal grounds?&lt;/P&gt;&lt;P&gt;Is gnd necessary when tranceivers are optoisolated?&lt;/P&gt;&lt;P&gt;Split grounds, high-z to gnd and Vcc at each node?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Anders J&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 02 Mar 2011 10:44:32 GMT</pubDate>
    <dc:creator>AndersJ</dc:creator>
    <dc:date>2011-03-02T10:44:32Z</dc:date>
    <item>
      <title>CAN bus - To ground or not to ground</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/CAN-bus-To-ground-or-not-to-ground/m-p/187339#M14143</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is it necessary to pass a a third wire on the bus to connect node signal grounds?&lt;/P&gt;&lt;P&gt;Is gnd necessary when tranceivers are optoisolated?&lt;/P&gt;&lt;P&gt;Split grounds, high-z to gnd and Vcc at each node?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Anders J&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Mar 2011 10:44:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/CAN-bus-To-ground-or-not-to-ground/m-p/187339#M14143</guid>
      <dc:creator>AndersJ</dc:creator>
      <dc:date>2011-03-02T10:44:32Z</dc:date>
    </item>
    <item>
      <title>Re: CAN bus - To ground or not to ground</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/CAN-bus-To-ground-or-not-to-ground/m-p/187340#M14144</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Not only is it necessary, it is required by the CAN standard.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Needless to say, there needs to be &lt;EM&gt;some&lt;/EM&gt; sort of common ground reference between two electronic devices, or all bets are off if they try to communicate.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What will happen if you don't have a dedicated signal ground is usually that the supply ground becomes the reference instead. Meaning that the poor CAN signal will be dragged in all the dirt &amp;amp; noise there is on the supply.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Various crapplications manage to get away with not using ground only because there are plenty of high-quality CAN tranceivers on the market that can handle large voltage differences and transients, and differential comparison in CAN also helps to hide away the design flaws.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;And of course it is utterly pointless to bother with EMI filters, PCB design for EMC, cable shielding etc etc if you don't even have a signal ground.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Mar 2011 20:17:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/CAN-bus-To-ground-or-not-to-ground/m-p/187340#M14144</guid>
      <dc:creator>Lundin</dc:creator>
      <dc:date>2011-03-02T20:17:17Z</dc:date>
    </item>
  </channel>
</rss>