<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Vtst on HC908QT1/2 in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Vtst-on-HC908QT1-2/m-p/187012#M14088</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Thanks for the advice, peg and Ake.&amp;nbsp; 10k seems&amp;nbsp; a bit large to put on Vdd, did you mean to put 10k on Vtst?&amp;nbsp; I'll order some more parts tonight and check it out.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Thanks again!&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 22 Sep 2008 10:18:44 GMT</pubDate>
    <dc:creator>Impudence</dc:creator>
    <dc:date>2008-09-22T10:18:44Z</dc:date>
    <item>
      <title>Vtst on HC908QT1/2</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Vtst-on-HC908QT1-2/m-p/187009#M14085</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I am having some troubles with getting into monitor mode with the high voltage.&amp;nbsp; When I apply Vtst to the IRQ pin (I am using 8.5V for Vtst and 5V for Vdd), the chip starts to heat up surprisingly quickly and reaches over 100C.&amp;nbsp; This seems to be due to a large amount of current being drawn by the device via the IRQ pin.&amp;nbsp;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have two questions.&amp;nbsp; Is this normal?&amp;nbsp; If it is, how long can the device survive 8.5V on the IRQ pin?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'll have to order some more of these chips before I can try anything else, but I thought I'd ask here for advice.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Sep 2008 07:24:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Vtst-on-HC908QT1-2/m-p/187009#M14085</guid>
      <dc:creator>Impudence</dc:creator>
      <dc:date>2008-09-19T07:24:08Z</dc:date>
    </item>
    <item>
      <title>Re: Vtst on HC908QT1/2</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Vtst-on-HC908QT1-2/m-p/187010#M14086</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello and welcome to the fora Impudence,&lt;BR /&gt;&lt;BR /&gt;This is definitely not normal! I would say you have damaged the device here. There should not be any noticeable heating of the chip when Vtst is applied to it.&lt;BR /&gt;Accidently applying the high voltage to the wrong pin could do this. Normally one would use a series resistor with this voltage source to limit the possibility damage in this case.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Sep 2008 07:48:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Vtst-on-HC908QT1-2/m-p/187010#M14086</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2008-09-19T07:48:44Z</dc:date>
    </item>
    <item>
      <title>Re: Vtst on HC908QT1/2</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Vtst-on-HC908QT1-2/m-p/187011#M14087</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi,&lt;/DIV&gt;&lt;DIV&gt;You should put a 10 KOhm resistor in series with the Vdd.&lt;/DIV&gt;&lt;DIV&gt;If you connect it directly, the chip might latchup and burn.&lt;/DIV&gt;&lt;DIV&gt;Insert the resistor, value not too critical, and try it once more.&lt;/DIV&gt;&lt;DIV&gt;If it still draws a lot of current, measure the voltage on the Vdd input, then you will have to replace the HC908QT MCU.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Ake&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Sep 2008 15:11:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Vtst-on-HC908QT1-2/m-p/187011#M14087</guid>
      <dc:creator>Ake</dc:creator>
      <dc:date>2008-09-19T15:11:28Z</dc:date>
    </item>
    <item>
      <title>Re: Vtst on HC908QT1/2</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Vtst-on-HC908QT1-2/m-p/187012#M14088</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Thanks for the advice, peg and Ake.&amp;nbsp; 10k seems&amp;nbsp; a bit large to put on Vdd, did you mean to put 10k on Vtst?&amp;nbsp; I'll order some more parts tonight and check it out.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Thanks again!&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Sep 2008 10:18:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Vtst-on-HC908QT1-2/m-p/187012#M14088</guid>
      <dc:creator>Impudence</dc:creator>
      <dc:date>2008-09-22T10:18:44Z</dc:date>
    </item>
    <item>
      <title>Re: Vtst on HC908QT1/2</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Vtst-on-HC908QT1-2/m-p/187013#M14089</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;Yes I presume he means Vtst as well. 10k seems a little high to me as well but if it works, it is safer. Actually I checked my programmer and it only has 180R but the Vtst is stolen from the MAX232 so it is already a fairly high impedance source.&lt;BR /&gt;&lt;BR /&gt;I checked a couple of manuals and they all show 10k in the example circuit for MON08 programming.&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Sep 2008 10:52:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Vtst-on-HC908QT1-2/m-p/187013#M14089</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2008-09-22T10:52:53Z</dc:date>
    </item>
    <item>
      <title>Re: Vtst on HC908QT1/2</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Vtst-on-HC908QT1-2/m-p/187014#M14090</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi,&lt;/DIV&gt;&lt;DIV&gt;Ohoh, I am sorry, I got the resistor values mixed up.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Look at Figure 15-11 in the MC68HC908QY4/D, there should be a 9.1 V applied to /IRQ.&lt;/DIV&gt;&lt;DIV&gt;This is done with a 1 K to +12 V and a 9.1 V zener diode.&lt;/DIV&gt;&lt;DIV&gt;The 10 K resistor I was talking about, is just a pullup on the /RST pin.&lt;/DIV&gt;&lt;DIV&gt;This will always put the HC908QY/QT in Monitor mode&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The other way is to use the schematic in Figure 15-12, or 15-13 depending if you want to use the external/internal clock. But this is only good for first time programming, that is the reset vector must be 0xff, 0xff.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Ake&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Sep 2008 14:10:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Vtst-on-HC908QT1-2/m-p/187014#M14090</guid>
      <dc:creator>Ake</dc:creator>
      <dc:date>2008-09-23T14:10:04Z</dc:date>
    </item>
  </channel>
</rss>