<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Re: MMA7260 dynamic vs. static acceleration</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MMA7260-dynamic-vs-static-acceleration/m-p/185688#M13886</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you have selected the 1.5g range, and you are applying a 1g offset due to gravity, overload in one direction will occur with additional acceleration of 0.5g.&amp;nbsp; Your "shaking" may well exeed this level, resulting in saturation of tha analog output signal.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Perhaps you should try one of the less sensitive settings of the acelerometer to ascertain if this is the cause.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 24 Feb 2011 09:37:57 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2011-02-24T09:37:57Z</dc:date>
    <item>
      <title>MMA7260 dynamic vs. static acceleration</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MMA7260-dynamic-vs-static-acceleration/m-p/185686#M13884</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using the MMA7260 accelerometer located on the DEMOJM evaluation board.&lt;/P&gt;&lt;P&gt;The volatge limits go from .85 to 2.45 volts with 1.65 volts at the 0g point.&lt;/P&gt;&lt;P&gt;If I shake the accelerometer about the x-acis then I see the voltage swings from .85 to 2.45 volts.&lt;/P&gt;&lt;P&gt;So far so good.&lt;/P&gt;&lt;P&gt;Now I tilt the board 90 degress to each side of horizontal and the voltage does change in the correct direction BUT&lt;/P&gt;&lt;P&gt;it never goes to the limits of .85 and 2.45. It stops short by about .3 volts.&lt;/P&gt;&lt;P&gt;Does anyone know why?&lt;/P&gt;&lt;P&gt;Am I doing something wrong?&lt;/P&gt;&lt;P&gt;THANK YOU...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Feb 2011 23:05:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MMA7260-dynamic-vs-static-acceleration/m-p/185686#M13884</guid>
      <dc:creator>johnpaul013</dc:creator>
      <dc:date>2011-02-23T23:05:08Z</dc:date>
    </item>
    <item>
      <title>Re: MMA7260 dynamic vs. static acceleration</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MMA7260-dynamic-vs-static-acceleration/m-p/185687#M13885</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;JohnPaul,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When you tilt it +/- 90 degrees you are applying +/- 1G of acceleration.&amp;nbsp; By my calculations you are getting .5v per G out of the sensor.&amp;nbsp; When you are shaking it, it seems to be maxing out at 8/5ths of a G or 1.6G.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What is the volts per G supposed to be?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Peter House&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Feb 2011 06:09:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MMA7260-dynamic-vs-static-acceleration/m-p/185687#M13885</guid>
      <dc:creator>PeterHouse</dc:creator>
      <dc:date>2011-02-24T06:09:23Z</dc:date>
    </item>
    <item>
      <title>Re: MMA7260 dynamic vs. static acceleration</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MMA7260-dynamic-vs-static-acceleration/m-p/185688#M13886</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you have selected the 1.5g range, and you are applying a 1g offset due to gravity, overload in one direction will occur with additional acceleration of 0.5g.&amp;nbsp; Your "shaking" may well exeed this level, resulting in saturation of tha analog output signal.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Perhaps you should try one of the less sensitive settings of the acelerometer to ascertain if this is the cause.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Feb 2011 09:37:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MMA7260-dynamic-vs-static-acceleration/m-p/185688#M13886</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2011-02-24T09:37:57Z</dc:date>
    </item>
    <item>
      <title>Re: MMA7260 dynamic vs. static acceleration</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MMA7260-dynamic-vs-static-acceleration/m-p/185689#M13887</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For the sensitivity that I am using, it should be .8 volts per G.&lt;/P&gt;&lt;P&gt;The datasheet is as follows:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; x-axis parallel to gravity = 1.65V (mid-supply) of the 0 to 3.3 reference voltage.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; tilted 90 left on x-axis should be +1G or 2.45 volts.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; tilted 90 right on x-axis should be -1G or .85 volts.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; So at the current sensitivity of .8 volts per G then these numbers make sense.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; However, in real life when I tilt the accelerometer 90 degrees I see 2.15 volts to 1.15 volts.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; But shaking it very hard along the x-axis produces the 2.45 volts to .85 volts.&lt;/P&gt;&lt;P&gt;&amp;nbsp; Any help would be appreciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp; Thanks,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; --JP&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Feb 2011 03:01:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MMA7260-dynamic-vs-static-acceleration/m-p/185689#M13887</guid>
      <dc:creator>johnpaul013</dc:creator>
      <dc:date>2011-02-25T03:01:09Z</dc:date>
    </item>
  </channel>
</rss>