<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックIssue programming HC08 GZ60 with P&amp;E USB MON08 USB</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Issue-programming-HC08-GZ60-with-P-E-USB-MON08-USB/m-p/185644#M13882</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;Hello,&lt;/DIV&gt;&lt;DIV&gt;I have been using the demo 908GZ60 board to develop some code, and finally just made my own PCB with the HC08GZ60.&lt;/DIV&gt;&lt;DIV&gt;I populated the board, and flashed a sample program, which only sets up the micro, but does not do anything. I use it to make sure I can flash on my PCB.&lt;/DIV&gt;&lt;DIV&gt;Well, everything seemed OK, codewarrior was able to commmunicate with the target board, pass security, etc...erase, flash, verify, and at the end of the programming cycle, it tries to re-initialize the target board and that's when it fails.&lt;/DIV&gt;&lt;DIV&gt;It loses commmunication with the target board, and the ping, reset do not work either.&lt;/DIV&gt;&lt;DIV&gt;I tried this again with a brand new micro, and an unpopulated bosard (basically, only the HC08 and the bypass caps on VCC5) and the same happened. It seems I can only program it once, and then it is "dead".&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Am I missing something???&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I attached the circuit I use for the micro.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;BTW: The test code works repeatadly on the demo board...&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks for anyone who can give me some pointers.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;H-&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 13 Sep 2008 05:44:37 GMT</pubDate>
    <dc:creator>Haz</dc:creator>
    <dc:date>2008-09-13T05:44:37Z</dc:date>
    <item>
      <title>Issue programming HC08 GZ60 with P&amp;E USB MON08 USB</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Issue-programming-HC08-GZ60-with-P-E-USB-MON08-USB/m-p/185644#M13882</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;Hello,&lt;/DIV&gt;&lt;DIV&gt;I have been using the demo 908GZ60 board to develop some code, and finally just made my own PCB with the HC08GZ60.&lt;/DIV&gt;&lt;DIV&gt;I populated the board, and flashed a sample program, which only sets up the micro, but does not do anything. I use it to make sure I can flash on my PCB.&lt;/DIV&gt;&lt;DIV&gt;Well, everything seemed OK, codewarrior was able to commmunicate with the target board, pass security, etc...erase, flash, verify, and at the end of the programming cycle, it tries to re-initialize the target board and that's when it fails.&lt;/DIV&gt;&lt;DIV&gt;It loses commmunication with the target board, and the ping, reset do not work either.&lt;/DIV&gt;&lt;DIV&gt;I tried this again with a brand new micro, and an unpopulated bosard (basically, only the HC08 and the bypass caps on VCC5) and the same happened. It seems I can only program it once, and then it is "dead".&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Am I missing something???&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I attached the circuit I use for the micro.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;BTW: The test code works repeatadly on the demo board...&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks for anyone who can give me some pointers.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;H-&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 13 Sep 2008 05:44:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Issue-programming-HC08-GZ60-with-P-E-USB-MON08-USB/m-p/185644#M13882</guid>
      <dc:creator>Haz</dc:creator>
      <dc:date>2008-09-13T05:44:37Z</dc:date>
    </item>
    <item>
      <title>Re: Issue programming HC08 GZ60 with P&amp;E USB MON08 USB</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Issue-programming-HC08-GZ60-with-P-E-USB-MON08-USB/m-p/185645#M13883</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Got it...&lt;/DIV&gt;&lt;DIV&gt;IRQ was missing from the schematic. Deleted in the last rev. because WAKE-UP was no longer needed, without paying attention to the programming requirements.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I guess it threw me off as the connections being OK when the board programmed the first time...&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Admin, feel free to delete post if needed.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks,&lt;/DIV&gt;&lt;DIV&gt;H-&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 13 Sep 2008 13:19:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Issue-programming-HC08-GZ60-with-P-E-USB-MON08-USB/m-p/185645#M13883</guid>
      <dc:creator>Haz</dc:creator>
      <dc:date>2008-09-13T13:19:30Z</dc:date>
    </item>
  </channel>
</rss>