<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: HCS08SGFNVMSSD SGF driver in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08SGFNVMSSD-SGF-driver/m-p/185600#M13874</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Hello Pepe,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Keep in mind that the COPE bit within the SOPT register is write once after reset.&amp;nbsp; If the Beekit code already has written to this register, you won't be able to alter the previous setting.&amp;nbsp; If this is the case, you will need to change&amp;nbsp;the Beekit&amp;nbsp;code so as to disable the COP facility, or alternatively provide periodic COP timer&amp;nbsp;reset whilst waiting for the flash erase to complete.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Regards,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Mac&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;Message Edited by bigmac on &lt;SPAN class="date_text"&gt;2008-02-14&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;04:25 AM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 14 Feb 2008 01:16:31 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2008-02-14T01:16:31Z</dc:date>
    <item>
      <title>HCS08SGFNVMSSD SGF driver</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08SGFNVMSSD-SGF-driver/m-p/185596#M13870</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm working in a project with a SRB MC1321X and I need to program the flash. In other thread, I saw HCS08SGFNVMSSD SGF driver and I have integrated this code into my project. The problem is when I use the BDM Multilink step by step the project works correctly, but when I run it in normal mode the MC1321X doesn't reply.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have configured the clock correctly to have from 150kHz to 200kHz.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Has anybody worked with HCS08SGFNVMSSD? I need help.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;My best regards, PEPE&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Feb 2008 19:43:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08SGFNVMSSD-SGF-driver/m-p/185596#M13870</guid>
      <dc:creator>josehida</dc:creator>
      <dc:date>2008-02-04T19:43:31Z</dc:date>
    </item>
    <item>
      <title>Re: HCS08SGFNVMSSD SGF driver</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08SGFNVMSSD-SGF-driver/m-p/185597#M13871</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Here is a possibility. Do you have interrupts disabled while erasing?&lt;BR /&gt;If you don't disable interrupts, it will work while single stepping, but crash when not.&lt;BR /&gt;It because the vectors are not available while erasing and if one happens, the machine will crash.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Feb 2008 21:32:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08SGFNVMSSD-SGF-driver/m-p/185597#M13871</guid>
      <dc:creator>JimDon</dc:creator>
      <dc:date>2008-02-04T21:32:32Z</dc:date>
    </item>
    <item>
      <title>Re: HCS08SGFNVMSSD SGF driver</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08SGFNVMSSD-SGF-driver/m-p/185598#M13872</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Hello Pepe,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Does your code, presumably the part that&amp;nbsp;runs from RAM at this point, clear the COP timer whilst waiting for an erase to complete?&amp;nbsp; COP timeout is possible during the erase period, but is prevented from doing so during background debug mode.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Regards,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Mac&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Feb 2008 19:24:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08SGFNVMSSD-SGF-driver/m-p/185598#M13872</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2008-02-05T19:24:22Z</dc:date>
    </item>
    <item>
      <title>Re: HCS08SGFNVMSSD SGF driver</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08SGFNVMSSD-SGF-driver/m-p/185599#M13873</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Hi again,&lt;BR /&gt;&lt;BR /&gt;Thank you for your help, but before to initialize, erase and program the flash I write the following lines in my code:&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp; &amp;nbsp; __asm SEI;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; __asm lda&amp;nbsp;&amp;nbsp; #$33&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; __asm sta&amp;nbsp;&amp;nbsp; SOPT&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // ;disable COP&lt;BR /&gt;&lt;BR /&gt;Maybe I don't integrate well the code of HCS08SGFNVMSSD SGF because I load this driver in a 13192 EVB works perfectly then I make a MAC application with Beekit for 1321 SRB or 13192 EVB and I integrate the code in this application, it doesn't run.&lt;BR /&gt;Are there any application notes which describes how integrates it?&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://forums.freescale.com/message?board.id=8BITCOMM&amp;amp;message.id=9084" rel="nofollow" target="_blank"&gt;http://forums.freescale.com/message?board.id=8BITCOMM&amp;amp;message.id=9084" rel="nofollow" target="_blank&lt;/A&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Feb 2008 20:36:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08SGFNVMSSD-SGF-driver/m-p/185599#M13873</guid>
      <dc:creator>josehida</dc:creator>
      <dc:date>2008-02-13T20:36:14Z</dc:date>
    </item>
    <item>
      <title>Re: HCS08SGFNVMSSD SGF driver</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08SGFNVMSSD-SGF-driver/m-p/185600#M13874</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Hello Pepe,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Keep in mind that the COPE bit within the SOPT register is write once after reset.&amp;nbsp; If the Beekit code already has written to this register, you won't be able to alter the previous setting.&amp;nbsp; If this is the case, you will need to change&amp;nbsp;the Beekit&amp;nbsp;code so as to disable the COP facility, or alternatively provide periodic COP timer&amp;nbsp;reset whilst waiting for the flash erase to complete.&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Regards,&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;Mac&lt;/FONT&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;Message Edited by bigmac on &lt;SPAN class="date_text"&gt;2008-02-14&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;04:25 AM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Feb 2008 01:16:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08SGFNVMSSD-SGF-driver/m-p/185600#M13874</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2008-02-14T01:16:31Z</dc:date>
    </item>
  </channel>
</rss>