<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Can't Program or Enter Debug Mode on a MC9S08QE32 in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-t-Program-or-Enter-Debug-Mode-on-a-MC9S08QE32/m-p/185110#M13790</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Kef,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for the explanation.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;D&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 03 Aug 2012 04:20:59 GMT</pubDate>
    <dc:creator>Designer11</dc:creator>
    <dc:date>2012-08-03T04:20:59Z</dc:date>
    <item>
      <title>Can't Program or Enter Debug Mode on a MC9S08QE32</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-t-Program-or-Enter-Debug-Mode-on-a-MC9S08QE32/m-p/185107#M13787</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Guys,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm desperately needing your help on this issue. I designed a board with a QE32 uController and every time I used either the USB multilink or Multilink Universal I can't program the board or get the board to enter debug mode. The two Multilinks work great with the QG8 series.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;On the other hand, when I use the cyclone Pro with the board it enters debug mode and able to program the board without any problem. What I did for a test was I toggle a port on the MCU.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;D&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Aug 2012 02:15:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-t-Program-or-Enter-Debug-Mode-on-a-MC9S08QE32/m-p/185107#M13787</guid>
      <dc:creator>Designer11</dc:creator>
      <dc:date>2012-08-02T02:15:51Z</dc:date>
    </item>
    <item>
      <title>Re: Can't Program or Enter Debug Mode on a MC9S08QE32</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-t-Program-or-Enter-Debug-Mode-on-a-MC9S08QE32/m-p/185108#M13788</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I don't know why the QE32 microcontroller required the VDD Line to connect to the programming header, even if you are not using the Vdd voltage on the programmer header to power the target board.&amp;nbsp; But You have to connect it from the target board to your Multilink programmer,&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Aug 2012 22:56:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-t-Program-or-Enter-Debug-Mode-on-a-MC9S08QE32/m-p/185108#M13788</guid>
      <dc:creator>Designer11</dc:creator>
      <dc:date>2012-08-02T22:56:20Z</dc:date>
    </item>
    <item>
      <title>Re: Can't Program or Enter Debug Mode on a MC9S08QE32</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-t-Program-or-Enter-Debug-Mode-on-a-MC9S08QE32/m-p/185109#M13789</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Multilink is multivoltage tool. Since Vdd range is as big as 5 to 2.7V&amp;nbsp;or even less, you need to provide your&amp;nbsp;target Vdd to Multilink to make it able to convert logic levels&amp;nbsp;to internal Multilink levels properly.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Aug 2012 01:10:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-t-Program-or-Enter-Debug-Mode-on-a-MC9S08QE32/m-p/185109#M13789</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2012-08-03T01:10:07Z</dc:date>
    </item>
    <item>
      <title>Re: Can't Program or Enter Debug Mode on a MC9S08QE32</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-t-Program-or-Enter-Debug-Mode-on-a-MC9S08QE32/m-p/185110#M13790</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Kef,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for the explanation.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;D&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Aug 2012 04:20:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-t-Program-or-Enter-Debug-Mode-on-a-MC9S08QE32/m-p/185110#M13790</guid>
      <dc:creator>Designer11</dc:creator>
      <dc:date>2012-08-03T04:20:59Z</dc:date>
    </item>
  </channel>
</rss>