<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 SPI buffer for Mc08</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/SPI-buffer-for-Mc08/m-p/184091#M13621</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hi. Im am wondering if i is possible to create a 12 bit buffer for spi data instead of a 2 byte buffer? If so, how do i do it?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 23 May 2009 13:17:47 GMT</pubDate>
    <dc:creator>AndriesN</dc:creator>
    <dc:date>2009-05-23T13:17:47Z</dc:date>
    <item>
      <title>SPI buffer for Mc08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/SPI-buffer-for-Mc08/m-p/184091#M13621</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hi. Im am wondering if i is possible to create a 12 bit buffer for spi data instead of a 2 byte buffer? If so, how do i do it?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 23 May 2009 13:17:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/SPI-buffer-for-Mc08/m-p/184091#M13621</guid>
      <dc:creator>AndriesN</dc:creator>
      <dc:date>2009-05-23T13:17:47Z</dc:date>
    </item>
    <item>
      <title>Re: SPI buffer for Mc08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/SPI-buffer-for-Mc08/m-p/184092#M13622</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello and welcome to the fora, Andries.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What are you trying to achieve?&lt;/P&gt;&lt;P&gt;The SPI buffers are implemented in hardware, you cannot change this.&lt;/P&gt;&lt;P&gt;The SPI will always shift out 8 bits at a time with every load of SCID.&lt;/P&gt;&lt;P&gt;Most peripherals that need less than a multiple of 8 bits are aware of this and allow the unused more significant bits to be still sent but all at zero or don't care.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Jun 2009 04:21:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/SPI-buffer-for-Mc08/m-p/184092#M13622</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2009-06-02T04:21:03Z</dc:date>
    </item>
  </channel>
</rss>