<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: For MC9S08AW16 use flash beyond 16K in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/For-MC9S08AW16-use-flash-beyond-16K/m-p/184075#M13620</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, and welcome to the forum.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;To increase the amount of flash beyond 16K, you would need to&amp;nbsp;alternatively select either the 32K part of the 60K part.&amp;nbsp;&amp;nbsp;The appropriate PRM file would be used, using the new project wizard to create a project with the larger device as a target.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 21 Feb 2011 19:40:59 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2011-02-21T19:40:59Z</dc:date>
    <item>
      <title>For MC9S08AW16 use flash beyond 16K</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/For-MC9S08AW16-use-flash-beyond-16K/m-p/184074#M13619</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For MC9S08AW16 is it possible to extend the flash beyond 16K by changing the settings in linker file?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Feb 2011 14:12:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/For-MC9S08AW16-use-flash-beyond-16K/m-p/184074#M13619</guid>
      <dc:creator>rohitb</dc:creator>
      <dc:date>2011-02-17T14:12:30Z</dc:date>
    </item>
    <item>
      <title>Re: For MC9S08AW16 use flash beyond 16K</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/For-MC9S08AW16-use-flash-beyond-16K/m-p/184075#M13620</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, and welcome to the forum.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;To increase the amount of flash beyond 16K, you would need to&amp;nbsp;alternatively select either the 32K part of the 60K part.&amp;nbsp;&amp;nbsp;The appropriate PRM file would be used, using the new project wizard to create a project with the larger device as a target.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Feb 2011 19:40:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/For-MC9S08AW16-use-flash-beyond-16K/m-p/184075#M13620</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2011-02-21T19:40:59Z</dc:date>
    </item>
  </channel>
</rss>