<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックPower Lib for SMAC</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Power-Lib-for-SMAC/m-p/127145#M1355</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there a direct implementation of the PWRLIB library for the SMAC?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;K&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 24 Feb 2006 05:32:36 GMT</pubDate>
    <dc:creator>kaiki</dc:creator>
    <dc:date>2006-02-24T05:32:36Z</dc:date>
    <item>
      <title>Power Lib for SMAC</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Power-Lib-for-SMAC/m-p/127145#M1355</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there a direct implementation of the PWRLIB library for the SMAC?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;K&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Feb 2006 05:32:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Power-Lib-for-SMAC/m-p/127145#M1355</guid>
      <dc:creator>kaiki</dc:creator>
      <dc:date>2006-02-24T05:32:36Z</dc:date>
    </item>
    <item>
      <title>Re: Power Lib for SMAC</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Power-Lib-for-SMAC/m-p/127146#M1356</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi,&lt;/DIV&gt;&lt;DIV&gt;in SMAC there are primitives like: MLMEHibernateRequest or MLMEWakeRequest or.....&amp;nbsp; These functions can be used to change the transiver power&amp;nbsp;mode, also you can use the STOP modes to sleep the microprocessor.&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I hope to be usefull!&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;bye.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Feb 2006 18:58:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Power-Lib-for-SMAC/m-p/127146#M1356</guid>
      <dc:creator>xevi</dc:creator>
      <dc:date>2006-02-24T18:58:40Z</dc:date>
    </item>
    <item>
      <title>Re: Power Lib for SMAC</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Power-Lib-for-SMAC/m-p/127147#M1357</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi,&lt;BR /&gt;So when I'm ready to put the MCU to sleep I am completely switching off the Radio with a reset so I don't need to HibernateRequest or wakeRequest.&lt;BR /&gt;&lt;BR /&gt;However the problem I am having is to have a RTI timer running while the mcu is in Stop2 and have that wake me up. Are there any samples out there that show how to do this?&lt;BR /&gt;&lt;BR /&gt;But here is the greater problem I'm trying to solve :&lt;BR /&gt;I need to switch on once in a while and listen for any data specifically for me and go back to sleep if there isn't anything.&lt;BR /&gt;The only problem is that my environment is quite noisy (lots of 802.15.4 packets flying around) so its going to be a real current drain to listen for a packet, decode it and discard the ones not meant for me and go back to sleep.&lt;BR /&gt;Receive mode is a costly 37 mA and an active run mode on the MCU to decode and discard a packet.&lt;BR /&gt;&lt;BR /&gt;Can anyone suggest any strategies to minimize current drain in this scenario?&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Mar 2006 01:19:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Power-Lib-for-SMAC/m-p/127147#M1357</guid>
      <dc:creator>kaiki</dc:creator>
      <dc:date>2006-03-02T01:19:34Z</dc:date>
    </item>
  </channel>
</rss>