<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックS08jm60 with USB and 32KHZ clock</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/S08jm60-with-USB-and-32KHZ-clock/m-p/182823#M13468</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I wish to use the s08jm60 with USB, so the bus speed must be 24mhz.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The data sheet shows an example of using a 4mhz xtal which is divided down to 32khz&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;to drive the PLL which generates to 48mhz main clock.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have an external 32khz clock source (from a RTC ic) . Can I use this to feed to PLL, rather than a 4mhz xtal?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The data sheet has AC specs for 5volt operation only.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Can the micro be run at full speed (24mhz bus) at 3.3Volt ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 01 Sep 2008 04:11:18 GMT</pubDate>
    <dc:creator>donw</dc:creator>
    <dc:date>2008-09-01T04:11:18Z</dc:date>
    <item>
      <title>S08jm60 with USB and 32KHZ clock</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/S08jm60-with-USB-and-32KHZ-clock/m-p/182823#M13468</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I wish to use the s08jm60 with USB, so the bus speed must be 24mhz.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The data sheet shows an example of using a 4mhz xtal which is divided down to 32khz&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;to drive the PLL which generates to 48mhz main clock.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have an external 32khz clock source (from a RTC ic) . Can I use this to feed to PLL, rather than a 4mhz xtal?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The data sheet has AC specs for 5volt operation only.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Can the micro be run at full speed (24mhz bus) at 3.3Volt ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Sep 2008 04:11:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/S08jm60-with-USB-and-32KHZ-clock/m-p/182823#M13468</guid>
      <dc:creator>donw</dc:creator>
      <dc:date>2008-09-01T04:11:18Z</dc:date>
    </item>
    <item>
      <title>Re: S08jm60 with USB and 32KHZ clock</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/S08jm60-with-USB-and-32KHZ-clock/m-p/182824#M13469</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello Donw,&lt;BR /&gt;&lt;BR /&gt;According to the DS, that is not possible. Page 293 (USB clock requirements) states that the MCG must operate in PEE (PLL engaged external) mode with a 2 or 4MHz crystal.&lt;BR /&gt;&lt;BR /&gt;The DS also states that the PLL must have a frequency within the range of 1 MHz to 2MHz after divided by RDIV. Section 12.4.6 (External reference clock) states that when using PEE and PDE modes, the external reference clock must be within 1MHz and 16MHz.&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Sep 2008 22:24:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/S08jm60-with-USB-and-32KHZ-clock/m-p/182824#M13469</guid>
      <dc:creator>fabio</dc:creator>
      <dc:date>2008-09-03T22:24:10Z</dc:date>
    </item>
    <item>
      <title>Re: S08jm60 with USB and 32KHZ clock</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/S08jm60-with-USB-and-32KHZ-clock/m-p/182825#M13470</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I understand that a 4MHz crystal would work fine for USB usage. However, I wonder why the DEMOJM board uses a 12MHz crystal. Is there any advantage in that?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Moises&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Feb 2009 18:50:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/S08jm60-with-USB-and-32KHZ-clock/m-p/182825#M13470</guid>
      <dc:creator>Moizez</dc:creator>
      <dc:date>2009-02-19T18:50:32Z</dc:date>
    </item>
  </channel>
</rss>