<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックProblem with a MC68HC908AP16</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Problem-with-a-MC68HC908AP16/m-p/182793#M13460</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Good day, I have a problem with a MC68HC908AP16, when I work him at 3v it doesn't begin, the pin RTS stays in under, if I work him at 5v it works well that I can make so that it works me at 3v.&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;Thank you&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 31 Aug 2008 23:47:22 GMT</pubDate>
    <dc:creator>JrCL</dc:creator>
    <dc:date>2008-08-31T23:47:22Z</dc:date>
    <item>
      <title>Problem with a MC68HC908AP16</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Problem-with-a-MC68HC908AP16/m-p/182793#M13460</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Good day, I have a problem with a MC68HC908AP16, when I work him at 3v it doesn't begin, the pin RTS stays in under, if I work him at 5v it works well that I can make so that it works me at 3v.&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;Thank you&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 31 Aug 2008 23:47:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Problem-with-a-MC68HC908AP16/m-p/182793#M13460</guid>
      <dc:creator>JrCL</dc:creator>
      <dc:date>2008-08-31T23:47:22Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with a MC68HC908AP16</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Problem-with-a-MC68HC908AP16/m-p/182794#M13461</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello, and welcome to the forum.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The 908AP16 is unsuitable for operation from 3.3 volts.&amp;nbsp; The Vdd&amp;nbsp;voltage range specified in the datasheet is 4.5-5.5 volts.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;As the supply voltage increases, the LVI module will remain in the reset condition until the Vdd rises above typically 3.45 volts (3.65 volts maximum threshold).&amp;nbsp; But the normal operating voltage should not be less than 4.5 volts.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Mac&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Sep 2008 11:31:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Problem-with-a-MC68HC908AP16/m-p/182794#M13461</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2008-09-01T11:31:12Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with a MC68HC908AP16</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Problem-with-a-MC68HC908AP16/m-p/182795#M13462</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;The 908AP16 functional operating range is specified as being 2.7-5.5V in its datasheet.&amp;nbsp; The 908AP16A is specified to run @ 4.5-5.5V.&lt;BR /&gt;&lt;BR /&gt;K&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Sep 2008 21:04:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Problem-with-a-MC68HC908AP16/m-p/182795#M13462</guid>
      <dc:creator>Klined</dc:creator>
      <dc:date>2008-09-04T21:04:47Z</dc:date>
    </item>
  </channel>
</rss>