<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: rs08 internal voltage regulator ... what does it do?</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/rs08-internal-voltage-regulator-what-does-it-do/m-p/181926#M13324</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello Peter,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;For this application, I assume you would be using the KA8 device, with the availability of an ADC module.&amp;nbsp; It would appear that the voltage regulator that you refer to is used internally, but does not affect the operation of this module.&amp;nbsp; The reference voltage for the ADC would&amp;nbsp;use&amp;nbsp;internal connections to Vdd and Vss.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;However, if the thermistor and resistor&amp;nbsp;were to be&amp;nbsp;series connected between Vdd and Vss, with the junction applied to an ADC input, the measurement would be ratiometric, and independent of actual Vdd level.&amp;nbsp; With the thermistor in the upper leg, the ADC output value would be represented by the formula -&lt;/DIV&gt;&lt;DIV&gt;N = Nmax / (1 + Rth / R)&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;This would give an increasing value for increase of temperature (assuming NTC thermistor), but would be quite non-linear.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Mac&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Aug 2008 21:51:14 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2008-08-26T21:51:14Z</dc:date>
    <item>
      <title>rs08 internal voltage regulator ... what does it do?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/rs08-internal-voltage-regulator-what-does-it-do/m-p/181925#M13323</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; I am using the KA2 and KA8 parts ..&amp;nbsp;&amp;nbsp;&amp;nbsp; they are great little parts!!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;For a cost sensitive project I am considering the need for&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;an external voltage regulator. Vcc will initially be 4.5v and&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;over the life of the supply battery drop to around 3v.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Core activity is to measure temperature using a thermistor and&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;a reference resistor and then to manipulate a relay as determined by the code.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The KA2 datasheet mentions that the parts have an internal&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;voltage regulator that will drop the supplied voltage to a lower level&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;and I am wondering what this level is and if it is fixed .. and really&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;if this internal voltage regulation will be sufficient for my project and&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;that external regulation is not really needed for such a simple task.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Will somebody in the know provide a little more detail about the&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;internal voltage regulator?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks a lot.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Peter K&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Aug 2008 16:18:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/rs08-internal-voltage-regulator-what-does-it-do/m-p/181925#M13323</guid>
      <dc:creator>PeterK</dc:creator>
      <dc:date>2008-08-26T16:18:19Z</dc:date>
    </item>
    <item>
      <title>Re: rs08 internal voltage regulator ... what does it do?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/rs08-internal-voltage-regulator-what-does-it-do/m-p/181926#M13324</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello Peter,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;For this application, I assume you would be using the KA8 device, with the availability of an ADC module.&amp;nbsp; It would appear that the voltage regulator that you refer to is used internally, but does not affect the operation of this module.&amp;nbsp; The reference voltage for the ADC would&amp;nbsp;use&amp;nbsp;internal connections to Vdd and Vss.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;However, if the thermistor and resistor&amp;nbsp;were to be&amp;nbsp;series connected between Vdd and Vss, with the junction applied to an ADC input, the measurement would be ratiometric, and independent of actual Vdd level.&amp;nbsp; With the thermistor in the upper leg, the ADC output value would be represented by the formula -&lt;/DIV&gt;&lt;DIV&gt;N = Nmax / (1 + Rth / R)&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;This would give an increasing value for increase of temperature (assuming NTC thermistor), but would be quite non-linear.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Mac&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Aug 2008 21:51:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/rs08-internal-voltage-regulator-what-does-it-do/m-p/181926#M13324</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2008-08-26T21:51:14Z</dc:date>
    </item>
  </channel>
</rss>