<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Re: MC13213 &amp; SMAC</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC13213-SMAC/m-p/127072#M1332</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello,how can i get mc13213 SMAC demo applications? Where did you download the code?Could you help me,friend?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 16 Nov 2012 09:09:39 GMT</pubDate>
    <dc:creator>kingking</dc:creator>
    <dc:date>2012-11-16T09:09:39Z</dc:date>
    <item>
      <title>MC13213 &amp; SMAC</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC13213-SMAC/m-p/127070#M1330</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;Hi,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I am using one of the SMAC demo applications to test my custom board with MC13213. It looks like reading from any of the modem registers (SPI singular transaction) gives back 0x0000!?! The writing should work, because I am able to change the CLKO from the default after modem reset&amp;nbsp;32.78....KHz to 8MHZ (this only can be done by&amp;nbsp;successful write to the 0x0A register). Of cause I can suspect my hardware, but then why the writing works?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Any ideas....&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thank you!&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Aug 2006 16:46:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC13213-SMAC/m-p/127070#M1330</guid>
      <dc:creator>Anani</dc:creator>
      <dc:date>2006-08-18T16:46:02Z</dc:date>
    </item>
    <item>
      <title>Re: MC13213 &amp; SMAC</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC13213-SMAC/m-p/127071#M1331</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;It may be possible that you have shorted the MISO pin to ground, or that you are applying some sort of loading to that pin. I, too, have had some trouble with a custom board and the MC1321x. I think a lot of it had to do with loading the test pins, although my results were somewhat sporadic. Sometimes I could look at the serial communication between the modem and mcu, other times I couldn't. The clincher for me was figuring out that on one of my boards, by loading the IRQ pin with the scope, I flatlined all the other SPI lines. Do you have test points for the test pins on the MCU? The MC1321x reference manual doesn't tell you what they correspond to (merely saying that you're not supposed to connect them. Another hint, I think), but they are, as found in a reference design provided by Freescale:&lt;BR /&gt;&lt;BR /&gt;Pin 65: PTE5/SPICLK&lt;BR /&gt;Pin 66: PTE4/MOSI&lt;BR /&gt;Pin 67: PTE3/MISO&lt;BR /&gt;Pin 68: PTE2/CE_B&lt;BR /&gt;Pin 69: IRQ/IRQ&lt;BR /&gt;Pin 70: PTD1/RXTXEN&lt;BR /&gt;Pin 71: PTD3/RST_B&lt;BR /&gt;&lt;BR /&gt;Do you have another board that you could try SMAC on?&lt;BR /&gt;&lt;BR /&gt;Hope that helps.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 19 Aug 2006 00:21:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC13213-SMAC/m-p/127071#M1331</guid>
      <dc:creator>RedMountain</dc:creator>
      <dc:date>2006-08-19T00:21:24Z</dc:date>
    </item>
    <item>
      <title>Re: MC13213 &amp; SMAC</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC13213-SMAC/m-p/127072#M1332</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello,how can i get mc13213 SMAC demo applications? Where did you download the code?Could you help me,friend?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Nov 2012 09:09:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC13213-SMAC/m-p/127072#M1332</guid>
      <dc:creator>kingking</dc:creator>
      <dc:date>2012-11-16T09:09:39Z</dc:date>
    </item>
  </channel>
</rss>