<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ATD single conversion mode in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ATD-single-conversion-mode/m-p/181900#M13309</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BR /&gt;Processor Expert will generate a very nice system for this, that will sample the channels.&lt;BR /&gt;Recommend you create a separate test project, generate the code and see how it all works.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Aug 2008 20:30:46 GMT</pubDate>
    <dc:creator>JimDon</dc:creator>
    <dc:date>2008-08-26T20:30:46Z</dc:date>
    <item>
      <title>ATD single conversion mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ATD-single-conversion-mode/m-p/181899#M13308</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hi all&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am wotking on zigbe 1321x boards.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I want to use 2 ATD channels. Because there is only one ATD, I can't convert both channels at once. I should do a single conversion on the first input, then do a single conversion on the second input and again return to the first input and so on.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;My question is about the conversion mode. Should I use single conversion mode or continous mode in this case? If continous mode, how can I do this? and&amp;nbsp; If single conversion mode, should I use a timer? I know timers on this board can not be less than 4 milliseconds(250Hz).&amp;nbsp; What should I do for achieving more&amp;nbsp; sampling frequencies?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;THANKS ALOT&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Aug 2008 12:34:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/ATD-single-conversion-mode/m-p/181899#M13308</guid>
      <dc:creator>bitasobhani</dc:creator>
      <dc:date>2008-08-26T12:34:52Z</dc:date>
    </item>
    <item>
      <title>Re: ATD single conversion mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ATD-single-conversion-mode/m-p/181900#M13309</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BR /&gt;Processor Expert will generate a very nice system for this, that will sample the channels.&lt;BR /&gt;Recommend you create a separate test project, generate the code and see how it all works.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Aug 2008 20:30:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/ATD-single-conversion-mode/m-p/181900#M13309</guid>
      <dc:creator>JimDon</dc:creator>
      <dc:date>2008-08-26T20:30:46Z</dc:date>
    </item>
    <item>
      <title>Re: ATD single conversion mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ATD-single-conversion-mode/m-p/181901#M13310</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello bitasobhani,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;You should use single conversion mode and then you can launch a conversion each time you want (once you select one of yor 2 channels : for that, a conversion occurs each time you set ATD1SC in single conversion mode).&lt;/DIV&gt;&lt;DIV&gt;In continious conversion mode, a conversion occurs at each step of the program at tthe highest speed of the ATD on the same channel until you change it, so more supply current is needed.&lt;/DIV&gt;&lt;DIV&gt;You don't need to use use timer because in single mode once CCF flags is set it is automaticaly cleared after that.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I hope I have answered some your questions.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;To help, i can give a programm. Sadly, It is using only one channel.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;void ADC_INI(void)&lt;BR /&gt;&amp;nbsp;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ATD1PE = 1;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ATD1C=0x80;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ATD1SC_ATDIE = 0;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ATD1SC_ATDCO = 0;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ATD1SC_ATDCH = 0;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;}&lt;BR /&gt;void ADC_INI(void);&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;void main(void)&lt;BR /&gt;&amp;nbsp;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PTDDD = 0xFF;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PTDD = 0x00;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; for(;&lt;IMG alt=":smileywink:" class="emoticon emoticon-smileywink" id="smileywink" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-wink.gif" title="Smiley Wink" /&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; __RESET_WATCHDOG(); /* feeds the dog */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ADC_INI();&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; if(ATD1R &amp;lt;= 32768)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PTDD_PTDD0 = 1;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PTDD_PTDD1 = 1;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PTDD_PTDD3 = 1;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PTDD_PTDD4 = 1;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; if(ATD1R &amp;gt; 32768)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PTDD_PTDD0 = 0;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PTDD_PTDD1 = 0;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PTDD_PTDD3 = 0;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PTDD_PTDD4 = 0;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;seb332&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Aug 2008 20:49:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/ATD-single-conversion-mode/m-p/181901#M13310</guid>
      <dc:creator>seb332</dc:creator>
      <dc:date>2008-08-26T20:49:49Z</dc:date>
    </item>
  </channel>
</rss>