<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックMMA7660FC: 1.172g on a static table?</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MMA7660FC-1-172g-on-a-static-table/m-p/181748#M13273</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I am putting MMA7660FC on a desktop with its top surface heading up, and queries its ZOUT value, I consistently get result indicating larger than 1g. The HEX figures are 0x17, ox18 or 0x19, with 0x19 most occurs most frequently. By referring to “Appendix C - MMA7660FC Acquisition Code Table” value 0x19 indicates 1.172g, which is impossible since the assembled PCB board is on a static desktop board, not on a plane or elsewhere.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Did I make something wrong, or the chip might be just defective?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="http://forums.freescale.com/freescale/attachments/freescale/8BITCOMM/20451/1/acquisition.png"&gt;&lt;IMG border="0" src="http://forums.freescale.com/freescale/attachments/freescale/8BITCOMM/20451/1/acquisition.png" /&gt;&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Bob&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 23 Jul 2012 02:16:53 GMT</pubDate>
    <dc:creator>Bobli</dc:creator>
    <dc:date>2012-07-23T02:16:53Z</dc:date>
    <item>
      <title>MMA7660FC: 1.172g on a static table?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MMA7660FC-1-172g-on-a-static-table/m-p/181748#M13273</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I am putting MMA7660FC on a desktop with its top surface heading up, and queries its ZOUT value, I consistently get result indicating larger than 1g. The HEX figures are 0x17, ox18 or 0x19, with 0x19 most occurs most frequently. By referring to “Appendix C - MMA7660FC Acquisition Code Table” value 0x19 indicates 1.172g, which is impossible since the assembled PCB board is on a static desktop board, not on a plane or elsewhere.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Did I make something wrong, or the chip might be just defective?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="http://forums.freescale.com/freescale/attachments/freescale/8BITCOMM/20451/1/acquisition.png"&gt;&lt;IMG border="0" src="http://forums.freescale.com/freescale/attachments/freescale/8BITCOMM/20451/1/acquisition.png" /&gt;&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Bob&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Jul 2012 02:16:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MMA7660FC-1-172g-on-a-static-table/m-p/181748#M13273</guid>
      <dc:creator>Bobli</dc:creator>
      <dc:date>2012-07-23T02:16:53Z</dc:date>
    </item>
  </channel>
</rss>